Test & Tools
  • Technologies
  • More
Test & Tools
Forum Torque Screwdrivers - What do you use?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 389 subscribers
  • Views 5274 views
  • Users 0 members are here
  • torque_tools
  • screwdrivers
  • tools
Related

Torque Screwdrivers - What do you use?

tbartonnewark
tbartonnewark over 8 years ago

Hi

 

I work at Newark and I'm reviewing Torque Screwdrivers.  Do you use them?  If so what increment range is common and are you using metric or imperial.

 

My background is in rough electrical work, but I'm interested in how the torque screwdrivers are used by engineers or if they are used in PCB assembly.

 

Thanks

 

TB

  • Sign in to reply
  • Cancel

Top Replies

  • rsc
    rsc over 8 years ago +4 suggested
    Hi Tom, When I worked for Bosch we used many types of torque drivers from a few g-mm to several hundred Nm. To get the best control of clamping force, you need a device that also measures rotation angle…
  • abrain
    abrain over 8 years ago +2 suggested
    Hi Tom, I’ve recently been using one of these Wera Wera torque screwdrivers, which goes up to 3Nm and was ideal for the M3 screws used to hold some enclosures together. Personally it’s rare I use them…
Parents
  • three-phase
    0 three-phase over 8 years ago

    Personally I have only really used torque settings on high current electrical apparatus and batteries which is well out of the range offered by torque screwdrivers.

     

    The use of torque screwdrivers in the UK within the electrical industry is becoming more wide spread mostly because of the interpretation of a regulation in BS7671 and the drive by the assessment body inspectors who have started to push for their use when the carry out assessments on electricians.

     

    The regulation requires electrical accessories to be installed in accordance with the manufacturer's instructions and a number of manufacturers now are starting to add torques settings for consumer units and MCBs into their literature.

     

    Popular units in the UK are from Wera and Whia, both are VDE approved and go up to 3Nm. Screwdrivers generally need a yearly calibration to be compliant. As I am UK its metric I am afraid.

     

    They are not a popular choice with old school electricians, but interestingly they can be effective for preventing over-tightening, that can damage the apparatus, just as much as not getting the terminals tight enough.

     

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • three-phase
    0 three-phase over 8 years ago

    Personally I have only really used torque settings on high current electrical apparatus and batteries which is well out of the range offered by torque screwdrivers.

     

    The use of torque screwdrivers in the UK within the electrical industry is becoming more wide spread mostly because of the interpretation of a regulation in BS7671 and the drive by the assessment body inspectors who have started to push for their use when the carry out assessments on electricians.

     

    The regulation requires electrical accessories to be installed in accordance with the manufacturer's instructions and a number of manufacturers now are starting to add torques settings for consumer units and MCBs into their literature.

     

    Popular units in the UK are from Wera and Whia, both are VDE approved and go up to 3Nm. Screwdrivers generally need a yearly calibration to be compliant. As I am UK its metric I am afraid.

     

    They are not a popular choice with old school electricians, but interestingly they can be effective for preventing over-tightening, that can damage the apparatus, just as much as not getting the terminals tight enough.

     

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer