Test & Tools
  • Technologies
  • More
Test & Tools
Forum Torque Screwdrivers - What do you use?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 389 subscribers
  • Views 5277 views
  • Users 0 members are here
  • torque_tools
  • screwdrivers
  • tools
Related

Torque Screwdrivers - What do you use?

tbartonnewark
tbartonnewark over 8 years ago

Hi

 

I work at Newark and I'm reviewing Torque Screwdrivers.  Do you use them?  If so what increment range is common and are you using metric or imperial.

 

My background is in rough electrical work, but I'm interested in how the torque screwdrivers are used by engineers or if they are used in PCB assembly.

 

Thanks

 

TB

  • Sign in to reply
  • Cancel

Top Replies

  • rsc
    rsc over 8 years ago +4 suggested
    Hi Tom, When I worked for Bosch we used many types of torque drivers from a few g-mm to several hundred Nm. To get the best control of clamping force, you need a device that also measures rotation angle…
  • abrain
    abrain over 8 years ago +2 suggested
    Hi Tom, I’ve recently been using one of these Wera Wera torque screwdrivers, which goes up to 3Nm and was ideal for the M3 screws used to hold some enclosures together. Personally it’s rare I use them…
Parents
  • doug65
    0 doug65 over 8 years ago

    Where I work we do a variety of torque control applications:

     

    My preference is to use an electronically controlled tool. (Atlas Copco / Weber) These give an advantage of being able to control the speed in which the screw goes in. You can also report torque angle which helps in finding a stripped or cross threaded screw.  A toll set-up would cost several thousand dollars, so not economical for a few screws.

     

    When just needing a few screws I would suggest using a calibrated gage quality tool.

     

    I do calibrations for the company I work and have calibrated many store brand torque tools for employee home use and see them be off by 30% right out of the package.  If it is important enough to check it might as well be right.

     

    As far as metric or imperial, most specifications are metric for our use. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • doug65
    0 doug65 over 8 years ago

    Where I work we do a variety of torque control applications:

     

    My preference is to use an electronically controlled tool. (Atlas Copco / Weber) These give an advantage of being able to control the speed in which the screw goes in. You can also report torque angle which helps in finding a stripped or cross threaded screw.  A toll set-up would cost several thousand dollars, so not economical for a few screws.

     

    When just needing a few screws I would suggest using a calibrated gage quality tool.

     

    I do calibrations for the company I work and have calibrated many store brand torque tools for employee home use and see them be off by 30% right out of the package.  If it is important enough to check it might as well be right.

     

    As far as metric or imperial, most specifications are metric for our use. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer