Test & Tools
  • Technologies
  • More
Test & Tools
Forum Power Cables - Where to get nice ones
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 11 answers
  • Subscribers 387 subscribers
  • Views 3210 views
  • Users 0 members are here
  • banana plug
  • power supply
  • alligator clip
  • cables
  • flexible
Related

Power Cables - Where to get nice ones

kas.lewis
kas.lewis over 8 years ago

Hello All,

 

I'm looking for power cables to be used with my various power supplies. I need one end to have a banana connector and the second end to have an alligator clip. The reason I'm asking is because there are so many cables out there (even when doing a search on farnell/newark). I am preferably looking for one with silicone insulation. The reason I'm looking for this is I would really like a cable that is very flexible and can easily weave its way around my working space.

 

Any suggestions or even better product numbers would be great.

 

Thanks

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +5 suggested
    Kas, I like these a lot (with ez-hook ends): http://www.newark.com/pomona/3782-36-2/test-lead-red-914-4mm-60v-5a/dp/10M4287?st=3782-36 http://www.newark.com/pomona/3782-36-0/test-lead-black-914-4mm-60v…
  • shabaz
    shabaz over 8 years ago +5 suggested
    Hi Kas, I was going to stick this photo in a discussion earlier in the week, but didn't get around to it - it's possibly an alternative solution for some scenarios. These are really low-cost banana plug…
  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Kas, I like to make my own also. I like to use the Pomona Hookup wire which is available in Red or Black. http://www.newark.com/w/c/cable-wire-cable-assemblies/hook-up-wire-single-conductor/prl/results…
Parents
  • dougw
    0 dougw over 8 years ago

    I've seen some really classy banana plug cables, but not with alligator clips on them. The ones with alligator clips tend to be either flimsey, low capacity wire or stiff insulation or both.

    One thing I do is plug alligator clips onto banana plugs like in this picture:

    image

    This way you can use good banana cables in multipurpose roles. Unfortunately, I don't have any great commercial banana cables.

    The test leads above are 20 gage wire with high strand count (128 strands) and silicone insulation - very "wet noodle" flexible, no-tangle, low-friction with good current capacity (20A) - but they are custom made. I'm still deciding on how to implement appropriate strain relief. I have some clips with plastic insulating boots, but the white insulated clip above is much easier to operate.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 8 years ago

    I've seen some really classy banana plug cables, but not with alligator clips on them. The ones with alligator clips tend to be either flimsey, low capacity wire or stiff insulation or both.

    One thing I do is plug alligator clips onto banana plugs like in this picture:

    image

    This way you can use good banana cables in multipurpose roles. Unfortunately, I don't have any great commercial banana cables.

    The test leads above are 20 gage wire with high strand count (128 strands) and silicone insulation - very "wet noodle" flexible, no-tangle, low-friction with good current capacity (20A) - but they are custom made. I'm still deciding on how to implement appropriate strain relief. I have some clips with plastic insulating boots, but the white insulated clip above is much easier to operate.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to dougw

    I'm a heat-shrink tubing fan : )

    In the photo below are the part codes of the clips/banana plugs I've tried, but I also like the alligator clip style you've shown, the insulated types which push onto the plugs. There are some chunkier versions like that too, which will hold fat but also very thin wires.. I'll try to find their part number.

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer