Test & Tools
  • Technologies
  • More
Test & Tools
Forum Power Cables - Where to get nice ones
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 11 answers
  • Subscribers 387 subscribers
  • Views 3200 views
  • Users 0 members are here
  • banana plug
  • power supply
  • alligator clip
  • cables
  • flexible
Related

Power Cables - Where to get nice ones

kas.lewis
kas.lewis over 8 years ago

Hello All,

 

I'm looking for power cables to be used with my various power supplies. I need one end to have a banana connector and the second end to have an alligator clip. The reason I'm asking is because there are so many cables out there (even when doing a search on farnell/newark). I am preferably looking for one with silicone insulation. The reason I'm looking for this is I would really like a cable that is very flexible and can easily weave its way around my working space.

 

Any suggestions or even better product numbers would be great.

 

Thanks

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +5 suggested
    Kas, I like these a lot (with ez-hook ends): http://www.newark.com/pomona/3782-36-2/test-lead-red-914-4mm-60v-5a/dp/10M4287?st=3782-36 http://www.newark.com/pomona/3782-36-0/test-lead-black-914-4mm-60v…
  • shabaz
    shabaz over 8 years ago +5 suggested
    Hi Kas, I was going to stick this photo in a discussion earlier in the week, but didn't get around to it - it's possibly an alternative solution for some scenarios. These are really low-cost banana plug…
  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Kas, I like to make my own also. I like to use the Pomona Hookup wire which is available in Red or Black. http://www.newark.com/w/c/cable-wire-cable-assemblies/hook-up-wire-single-conductor/prl/results…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi Kas,

    I like to make my own also. I like to use the Pomona Hookup wire which is available in Red or Black.

     

    http://www.newark.com/w/c/cable-wire-cable-assemblies/hook-up-wire-single-conductor/prl/results?st=Pomona+wire

     

    This is very nice flexible wire with 192 strands of #41 wire for a core and 10Kvp insulation on the outside and rated for 20A. For the banana plugs I like to use the gold plated ones that are made for hooking up speakers.

     

    https://www.ebay.com/itm/14-Nakamichi-Speaker-banana-plug-Audio-Adapter-connector-24K-Gold-N0534-USA/182198436019?epid=1652066358&hash=item2a6bdf80b3:g:P-wAAOxy-gBR~raK

     

    I usually wrap the wire from the pomona lead with #22 or #24 ga solid wire before I put it into the Nakamichi plugs as they are designed for heavier gauge wire. The insulators screw on from the front of the plug so they are easy to deal with.

     

    I have not been totally happy with my choice of alligator clips so I will not make a recommendation on this but I will watch this thread as I bet someone has a source for some exceptional alligator clips. I want some that have good closure of the jaws so that I can grab small gauge wire without it slipping out.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 8 years ago in reply to jw0752

    You link for hook up wire is a E14 members profile.. I'm not sure that's the link you intended to provide. Other than that I'm starting to like the idea of making my own cables with parts I prefer image

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 8 years ago in reply to jw0752

    You link for hook up wire is a E14 members profile.. I'm not sure that's the link you intended to provide. Other than that I'm starting to like the idea of making my own cables with parts I prefer image

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to kas.lewis

    Hi Kas,

    Thanks for the heads up on the incorrect link that I provided. I have corrected it and it should take you to the right place now. The Pomona wire is excellent and I use a lot of it to make patch cables as well as meter probe wires.

    John

     

    Here it is again incase you don't want to return to my previous post.

     

    http://www.newark.com/w/c/cable-wire-cable-assemblies/hook-up-wire-single-conductor/prl/results?st=Pomona+wire

     

    John