Test & Tools
  • Technologies
  • More
Test & Tools
Forum Need Windows USB Driver for TENMA 72-13210 (electronic dc-load 30A/120V 300W)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 45 replies
  • Answers 7 answers
  • Subscribers 390 subscribers
  • Views 19583 views
  • Users 0 members are here
  • tenma 72-13210
  • windows 7
  • windows
  • tenma 72-13200
  • tenma 72 13200
  • tenma 72 13210
  • win7
  • usb-driver
Related

Need Windows USB Driver for TENMA 72-13210 (electronic dc-load 30A/120V 300W)

simonwahlmann
simonwahlmann over 8 years ago

Dear all,

does anyone has an idea where to find the "windows usb-driver" for this device?

 

     TENMA 72-13210 (electronic dc-load 30A/120V 300W)

 

It's not present on the attached original CD and I also couldn't find it anywhere in the internet.

 

Thanks for your support!!!

 

UPDATE 17th of Sep. 2018

Thanks for your replies so far!!!

 

The device is listed twice at "other devices" when I plug in the usb-port:

     - SZ KORAD USB Mode

    -  SZ KORAD USB Mode

 

With a CD no driver but a list of commands to control the device is provided.

There is also a Windows executable for a connection test. Its frontend shows three tabs, one for each communication port

     - Ethernet

     - RS232

     - USB

The USB obviously didn't work, because the devices had no drivers installed.

Using an rs232 to usb adapter I was able to control the device via the RS232 port. The device was then listed as "USB Serial Port (COM11)" with an FTDI driver being used.

This might be a workaround but I need to decide whether or not to oder more of these devices. So an inusable usb-port will influence my decission.

 

I tried out some random usb drivers ending up with an immediate system shutdown.

 

What else could I try?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 8 years ago in reply to simonwahlmann +2
    I have examined the drivers and they are as I expected - just basic INFs to get a USB CDC recognized with Windows' own usbser.sys driver. Unfortunately the ones there have NOT got your VID/PID pair covered…
  • dmxdesign
    dmxdesign over 7 years ago +2 verified
    Hi all i have finally got this all to work after some digging by Devinder from farnell tech suppoprt the zip file a pdf on how to resolve the usb in device manager and a folder with the serial port driver…
  • ayush_1921
    ayush_1921 over 1 year ago in reply to dmxdesign +2 suggested
    found in fernel deep with gui and terminal interface,as it farnell rebrand 3175898.zip
Parents
  • mcb1
    0 mcb1 over 8 years ago

    So this may be a bit obvious but I have to ask.

    You've tried running the setup.exe listed with CD contents ...??

     

    It seems there are various msi and cab files which are windows based files to load something.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    So this may be a bit obvious but I have to ask.

    You've tried running the setup.exe listed with CD contents ...??

     

    It seems there are various msi and cab files which are windows based files to load something.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • sjbaxter
    0 sjbaxter over 8 years ago in reply to mcb1

    The setup.exe just installs a NI Labview application to drive the Load remotely. But it only supports RS232 and USB (not LAN) and does not install any USB drivers, so the USB doesn't work on that application either. It does install a 2014 Labview core and VISA libraries, but the application doesn't actually use those!

     

    I have had an email from KORAD support saying that they have just supplied Farnell Tech Support with a solution. I don't know if thats the one that Farnell sent to me last week or something newer based on the detailed information I have supplied. If it's the one I got last week, that doesn't work either, so we'll wait and see if Farnell come up with something newer that finally addresses this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to sjbaxter

    Oh ...

     

    I've found hat the PID and VID direct Windows where to find the details for a device.

    Obviously it isn't working and most likely because of the hoops Windows would make the vendor jump through.

     

    Typically you can tell Windows that you're installing a generic device, and choose Com Port/Modem, which then allows you to get down to the actual file, but in your case it looks like the ini file isn't there.

    You can often default it to a COM port, and it will simply behave as one, but you'll need to set the speed.

     

    It's strange they have these two entries

    ³   ³       Microsoft Windows Driver Kit License - English.rtf

    ³   ³       OPC Classic COM License - English.pdf

    Hopefully they have a more user friendly solution.

     

    Mark