Test & Tools
  • Technologies
  • More
Test & Tools
Forum Simple Electronic DC Load Conditional Oscillations
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 18 answers
  • Subscribers 387 subscribers
  • Views 8119 views
  • Users 0 members are here
  • electronic_dc_load
Related

Simple Electronic DC Load Conditional Oscillations

jw0752
jw0752 over 8 years ago

I have recently completed a build of a simple DC electronic load with the specifications of 1 mA to 2000 ma and up to 55 Volts as long as total power is kept below 60 Watts. I will be blogging about this build in the coming days.

 

During the prototyping phase of the project I had no problems with oscillations but moving the design to a circuit board always has the potential to change things. In this case I find that the unit works properly if I bring up the load from a low current to the desired level or if I bring the voltage applied to the load from a low level up to the desired voltage. If however I have the load set for any value over 250 mA and then apply a voltage above 6 volts I will get an oscillation that is undesirable. Once the unit is powered and free of oscillation I am able to move the voltage to any level and the load to any level without any recurrence of the oscillation. It seems that it is just the initial impact of full voltage into a previously set load that is greater than 250 mA that triggers the oscillation.

 

Now it is very possible that the design that I have used, which has a general traditional layout with my own modifications frankensteined into it, is bad. Since I am not an engineer I can do things like this but if I fail then I need the engineers to help me clean up my mess. Here is a schematic of the project and any insights on how I can make the unit oscillation proof will be welcome.

 

image

Since this is just a tool for my own shop I can live with the oscillation anomaly as the power or the load can just routinely be brought together gently but aesthetically it would be nice if it didn't have to be babied.

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • hlipka
    hlipka over 8 years ago in reply to jw0752 +8 verified
    Things to notice: the LT1006 is not a rail-to-rail opamp. With 5V suppy its output goes up to between 4.0 and 4.4V (best case), depending on the load, which is not enough to ensure the IRF234 is fully…
  • hlipka
    hlipka over 8 years ago in reply to jw0752 +7 suggested
    Using a R2R-Opamp only solves part of the problem. When looking at the data sheet for the IRF234, especially at the diagram 'drain current vs. gate voltage', you see that even at 5V gate voltage only 1A…
  • hlipka
    hlipka over 8 years ago +6 suggested
    I cannot see the image (and directly using its URL says 'no permission'). One change that happens between a breadboard and a PCB is that on a breadboard usually the parasitic capacities are higher. This…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    I will try to repost the image of the schematic here:

     

    image

     

    I originally tried to paste it into the text and it looks really good on my end but apparently it didn't work for everyone. Thanks for the heads up hlipka

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to jw0752

    Hi John,

     

    Awesome project : ) Looking forward to reading about it more in your blog posts.

    I'm wondering if it is caused by the combination of C4 and R6. When the system is powered up for the first time, C4 is like a short, so there is a lot of current passing through R6 (from the source of the MOSFET, through C4, and up R6, to load ground. That will cause a voltage across R6, which means the voltage to the op-amp is changing. If the load is at 1A, that means the op-amp supply voltage has changed by 0.5V, which is quite significant.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago in reply to jw0752

    Hi John,

     

    Awesome project : ) Looking forward to reading about it more in your blog posts.

    I'm wondering if it is caused by the combination of C4 and R6. When the system is powered up for the first time, C4 is like a short, so there is a lot of current passing through R6 (from the source of the MOSFET, through C4, and up R6, to load ground. That will cause a voltage across R6, which means the voltage to the op-amp is changing. If the load is at 1A, that means the op-amp supply voltage has changed by 0.5V, which is quite significant.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to shabaz

    Thanks Shabaz,

     

    I feed off the inspiration that I get here on the forum. There have been several projects lately, principally your Kelvin Probes and Frank's Milliammeter that have got me building. I will post a complete report when I finish.

     

    John

    • Cancel
    • Vote Up +4 Vote Down