Test & Tools
  • Technologies
  • More
Test & Tools
Forum Simple Electronic DC Load Conditional Oscillations
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 18 answers
  • Subscribers 387 subscribers
  • Views 8119 views
  • Users 0 members are here
  • electronic_dc_load
Related

Simple Electronic DC Load Conditional Oscillations

jw0752
jw0752 over 8 years ago

I have recently completed a build of a simple DC electronic load with the specifications of 1 mA to 2000 ma and up to 55 Volts as long as total power is kept below 60 Watts. I will be blogging about this build in the coming days.

 

During the prototyping phase of the project I had no problems with oscillations but moving the design to a circuit board always has the potential to change things. In this case I find that the unit works properly if I bring up the load from a low current to the desired level or if I bring the voltage applied to the load from a low level up to the desired voltage. If however I have the load set for any value over 250 mA and then apply a voltage above 6 volts I will get an oscillation that is undesirable. Once the unit is powered and free of oscillation I am able to move the voltage to any level and the load to any level without any recurrence of the oscillation. It seems that it is just the initial impact of full voltage into a previously set load that is greater than 250 mA that triggers the oscillation.

 

Now it is very possible that the design that I have used, which has a general traditional layout with my own modifications frankensteined into it, is bad. Since I am not an engineer I can do things like this but if I fail then I need the engineers to help me clean up my mess. Here is a schematic of the project and any insights on how I can make the unit oscillation proof will be welcome.

 

image

Since this is just a tool for my own shop I can live with the oscillation anomaly as the power or the load can just routinely be brought together gently but aesthetically it would be nice if it didn't have to be babied.

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • hlipka
    hlipka over 8 years ago in reply to jw0752 +8 verified
    Things to notice: the LT1006 is not a rail-to-rail opamp. With 5V suppy its output goes up to between 4.0 and 4.4V (best case), depending on the load, which is not enough to ensure the IRF234 is fully…
  • hlipka
    hlipka over 8 years ago in reply to jw0752 +7 suggested
    Using a R2R-Opamp only solves part of the problem. When looking at the data sheet for the IRF234, especially at the diagram 'drain current vs. gate voltage', you see that even at 5V gate voltage only 1A…
  • hlipka
    hlipka over 8 years ago +6 suggested
    I cannot see the image (and directly using its URL says 'no permission'). One change that happens between a breadboard and a PCB is that on a breadboard usually the parasitic capacities are higher. This…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    Way back in the days at NZ Post Office power supplies were hard to get, and therefore building our own was the most cost effective.

    The designer/builder of one of our had similar instability issues, and I recall it got resolved withgenerous applications of 0.1uF caps in the right places.

     

    I was thinking you need some across the supply of both op amps, as close as possible with short leads, and across the output as well.

    I'd also add a 0.1 across C3 or at least filter the zener.

     

     

    I used to have the schematic for our electronic load ... it was the same power supply effectively in reverse and heating up nichrome wire.

    In those days Fets were something still to be available, and good old 2N3055 (4 of them in parallel) was the transistor of choice (although later I think we uprated)

     

    When you get it fixed, I may have a use for it. image

     

    Cheers

    Mark

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    Way back in the days at NZ Post Office power supplies were hard to get, and therefore building our own was the most cost effective.

    The designer/builder of one of our had similar instability issues, and I recall it got resolved withgenerous applications of 0.1uF caps in the right places.

     

    I was thinking you need some across the supply of both op amps, as close as possible with short leads, and across the output as well.

    I'd also add a 0.1 across C3 or at least filter the zener.

     

     

    I used to have the schematic for our electronic load ... it was the same power supply effectively in reverse and heating up nichrome wire.

    In those days Fets were something still to be available, and good old 2N3055 (4 of them in parallel) was the transistor of choice (although later I think we uprated)

     

    When you get it fixed, I may have a use for it. image

     

    Cheers

    Mark

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to mcb1

    Hi Mark,

    I have it working right now.After 6 hours and a redesigned board using a R to R Op Amp. I want to continue to test it for stability. The new build gave me even more problems with oscillations. My fix will probably not meet approval but it is the best I could come up with to get the results I was looking for. I will go into more detail tomorrow but right now it is 1:45 and I am going to crash.

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer