Test & Tools
  • Technologies
  • More
Test & Tools
Forum Inexpensive Soldering Iron?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 10 answers
  • Subscribers 387 subscribers
  • Views 9374 views
  • Users 0 members are here
Related

Inexpensive Soldering Iron?

keno
keno over 7 years ago

Hi,

 

As a poor student am looking for an inexpensive soldering iron for small infrequent projects.

 

Have done some searching and the least expensive I have found is Harbor Freight 30 Watt Lightweight Soldering Iron ($3.99 Compare to $9.99, Ironton 43985).  https://www.harborfreight.com/30-watt-lightweight-soldering-iron-69060.html

 

Appreciate any comments and other recommendations.

 

Thanks

 

Ken

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 7 years ago +5 suggested
    Hi Ken, I doubt anyone here will recommend a cheap soldering irons without temperature control for electronics. Better to spend a bit more if you can. Look for on that has adjustable temperature and changeable…
  • dougw
    dougw over 7 years ago in reply to fmilburn +5 suggested
    Frank is right, temperature control is important as soon as you can afford it. However I used a cheap uncontrolled iron for several decades before I could afford a temperature controlled iron. To use a…
  • fmilburn
    fmilburn over 7 years ago +5 suggested
    I have one of the Harbor Freight soldering iron that looks like the one you linked to which I kept for some reason. Here is the tip that came with it (top) next to the Hakko (bottom) I normally use. It…
Parents
  • fmilburn
    0 fmilburn over 7 years ago

    I have one of the Harbor Freight soldering iron that looks like the one you linked to which I kept for some reason.  Here is the tip that came with it (top) next to the Hakko (bottom) I normally use.  It looks like they cut off a nail and stuck it in image.  The Tenma irons will almost certainly be better than the Harbor Freight and the 25W non-adjustable linked above by rsjsouza appears to come with multiple tips and a decent way to remove them.

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rsjsouza
    0 rsjsouza over 7 years ago in reply to fmilburn

    fmilburn  wrote:

     

    (...) The Tenma irons will almost certainly be better than the Harbor Freight and the 25W non-adjustable linked above by rsjsouza appears to come with multiple tips and a decent way to remove them.

    I missed that. It is certainly a much better offer than the HF or the other model.

     

    Gough Lui, the unregulated irons take some time to heat up initially, but they are always operating at full power and therefore the recovery only becomes dependent on the thermal capacity of the iron. I can tell that even my FX888 has terrible recovery depending on the copper area I subject it to, but that is par for the course. I can compensate by cranking its temperature to 450°C but that can bring terrible consequences for the things being soldered.

     

    At any rate, one additional comment I would make is to be careful with capacitive coupling between the heating element inside the iron tip and the metallic housing. Depending on the construction, this may leak enough current to damage semiconductor devices. This is usually much reduced when dealing with low voltage controlled soldering stations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rsjsouza
    0 rsjsouza over 7 years ago in reply to fmilburn

    fmilburn  wrote:

     

    (...) The Tenma irons will almost certainly be better than the Harbor Freight and the 25W non-adjustable linked above by rsjsouza appears to come with multiple tips and a decent way to remove them.

    I missed that. It is certainly a much better offer than the HF or the other model.

     

    Gough Lui, the unregulated irons take some time to heat up initially, but they are always operating at full power and therefore the recovery only becomes dependent on the thermal capacity of the iron. I can tell that even my FX888 has terrible recovery depending on the copper area I subject it to, but that is par for the course. I can compensate by cranking its temperature to 450°C but that can bring terrible consequences for the things being soldered.

     

    At any rate, one additional comment I would make is to be careful with capacitive coupling between the heating element inside the iron tip and the metallic housing. Depending on the construction, this may leak enough current to damage semiconductor devices. This is usually much reduced when dealing with low voltage controlled soldering stations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to rsjsouza

    Actually, the thing may well be operating at full power all the time, but due to the lousy loose fit between the tip and the heater barrel in these cheap irons, I found my 60W cheap iron to have worse recovery characteristics and longer warm up time than my 50-or-so watt soldering station. I'll even admit to buying a 35W rated cheap iron thinking that 60W would be too much for fine electronic work only to find that took absurdly long to bring joints up to temperature resulting in some casualties. As a result, I'd have to say the coupling between the tip (related to tip design) and heater does matter.

     

    I do agree with capacitive coupling comment - in Earthed countries (like AU), I have had less issues with irons that have an Earth pin as they should have some connection/resistance to ground to dissipate ESD and stray charges

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rsjsouza
    0 rsjsouza over 7 years ago in reply to Gough Lui

    Gough Lui  wrote:

     

    Actually, the thing may well be operating at full power all the time, but due to the lousy loose fit between the tip and the heater barrel in these cheap irons, I found my 60W cheap iron to have worse recovery characteristics and longer warm up time than my 50-or-so watt soldering station. I'll even admit to buying a 35W rated cheap iron thinking that 60W would be too much for fine electronic work only to find that took absurdly long to bring joints up to temperature resulting in some casualties. As a result, I'd have to say the coupling between the tip (related to tip design) and heater does matter.

    I agree with you; thermal coupling is king. My old soldering irons had a very tight fit when hot, but I imagine the degradation of the material that was in close contact with the heating element probably reduced its efficiency - they quickly got a dark crust. Unfortunately I had no other reference to know how significant the degradation was.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer