Test & Tools
  • Technologies
  • More
Test & Tools
Forum Inexpensive Soldering Iron?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 10 answers
  • Subscribers 387 subscribers
  • Views 9372 views
  • Users 0 members are here
Related

Inexpensive Soldering Iron?

keno
keno over 7 years ago

Hi,

 

As a poor student am looking for an inexpensive soldering iron for small infrequent projects.

 

Have done some searching and the least expensive I have found is Harbor Freight 30 Watt Lightweight Soldering Iron ($3.99 Compare to $9.99, Ironton 43985).  https://www.harborfreight.com/30-watt-lightweight-soldering-iron-69060.html

 

Appreciate any comments and other recommendations.

 

Thanks

 

Ken

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 7 years ago +5 suggested
    Hi Ken, I doubt anyone here will recommend a cheap soldering irons without temperature control for electronics. Better to spend a bit more if you can. Look for on that has adjustable temperature and changeable…
  • dougw
    dougw over 7 years ago in reply to fmilburn +5 suggested
    Frank is right, temperature control is important as soon as you can afford it. However I used a cheap uncontrolled iron for several decades before I could afford a temperature controlled iron. To use a…
  • fmilburn
    fmilburn over 7 years ago +5 suggested
    I have one of the Harbor Freight soldering iron that looks like the one you linked to which I kept for some reason. Here is the tip that came with it (top) next to the Hakko (bottom) I normally use. It…
Parents
  • Gough Lui
    0 Gough Lui over 7 years ago

    I started my electronics endeavours with such cheap irons and needless to say, I'd never turn back. A lot of them have plated copper tips which are a pain in the butt, as once the coating breaks through, the bit erodes to nothing almost immediately as the solder leeches the copper. The shape of the bit is poor making fine work very problematic, the nichrome wire often gives off some unpleasant smells and they take absolutely ages to heat up to temperature and are "thermally balanced" aka unregulated, so you need to add in waiting time for heat to recover post-joint and watch the solder closely. I would attribute it to the cause of many lifted tracks from PCBs in my early days of building kits. Over long projects, the handle which is often hard plastic gets uncomfortably hot and often the temperature they come set for is hot enough to cause flux spatter.

     

    I've done many successful projects with such irons, which even included mounting the tip into a cordless drill and using a file to grind it back. But since then, I had graduated to better thermally-regulated irons and there is no looking back. The superior fine tip of such irons and feedback regulation means less heat, less flux spatter, less stress on components, less waiting between joints. I suppose it boils down to how much your patience, time, frustration and parts are worth! Aside from absolute apocalyptic circumstances, I wouldn't go back.

     

    At the least, get an iron from a proper brand - even a Hakko FX-888FX-888 can be had at a good price and isn't a bad iron if your budget stretches. I have a Metcal PS-900PS-900 which I keep safe, instead using a Tenma combination hot-air/soldering station which is fairly inexpensive but also much better. For those who need much cheaper, I've had decent experiences with Goot plug-in irons - better tips, faster warm-up and more comfort, but still with most of the downsides of the thermally balanced iron.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 7 years ago

    I started my electronics endeavours with such cheap irons and needless to say, I'd never turn back. A lot of them have plated copper tips which are a pain in the butt, as once the coating breaks through, the bit erodes to nothing almost immediately as the solder leeches the copper. The shape of the bit is poor making fine work very problematic, the nichrome wire often gives off some unpleasant smells and they take absolutely ages to heat up to temperature and are "thermally balanced" aka unregulated, so you need to add in waiting time for heat to recover post-joint and watch the solder closely. I would attribute it to the cause of many lifted tracks from PCBs in my early days of building kits. Over long projects, the handle which is often hard plastic gets uncomfortably hot and often the temperature they come set for is hot enough to cause flux spatter.

     

    I've done many successful projects with such irons, which even included mounting the tip into a cordless drill and using a file to grind it back. But since then, I had graduated to better thermally-regulated irons and there is no looking back. The superior fine tip of such irons and feedback regulation means less heat, less flux spatter, less stress on components, less waiting between joints. I suppose it boils down to how much your patience, time, frustration and parts are worth! Aside from absolute apocalyptic circumstances, I wouldn't go back.

     

    At the least, get an iron from a proper brand - even a Hakko FX-888FX-888 can be had at a good price and isn't a bad iron if your budget stretches. I have a Metcal PS-900PS-900 which I keep safe, instead using a Tenma combination hot-air/soldering station which is fairly inexpensive but also much better. For those who need much cheaper, I've had decent experiences with Goot plug-in irons - better tips, faster warm-up and more comfort, but still with most of the downsides of the thermally balanced iron.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer