Test & Tools
  • Technologies
  • More
Test & Tools
Forum DIY Lab PSU (or bench power supply): what to choose?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 5 answers
  • Subscribers 386 subscribers
  • Views 4359 views
  • Users 0 members are here
  • diy
  • power supplies
Related

DIY Lab PSU (or bench power supply): what to choose?

s1m0n3t
s1m0n3t over 6 years ago

I apologize if I will write a lot, I invite you to read only if you have a lot of free time... image

 

For some time now I have needed a versatile bench power supply, which would be useful for several general tests. I understand that the word "general" in electronics does not mean anything, because an instrument suitable for any situation is only a utopia, but from my experience I can say that it has hardly happened to me that I need voltages higher than 24V and currents higher than 3A, for small applications.

I would therefore like to build a power supply with two separate channels (possibly usable in series or in parallel), for example with maximum 2x15V.

I would like to have a very stable power supply with very low noise, so I would like it to be linear, not switching.

 

I have available (in addition to a nice metal case with "generous" dimensions) a 2x12V 6.25A (150VA) toroidal transformer. These two outputs, after being rectified, should give me 12 x 1.41 = 16.92V. After subtracting a dropout voltage, typically 1.5V, I should get my 15V per channel.

I also have two LT1083 linear regulators, which hold up to 7.5A continuous. They are very beautiful and have a TO-3P package easily mountable on a heatsink. But unfortunately it is an obsolete model, not replaced by any equivalent, so I would prefer not to use them, to make a future replacement easy, should one break.

I have found many solutions with linear regulators and a current of many amps, both with many regulators (like LM317 and equivalent) in parallel, and with bridge-connected mosfets.

 

Then I would have to make other choices:

1) Start from 1.2V of minimum voltage or adopt a more complex circuit to start from 0V

2) Adjust only the voltage or also the current (not of primary importance to me)

3) Use a simple analogue control with multiturn precision potentiometers and display to measure voltages and currents, or insert a microcontroller to control the settings with PWM, with a digital interface (in the future possibly also controlled by software)

 

But the crucial point is another: the maximum current and its dissipation.

If I want each channel to go from 0 to 15V, for low voltages I would have a maximum dropout of about 15V, which at 6A would require a dissipation of 90W !!!

Normally I would not reach this condition, because when could I ever need a 1V to 6A output? For example, it would be more likely to use 12V at 6A ((17-12) * 6 = 30W of dissipation). But I should still be in the worst conditions and I think that dissipating 90W of heat is really too much for a bench power supply, even with forced ventilation.

What do you think? What would you do for me? Settle for a much lower maximum current, not taking full advantage of my toroid? Make sure to limit the current as a function of the voltage, with a digital control, so as to keep the total dissipation below a set threshold?

After all, a good compromise could be having a precise linear variable power supply, with a low current, and a second switching power supply in case I need a higher current.

But even if I limit myself to 3A per channel, dissipating 45W of heat may not be that simple.

 

Any advice and opinions will be welcome...thank you in advice! image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +5 suggested
    Hi Simone, I feel for your desired voltage range, a good achievable aim for a linear PSU is 1A per channel. Once you've got that built you'll have something always usable, and can consider a higher-current…
  • dougw
    dougw over 6 years ago +5 suggested
    As you mention, you will likely need to keep the current to limits implied by practical heat dissipation methods. You could apply any excess current capacity to extra channels. For example some standard…
  • jeff_electron
    jeff_electron over 6 years ago +2 suggested
    Hmm tricky, the real problem is to get the best potential out of your toroid. power dissipation can normally be greatly reduced by putting a variable switcher behind the linear regulator allowing for a…
Parents
  • s1m0n3t
    0 s1m0n3t over 6 years ago

    Thank you shabaz for your precious point of view. I agree with the fact that 1A can be enough for many applications, but perhaps it is not so rare to need a little more current. I realize, however, that hoping to get 6A for the entire voltage range, while maintaining an exclusively linear configuration, is really too much.

    The idea of @dougw to get some useful fixed voltages (3.3V, 5V, 12V, for example with 1A) seems to me absolutely valid, but it would not meet the trivial needs of powering for example a 5V device with a current of 2 or 3 amps.

    It is true that on the one hand I would like to fully exploit the potential of the toroid that I have, but on the other hand I would like to obtain a good flexibility on the load that I can power: it is more likely to have to supply a device with a "generous" current at a single voltage , rather than several voltages simultaneously, each with a low current.

    Thank you so much @jeff_electron, you offered me so many ideas that could be developed. Despite all the controls mentioned could be done with analog stages (amplifiers, comparators, etc.), I could in fact centralize all the control logics on the firmware of a microcontroller.

    I was already undecided whether to keep everything analog, with two simple potentiometers, or to insert a digital control. But considering that I would still need to buy some panel displays to measure the voltage and current of the two channels, I might as well use a nice 20x4 alphanumeric display (which I already have), a microcontroller, perhaps with an external 4-channel ADC and a 4-channel DAC (for greater precision), and one or two temperature probes.

    In this way I could adjust a current limit selectable by the user (useful in some cases) and impose a limit according to a maximum tolerable temperature.

    I should choose whether to insert an analog constant current control stage, or two relays that simply isolate the outputs when the threshold is exceeded.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • s1m0n3t
    0 s1m0n3t over 6 years ago

    Thank you shabaz for your precious point of view. I agree with the fact that 1A can be enough for many applications, but perhaps it is not so rare to need a little more current. I realize, however, that hoping to get 6A for the entire voltage range, while maintaining an exclusively linear configuration, is really too much.

    The idea of @dougw to get some useful fixed voltages (3.3V, 5V, 12V, for example with 1A) seems to me absolutely valid, but it would not meet the trivial needs of powering for example a 5V device with a current of 2 or 3 amps.

    It is true that on the one hand I would like to fully exploit the potential of the toroid that I have, but on the other hand I would like to obtain a good flexibility on the load that I can power: it is more likely to have to supply a device with a "generous" current at a single voltage , rather than several voltages simultaneously, each with a low current.

    Thank you so much @jeff_electron, you offered me so many ideas that could be developed. Despite all the controls mentioned could be done with analog stages (amplifiers, comparators, etc.), I could in fact centralize all the control logics on the firmware of a microcontroller.

    I was already undecided whether to keep everything analog, with two simple potentiometers, or to insert a digital control. But considering that I would still need to buy some panel displays to measure the voltage and current of the two channels, I might as well use a nice 20x4 alphanumeric display (which I already have), a microcontroller, perhaps with an external 4-channel ADC and a 4-channel DAC (for greater precision), and one or two temperature probes.

    In this way I could adjust a current limit selectable by the user (useful in some cases) and impose a limit according to a maximum tolerable temperature.

    I should choose whether to insert an analog constant current control stage, or two relays that simply isolate the outputs when the threshold is exceeded.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 6 years ago in reply to s1m0n3t

    It's worth thinking about cost as well, depending upon what you hope to get out of the project.  I know you already have a number of the parts, but once you have to start acquiring more to support 'features', you'll find it hard to keep the cost below the purchase price of a cheap but useful unit. 

     

    If the aim is to get your power supply and have a great deal of fun getting there, which is what I did image, then crack on and keep us up to date on progress, it's always interesting to read about someone's project.  If cost may be an issue, CPC often have deals on cheaper PSUs that do all you want.  Check out their Bargain Corner - Test Equipment.  They only have single channel supplies right now but it changes; Shabaz and others have bought one of these and found it to be very good value.  CPC is part of Farnell in the UK - if you don't live here, check around local suppliers.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer