Test & Tools
  • Technologies
  • More
Test & Tools
Forum Consumption profile equipment
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 4 answers
  • Subscribers 387 subscribers
  • Views 2225 views
  • Users 0 members are here
  • tools
Related

Consumption profile equipment

jpnbino
jpnbino over 5 years ago

Hi all,

 

I've been searching for tools to measure ( profile)  the dynamic consumption of devices in normal operation and then give a report.

 

features desirable:

  • measure Max current, Average current
  • Max Voltage, Average current
  • Configurable voltage supply ( 0 ~ 12V )
  • can afford at least 1A
  • Good Software for reporting
  • Possibility to connect a battery and log the voltage and current

 

For instance, I've found was this one, but it is limited to 5V output max which is too low for my case (12v would be better ) :

https://www.qoitech.com/

 

If you people had a pleasant experience with any tool and can share, I'd appreciate it!

 

thanks,

  • Sign in to reply
  • Cancel

Top Replies

  • hlipka
    hlipka over 5 years ago +3 suggested
    The JouleScope should tick all boxes - 15V, 3A, 250kHz bandwidth. Its not exactly cheap, but for what it does its also not too expensive. Look for more current reviews - from what I remember the software…
  • michaelkellett
    michaelkellett over 5 years ago in reply to hlipka +3
    It looks quite good, and actually claims to switch the current sense resistors really fast - which must take a lot of effort since the resistance is so low on the 3A range. It's cheaper than the Quotech…
  • jpnbino
    jpnbino over 5 years ago in reply to michaelkellett +3
    Hi Michael, In my current work, we have basically all boards being powered by solar panels, batteries ( Lithium , Lead-acid battery), or supercap. Those boards are designed to: Wake up time to time read…
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi Joao,

     

    I think today if I had the choice, I'd go for a bench supply and a datalogger (see BK Precision or Hioki for instance), or a nice multimeter like DMM6500, and log to it or disk.

     

    Some of the all-in-one units intended for IoT use suggest they simulate a battery, but the only decent simulation of a LiPo is in Fortran, and so unless they are running that, I don't know how much value that is.

     

    The instruments above would be more versatile (albeit more costly).

     

    For low cost, a microcontroller and an ADC board could be used (could be an off-the-shelf ADC eval board).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jpnbino
    0 jpnbino over 5 years ago in reply to shabaz

    Hi Shabaz,

     

    Some of the all-in-one units intended for IoT use suggest they simulate a battery, but the only decent simulation of a LiPo is in Fortran

    Thanks for this info, I didn't know that.

     

    The instruments above would be more versatile (albeit more costly).

    As I was answering Michael below, I would go for it. I will search for the options and maybe I have enough material to convince my bosses.

     

    Could you check the answer I gave Michael below? I gave more details on the application and maybe it lights up some more ideas on you, but just if it does not bother you. Thank you!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to jpnbino

    Hi Joao,

     

    Your comments make sense. Also, incidentally, if there's a difference from (say) a few hundred nA between the lowest current sleep mode and the next level of current draw (say 1mA), then it can be possible to can spot that, at a useful bandwidth, and still be able to handle the highest expected current, with a single sense resistor (i.e. no switching) and a very low-cost INAxxx board (from TI), if the sense resistor is sized well per device-under-test, because a lot of IoT DUTs won't consume more than a few hundred milliamps of current (and your mentioned values also support this), and some will be just in tens of milliamps if they use low power radios. However if there are several sleep ranges close to each other then that's harder. Anyway, that could be part of an ultra-cheap option, sometimes needed perhaps. There's a short discussion here: Using the INA210-214 for Current Measurement for IoT Devices where it also mentions the possibility of moving the sizing problem to plugging in/out different gain INAxxx chips, instead of swapping out sense resistors, for different desired ranges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to shabaz

    Here's a thought - what we want is to measure over a huge dynamic range but most of the time accuracy is not that important - 1% would certainly be adequate.

    If you were to measure the voltage drop across a standard diode (or a transistor wired as a diode) it is accurately logarithmic with respect to current over many decades.

    And if you either control or measure its temperature it should be possible to remove the temperature dependence.

     

    Then you end up with a single range that can cover maybe six decades of current from 100mA to 100nA.

     

    I've messed about with the idea, and even bought some suitable transistors (you need low base and emitter resistance).

    Something like FZT849FZT849.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to shabaz

    Here's a thought - what we want is to measure over a huge dynamic range but most of the time accuracy is not that important - 1% would certainly be adequate.

    If you were to measure the voltage drop across a standard diode (or a transistor wired as a diode) it is accurately logarithmic with respect to current over many decades.

    And if you either control or measure its temperature it should be possible to remove the temperature dependence.

     

    Then you end up with a single range that can cover maybe six decades of current from 100mA to 100nA.

     

    I've messed about with the idea, and even bought some suitable transistors (you need low base and emitter resistance).

    Something like FZT849FZT849.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 5 years ago in reply to michaelkellett

    Hi Michael,

     

    A log method would be really neat, since accuracy isn't needed for most of these use-cases. A problem with the few existing all-in-one IoT tester devices, is that they still cost a lot, and sometimes several would be needed simultaneously, so then it's a huge cost for verifying transmit/idle/sleep behaviour that didn't need the accuracy in the first place. Battery life estimation isn't going to be much more accurate with those devices either.