Test & Tools
  • Technologies
  • More
Test & Tools
Forum Impact of scope noise when measuring signals
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 8 answers
  • Subscribers 385 subscribers
  • Views 12211 views
  • Users 0 members are here
Related

Impact of scope noise when measuring signals

Andrew J
Andrew J over 5 years ago

I'm currently taking noise measurements of a working circuit and I don't really understand how my scope's noise actually impacts what I see or measure so I'm hoping someone can explain it to me in non-technical (or at least not deep technical!) language.  I've measured the scope's noise floor(??) on channel 4:

 

image

Image 1: no connections

 

Scope has no probes connected, is set to maximise capture memory and is at the smallest V div possible.  I've shown RMS and pk-pk measurements (I believe RMS is more relevant to noise, is that right?)

 

Here I'm taking a signal measurement on channel 4, with the probe set at x1 using a pig-tail and the scope configured as: AC coupled, 20MHz bandwidth, peak detect acquisition, no other probes connected or channels turned on, measurements reset to zero first:

 

image

Image 2: measured signal (core signal is 0.37mV pk-pk)

 

What I'm interested in understanding:

  1. How does the scope noise measured when the channel is disconnected from a probe - noise floor? - impact on the measured signal?
  2. How do I take that into account when interpreting the signal?  For example, could I take the mean RMS value shown in image 1, from the mean RMS value in image 2?  Does it mean the scope just isn't capable of measuring signals around the min-max RMS values?
  3. I don't touch the probe once I've started taking measurements - it's connected on test points - but even a fractional movement can change the measured signal to the extent I can't trust that I've made a proper probe connection, if that makes sense.  Specifically, the amplitude of the 'spikes' can grow or shrink although the 'core' signal remains pretty much as-is; by 'core' I mean the bright green portion of what is shown.  Does that imply anything about the spikes not related to my circuit - environment noise?  Probing issue?
    I've turned off other devices and lights in the room with no impact.  I get the same signal measuring directly across an output cap (albeit a 10uF electrolytic.)  I've zoomed in to the signal in the image below - although regular, it doesn't look like switching noise:

 

image

Image 3: measured signal in image 2 zoomed in.

 

Please correct me where I've mistyped anything in the above - it helps me make sure I research the right thing and not the thing I think is right!! 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 5 years ago +6 verified
    Can't say I'm an expert, but here goes at my understanding: How does the scope noise measured when the channel is disconnected from a probe - noise floor? - impact on the measured signal? How do I take…
  • shabaz
    shabaz over 5 years ago in reply to Andrew J +3 suggested
    Hi Andrew, The 'scope noise can be higher than the power supply you're measuring, so on it's own the 'scope isn't going to provide the measurement you need I think. Regarding your question 1, you'll see…
  • DAB
    DAB over 5 years ago +2 suggested
    You raise some good issues. Without a probe attached you are getting noise through the input connectors. first thing to do is at least put a terminating load on the input so you are not picking up noise…
Parents
  • Jan Cumps
    0 Jan Cumps over 5 years ago

    If you are looking for a practical figure of the noise in your setup: handle the test leads as "an integral part of the oscilloscope".

    Attach a probe to the channel you want to test. Shortcut the ends.

    image

    Then watch the noise. This is a decent representation of the oscilloscope's noise floor in your setup.

     

    image

     

    If you want to have an indication of noise floor without probes (why?), then using a 50 Ohm or a plain shortcut at the input is better than an open input connector. Not ideal, but better. Set the channel to X1.

    A springy little piece of u-shape bent wire with one end into the BNC connector input and the other end touching the inside of the BNC shield part can do the job.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 5 years ago

    If you are looking for a practical figure of the noise in your setup: handle the test leads as "an integral part of the oscilloscope".

    Attach a probe to the channel you want to test. Shortcut the ends.

    image

    Then watch the noise. This is a decent representation of the oscilloscope's noise floor in your setup.

     

    image

     

    If you want to have an indication of noise floor without probes (why?), then using a 50 Ohm or a plain shortcut at the input is better than an open input connector. Not ideal, but better. Set the channel to X1.

    A springy little piece of u-shape bent wire with one end into the BNC connector input and the other end touching the inside of the BNC shield part can do the job.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 5 years ago in reply to Jan Cumps

    Thanks Jan, I responded to everyone in one post below.