Test & Tools
  • Technologies
  • More
Test & Tools
Forum Pocket Oscilloscopes, experiences?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 387 subscribers
  • Views 3141 views
  • Users 0 members are here
  • test
  • oscilloscope
  • picoscope
  • software
Related

Pocket Oscilloscopes, experiences?

Catwell
Catwell over 16 years ago
A friend of mine just bought a "pocket" Oscilloscope, a DSO nano to be exact. It's self contained, onboard LCD that rivals my cell phone's, 1Mhz bandwidth, stores waveforms, and is only single channel. Perhaps I am suffering from gadget lust here, but it looks amazing, and I feel I must have one. However, I've never used any o-scope on that scale. To anyone who has, what can I expect?  I like the portability, the functions, and defilitely the price. And I am aware that I can only measure signals of up to 100khz with a 1Mhz bandwidth, but I rarely need to exceed that frequency.


Cabe
  • Sign in to reply
  • Cancel

Top Replies

  • vsluiter
    vsluiter over 11 years ago in reply to aat14 +1
    We've had some nice discussions about oscilloscopes and their specs in this topic: http://www.element14.com/community/message/137641/l/re-recommendations-for-an-oscilloscope#137641 , especially on the…
Parents
  • dougw
    0 dougw over 11 years ago

    Hi Cabe,

    I have used a number of pocket scopes and USB scopes and the one I like the best (by far) is a DS203, sometimes called DSO Quad.

    It easily fits in a pocket and is extremely handy in many unexpected ways - like fitting in the video below without blocking the main subject matter. And having a battery-operated signal generator (completely isolated) can be very useful if such functionality is needed.

    It has 2 analog channels (72Ms/s) and 2 digital channels plus a signal generator - and is based on an ARM Cortex M3.

    It is fairly full featured with all the standard functionality and lots of other features - the only real warning that should be mentioned is that the user interface is not the usual scope knob layout, so count on a bit of a learning curve to become proficient at selecting settings.

    You can see it in use in some of my videos - like this one:

    Smarter Life Challenge - The Henrietta Project - Light Sensor

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    Hi Cabe,

    I have used a number of pocket scopes and USB scopes and the one I like the best (by far) is a DS203, sometimes called DSO Quad.

    It easily fits in a pocket and is extremely handy in many unexpected ways - like fitting in the video below without blocking the main subject matter. And having a battery-operated signal generator (completely isolated) can be very useful if such functionality is needed.

    It has 2 analog channels (72Ms/s) and 2 digital channels plus a signal generator - and is based on an ARM Cortex M3.

    It is fairly full featured with all the standard functionality and lots of other features - the only real warning that should be mentioned is that the user interface is not the usual scope knob layout, so count on a bit of a learning curve to become proficient at selecting settings.

    You can see it in use in some of my videos - like this one:

    Smarter Life Challenge - The Henrietta Project - Light Sensor

    Doug