Test & Tools
  • Technologies
  • More
Test & Tools
Forum Milliohm meter
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 388 subscribers
  • Views 3863 views
  • Users 0 members are here
  • meter
  • milliohm
Related

Milliohm meter

e14 Contributor
e14 Contributor over 12 years ago

Considering a milliohm meter to measure the resistance of windings in a 3-phase motor.  Typical resistance is in the range of 0.1 ohm and need to discern probably 0.001 ohm differences in order to determine if there are problems in the windings.

Any recommendations out there on milliohm meters?  Are the $400 units okay, or do I need to spend several thousand?

 

Steve G. in MD

  • Sign in to reply
  • Cancel

Top Replies

  • vsluiter
    vsluiter over 12 years ago +1
    Another way to measure milliohms reliably is to use a normal lab power supply and a decent multimeter with millivolt range. If you are allowed to pump 1A DC through a winding, measuring the voltage over…
  • mcb1
    mcb1 over 12 years ago in reply to ravi_butani +1
    All very useful ... but If I read correctly the intention was to check windings for a shorted turn.?? I turn shorted in 100, 200 or even 50 may not show any reading change, unless the motor had a previous…
  • nermash
    nermash over 12 years ago +1
    I fully agree that testing for shorted windings with a miliohm meter is not the best thing to do. I believe that there are some testers around for that purpose, probably based on the "ringer" type used…
  • element14jamie
    0 element14jamie over 12 years ago

    Hello Steve,

    Welcome to the element14 Community, we hope you are enjoying it! I will move this to the Test & Measurement area as it is a better fit.

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nermash
    0 nermash over 12 years ago

    My choice would probably be Cambridge/IET 510A with 1uOhm resolution and 0.02% basic accuracy image

    There are some deals on ebay from time to time, but it is pretty rare... I believe that new one cost around 2k USD.

     

    However, for more reasonable budget I would use my DER EE (IET) DE 5000 LCR meter, with 20000 counts on 20 ohm range (parallel/series mode) it has 1 m Ohm resolution, or DC resistance resolution of 10 m Ohms. Nice thing is that it is not expensive and it supports 4 wire measurement.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago

    A DC check (meter) is unlikely to show a shorted turn.

     

    If you check around they often use a 'growler' which is basically the primary winding of a transformer.

    If the armature under test is introduced the shorted turn represents a significant load (being a short) and it starts buzzing and vibrating as the magnetic field is loaded.

     

    couple of links

    http://www.vintage-radio.net/forum/showthread.php?t=14317

    http://www.google.co.nz/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&uact=8&ved=0CBsQFjAA&url=http%3A%2F%2Ftoshont.c…

     

    sorry got to run but try this in google, there are quite a few others.

    checking shorted turns

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago

    Another way to measure milliohms reliably is to use a normal lab power supply and a decent multimeter with millivolt range.

    If you are allowed to pump 1A  DC through a winding, measuring the voltage over the winding will give you the resistance (R=V/I -> with I = 1 -> R=V). Of course, increasing the current will increase resolution. If needed, you can buy / build a precision power resistor to check your current source once in a while.

    For measurements of this type, of course you'll need to use Kelvin Connections -> Kelvin Connected - ElectroWiki

    I've used a setup of this type to characterize contact resistance of several types of connectors. Do be aware that heating copper will increase its resistance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ravi_butani
    0 ravi_butani over 12 years ago

    Even you are using standard milliohm meters... Dont forget to calibrate it at every measurement to eliminate probe resistance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to ravi_butani

    All very useful ... but

     

    If I read correctly the intention was to check windings for a shorted turn.??

     

    I turn shorted in 100, 200 or even 50 may not show any reading change, unless the motor had a previous reading stored.

    I found the reference to the device

    http://en.wikipedia.org/wiki/Growler_%28electrical_device%29

    http://cr4.globalspec.com/thread/78322/shorted-turns-tester

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nermash
    0 nermash over 12 years ago

    I fully agree that testing for shorted windings with a miliohm meter is not the best thing to do.

    I believe that there are some testers around for that purpose, probably based on the "ringer" type used to check flyback transformers back in the TV repair days, I would probably try to measure impedance with an LCR meter and try to make some educated guess... However, I have never tried this, I don't work with poly phase AC systems, so take this with a grain of salt image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • philb6502
    0 philb6502 over 12 years ago

    Hi Steve,

    My Hameg 'scope has a "component tester" function for testing Semiconductors etc.

    It may be worth trying a component tester on the winding with a shorted turn...Comparing it to a winding that you know works.

    This would be more likely to work with windings with a higher DC resistance.

    philb

    .