Test & Tools
  • Technologies
  • More
Test & Tools
Forum Milliohm meter
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 388 subscribers
  • Views 3866 views
  • Users 0 members are here
  • meter
  • milliohm
Related

Milliohm meter

e14 Contributor
e14 Contributor over 12 years ago

Considering a milliohm meter to measure the resistance of windings in a 3-phase motor.  Typical resistance is in the range of 0.1 ohm and need to discern probably 0.001 ohm differences in order to determine if there are problems in the windings.

Any recommendations out there on milliohm meters?  Are the $400 units okay, or do I need to spend several thousand?

 

Steve G. in MD

  • Sign in to reply
  • Cancel

Top Replies

  • vsluiter
    vsluiter over 12 years ago +1
    Another way to measure milliohms reliably is to use a normal lab power supply and a decent multimeter with millivolt range. If you are allowed to pump 1A DC through a winding, measuring the voltage over…
  • mcb1
    mcb1 over 12 years ago in reply to ravi_butani +1
    All very useful ... but If I read correctly the intention was to check windings for a shorted turn.?? I turn shorted in 100, 200 or even 50 may not show any reading change, unless the motor had a previous…
  • nermash
    nermash over 12 years ago +1
    I fully agree that testing for shorted windings with a miliohm meter is not the best thing to do. I believe that there are some testers around for that purpose, probably based on the "ringer" type used…
Parents
  • philb6502
    0 philb6502 over 12 years ago

    Hi Steve,

    My Hameg 'scope has a "component tester" function for testing Semiconductors etc.

    It may be worth trying a component tester on the winding with a shorted turn...Comparing it to a winding that you know works.

    This would be more likely to work with windings with a higher DC resistance.

    philb

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • philb6502
    0 philb6502 over 12 years ago

    Hi Steve,

    My Hameg 'scope has a "component tester" function for testing Semiconductors etc.

    It may be worth trying a component tester on the winding with a shorted turn...Comparing it to a winding that you know works.

    This would be more likely to work with windings with a higher DC resistance.

    philb

    .