Test & Tools
  • Technologies
  • More
Test & Tools
Forum Mystery Part  What is it?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 387 subscribers
  • Views 1729 views
  • Users 0 members are here
Related

Mystery Part  What is it?

jw0752
jw0752 over 11 years ago

While salvaging a board marked as an Auto Focus Servo I came across this component the likes of which I have never seen before. It is marked with the following numbers: 16 0M 9330SMI. It is identified as Y1 on the print layer of the board. It has 2 visible contacts along the edges. I have not removed it yet to see if there are more underneath. The front of the component is clear glass. Inside the window I can see what looks like a golden mirror with two legs that come down and make contacts. This is for my curiosity so it isn't very important but if anyone knows what it is let me know. Photos are attached.

John

 

image

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago in reply to shabaz +1
    Hi Shabaz, Thanks for the insight into this part. You are right it is a little bit older, I would guess 10 years at least and from the construction of the board and the other components used perhaps a…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    probably a 16Mhz Xtal as part of an oscillator

     

    Crystals / resonators are typically marked with a Y, in this case Y1, the 16.0M is probably the frequency

     

    It is unusual to be clear but kind cool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    I actually didn't see the decimal point in the 16 . 0 until I had posted it. You are probably correct as it is wired with caps to ground on each leg just like traditional crystals. Can you think of any reason why they would have exposed the crystal? Does light affect the crystal?

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    I actually didn't see the decimal point in the 16 . 0 until I had posted it. You are probably correct as it is wired with caps to ground on each leg just like traditional crystals. Can you think of any reason why they would have exposed the crystal? Does light affect the crystal?

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 11 years ago in reply to jw0752

    Hi John!

     

    I have not seen one like that in a while, but it does look familiar. It's something to do with the manufacture/quality of the product, I'm guessing some factories were better at making reliable crystals with a glass enclosure,

    whereas cheaper ones had metal cans and the crystal just hanging in mid-air - I remember taking some apart!). So you've probably got a crystal which is old but was a high quality part for its time.

    Nowadays I'm sure things have changed due to process improvements, and many crystals have metal or ceramic enclosure and looks alone would not indicate as much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to shabaz

    Hi Shabaz,

    Thanks for the insight into this part. You are right it is a little bit older, I would guess 10 years at least and from the construction of the board and the other components used perhaps a little better quality too. When I get the chance I am going to hook it up in a simple oscillator circuit like we discussed a couple weeks ago and hit the crystal with a laser to see if the oscillation is affected. As you said it is probably just a neat way to package but the window peaks my curiosity about a light connection.

    John