Test & Tools
  • Technologies
  • More
Test & Tools
Forum Mystery Part  What is it?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 387 subscribers
  • Views 1713 views
  • Users 0 members are here
Related

Mystery Part  What is it?

jw0752
jw0752 over 11 years ago

While salvaging a board marked as an Auto Focus Servo I came across this component the likes of which I have never seen before. It is marked with the following numbers: 16 0M 9330SMI. It is identified as Y1 on the print layer of the board. It has 2 visible contacts along the edges. I have not removed it yet to see if there are more underneath. The front of the component is clear glass. Inside the window I can see what looks like a golden mirror with two legs that come down and make contacts. This is for my curiosity so it isn't very important but if anyone knows what it is let me know. Photos are attached.

John

 

image

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago in reply to shabaz +1
    Hi Shabaz, Thanks for the insight into this part. You are right it is a little bit older, I would guess 10 years at least and from the construction of the board and the other components used perhaps a…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    There was a time when quartz for oscillators (I think it had some application in IF filters early on as well, IIRC) was a strategic mineral, the only source of which was a mine in Arkansas.  Sometime after the war the US delivered a coupla tons of the stuff to Japan.  This is said to mark the beginning of trust in the new relationship.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    There was a time when quartz for oscillators (I think it had some application in IF filters early on as well, IIRC) was a strategic mineral, the only source of which was a mine in Arkansas.  Sometime after the war the US delivered a coupla tons of the stuff to Japan.  This is said to mark the beginning of trust in the new relationship.