Test & Tools
  • Technologies
  • More
Test & Tools
Forum Advice in oscilloscope needs
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 387 subscribers
  • Views 1886 views
  • Users 0 members are here
  • oscilloscope
  • logic_analyzer
  • advice
Related

Advice in oscilloscope needs

e14 Contributor
e14 Contributor over 11 years ago

Hi Guys,

Oscilloscope noob here! I am doing some various tinkering that I think I could use an oscilloscope for and I am wondering if the DS201 will do what I need. I have a bunch of old Commodore 64s that I would like to try and fix so I would like to check that the clock outputs from the various chips are working. Will the Nano be ok for this? Looking at thew review and the specs for the C64 I suspect not?

 

My other project is I am trying to interface a six button Sega Megadrive controller to a Arduino Pro Micro using the sketch from here: Sega Genesis controllers and Arduino revisited | Jon Thysell

However it is only working in 3 button mode yet the controller appears to work ok with a real megadrive so I want to be able to look at and measure the pulsed sequences that are sent to the controller so I can emulate them exactly with the Arduino. The pulse widths are around 20 microsecs but could be less. So do you think the Nano 201 will be able to show me what the exactly series of pulses being generated by the Megadrive are?

 

Obviously these are just hobbies so I am not looking to spend a lot of money but if it isnt going to be able to do what I need then I will look elsewhere maybe a second hand something? I have also thought that the Hantek 6022BE might be a better option perhaps?


Edit: Also I am wondering if what would be better for what i am wanting to do would be a logic analyser?

 

Thanks for the advice,

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor +1
    It would be at its limits at 8Mhz because its sampling is only 48Mhz so even a 4* overhead would barly give you 10Mhz An alternate option is to purchase an older analogue scope. there are very good and…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to e14 Contributor +1
    It's okay to buy a second hand analog scope. But It's also okay to buy a 2nd hand digital one. Since Rigol released their new DSxx4Z series, the price of second hand DS10x2's has gone down - almost to…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    I would go for a low cost but full oscilloscope

     

    the DS102 has only DC coupling so can not look at small signals with large DC offset

    limited to 200Khz at best so no good for uController clock pins and the like which often run in the Mhz ranges

    would not handle high speed I2C, SPI signals

     

     

    for a similar cost you can get a 2 channel scope with a full screen (4-7") depending on model and maker and it will with perhaps a 50Mhz bandwidth (Not sample rate, but actual bandwidth) and this will handle the common microcontrollers etc.

     

    something like the following

    500$ :- TBS1000B-EDU Digital Storage Oscilloscope | Tektronix

    For 250$ ish you can get one of these that has receved alot of good reviews, check out Dave Jones blog (the EEVBlog)  Rigol DS1052E 50MHz Digital Oscope with 2 Channels, USB Storage Access, 1 GSa/sec sampling: Science Lab Oscilloscopes: A…

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    I would go for a low cost but full oscilloscope

     

    the DS102 has only DC coupling so can not look at small signals with large DC offset

    limited to 200Khz at best so no good for uController clock pins and the like which often run in the Mhz ranges

    would not handle high speed I2C, SPI signals

     

     

    for a similar cost you can get a 2 channel scope with a full screen (4-7") depending on model and maker and it will with perhaps a 50Mhz bandwidth (Not sample rate, but actual bandwidth) and this will handle the common microcontrollers etc.

     

    something like the following

    500$ :- TBS1000B-EDU Digital Storage Oscilloscope | Tektronix

    For 250$ ish you can get one of these that has receved alot of good reviews, check out Dave Jones blog (the EEVBlog)  Rigol DS1052E 50MHz Digital Oscope with 2 Channels, USB Storage Access, 1 GSa/sec sampling: Science Lab Oscilloscopes: A…

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer