Test & Tools
  • Technologies
  • More
Test & Tools
Forum mini project: PICO-PI programmable Lab Switch (with SCPI and FreeRTOS)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 383 subscribers
  • Views 2155 views
  • Users 0 members are here
  • pico_freertos_smp
  • pico_freertos_scpi_switch
  • pico
  • scpi
Related

mini project: PICO-PI programmable Lab Switch (with SCPI and FreeRTOS)

Jan Cumps
Jan Cumps over 3 years ago

goal: make a programmable lab switch, that can switch a set of signals or supplies on or off

  • can be used in an automated process, with other lab instruments
  • may be used to switch power on/off, simulate a button click, switch an audio input on/off, ...
  • simple: you can control IO pins, that can drive a relay, FET, or any other switching element that can be controlled with a generic 3.3V GPIO.

image

reality: It 'll be a Pico with relais attached, and you control these over its USB port.
I've made several designs earlier, that use the patterns for this project:

  • SCPI library to turn user commands into to GPIO output pin state changes (yes: just on/of Grinning)
  • UART handling in FreeRTOS, with interrupt support
  • FreeRTOS concepts like: messaging, queues, semaphore, tasks

SCPI commands and matching LabVIEW driver will be compatible with a similar project I made for the Pi Propper.
A typical command would look like this:
:DIGITAL:OUTPUT0 ON

A LabVIEW flow:

image

real goal: it 'll be a showcase for using FreeRTOS with the PICO-PI in a real-world application. I've been testing out the multi-core version of the RTOS on the Pico lately, and this is a practical use case.
little bonus: It 'll run on FreeRTOS standard, and on the multi-core FreeRTOS SMP. On SMP, it 'll use both RP2040 cores.

If you have a Pico (or other RP2040 board), you can play along. No additional hardware required (the on-board LED will do) , and you can use a simple terminal (PuTTY, ...) or Python instead of LabVIEW.
I've attached the project skeleton to this post. It's a FreeRTOS blinky (already adapted for this project), a good way to check if you can successfully build a project for the Pico C SDK and the FreeRTOS port. That's the only assumption I make at the start of this series.

Link to all posts

freertos_scpi_switch_20221016.zip

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +6
    Genius little detail is the way to tame the long jumper wires on the breadboard. I am going to add this to my small helpful tricks folder of my prototyping toolbox.
  • ntewinkel
    ntewinkel over 3 years ago in reply to wolfgangfriedrich +3
    I noticed that too! Funny how sometimes the details stand out like that
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +2
    And reading that, I always wanted to know more about SCPI. rscasny this might be a good topic for an essentials lesson.
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    Genius little detail is the way to tame the long jumper wires on the breadboard. I am going to add this to my small helpful tricks folder of my prototyping toolbox. Thumbsup

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to wolfgangfriedrich

    I noticed that too!

    Funny how sometimes the details stand out like that Smiley

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 3 years ago in reply to wolfgangfriedrich

    I noticed that too!

    Funny how sometimes the details stand out like that Smiley

    • Cancel
    • Vote Up +3 Vote Down