Test & Tools
  • Technologies
  • More
Test & Tools
Forum goal for 2023: use a conical solder tip and enjoy it
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 382 subscribers
  • Views 28846 views
  • Users 0 members are here
Related

goal for 2023: use a conical solder tip and enjoy it

Jan Cumps
Jan Cumps over 3 years ago

You have to challenge your habits. I have always soldered with chisel and sloped/bevel round tips.
Many irons come with a conical tip. A lot of people solder happily with it.

image

I have several, to use with an iron that I like. But I don't like soldering with the conical tips. I am not good at it.
That's going to change this year. I'm going to try and always use these tips when appropriate, and learn to love them.
The real goal is to become better at soldering with the conical versions than I am now with chisel and sloped types. And to enjoy the adaption path.

I'll keep you posted.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago in reply to ntewinkel +5
    Hehe at least you got a choice : ) I didn't know of any other styles growing up, other than bevel. All the instructions taught everyone to use this style of tip: This is from the children's Ladybird…
  • shabaz
    shabaz over 3 years ago +4
    Maybe they are good on QFN. They look like they could be usable to drag the tip right into the corner when manually soldering QFN. I'm the same, no good with conical. Although the very finest/pointiest…
  • Gough Lui
    Gough Lui over 3 years ago +4
    I've used my conical so much that it's "turned" into a chisel :). My technique hasn't changed much really ... but I do prefer conical for the potential for fine-pitch touch-ups. Not as nice for transferring…
Parents
  • genebren
    genebren over 3 years ago

    My go to tip is the chisel (a very fine chisel that almost looks conical, only 1mm flat tip).  I too am no good with the conical.  Who would think that a 1mm flat could make that much difference?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 3 years ago in reply to genebren

    I think that Gough Lui stated the obvious issue that I have run into, poor heat transfer.  The rounded tip and sides of the cone, make it really difficult to get enough heat into the traces and component leads to get the solder to flow.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to genebren

    NASA has released their solder practice education videos for staff and contractors, and they demand the use of conical tips.

    Conical also allows for decent heat transfer, if you position the tip to match the area you want to heat.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to genebren

    I find the heat transfer issue is a tricky one - this is probably where my technique differs slightly to using chisel tips.

    I tend to find myself leaving a bit more of a "film" of solder on the conical as I go to solder the next joint. The tiny amount of solder forms a great bridge to transfer heat into the components. Others who "clean" the tip until it's completely bare will only be transferring heat at the contact points which could go slowly if a tiny bit of oxide film gets in the way.

    I guess this is something I've come to automatically adjust to - it doesn't pose me any problems anymore ... it's just remembering not to clean the tip too cleanly ... or maybe even providing a tiny bit of solder to the tip as the joint is being formed to accelerate the heat transfer.

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Jan Cumps

    Can you give me a reference for it? I have NASA-STD-87393.3 w/ Change 2 DEC 1997 which is the main standard.  Chapter 6.5 it says

    a. Select tools and equipment that provide a means of applying and controlling the
    amount of heat to the metals to be joined that is compatible with their size, shape, and thermal
    conductivity.
    b. Prohibit the use of soldering guns. 

    have/had the NASA soldering school cert (before Surface Mount). I normally work at least a 45-degree angle sometimes more. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Jan Cumps

    Can you give me a reference for it? I have NASA-STD-87393.3 w/ Change 2 DEC 1997 which is the main standard.  Chapter 6.5 it says

    a. Select tools and equipment that provide a means of applying and controlling the
    amount of heat to the metals to be joined that is compatible with their size, shape, and thermal
    conductivity.
    b. Prohibit the use of soldering guns. 

    have/had the NASA soldering school cert (before Surface Mount). I normally work at least a 45-degree angle sometimes more.