Test & Tools
  • Technologies
  • More
Test & Tools
Forum Observing 96MHz clock signal and its divisions leads to "strange" results
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 382 subscribers
  • Views 1914 views
  • Users 0 members are here
  • multicomp pro oscilloscope
  • dso
  • oscilloscope
Related

Observing 96MHz clock signal and its divisions leads to "strange" results

obones
obones 11 months ago

Hello all,

I'm toying (pun intended) with ideas in the context of a future challenge and while I'm not settled on what the thing should do, I'm decided on using the MAX32666FTHR2 board that I was gifted with a couple of years back.

The "Light Up Your Life Challenge" gave me a push to finally use the 8*8 WS2812B matrix that I once bought because it looked nice and was not expensive, and so I'm trying to hook it up to the board.

As I can't seem to get the proper output signal to send to the LEDs, I decided to observe what's coming out of the MAX32666 pins.

My first experiment was to use a continuous timer, whose clock is half the system clock (96MHz) and which toggles the output pin every time the counter reaches the comparison value. Here is what I get with two relatively high values:

image image

The signal should be a nice square wave, it does not look that clean, but I know there's always some rise and fall time coming into play.

But things get worse when the comparison value for the timer is even lower, like here with 3:

image

After further fiddling with the various peripherals on the MCU, I was able to output the 96MHz clock signal, and this is what I get:

image

I had to stop the oscilloscope because it was not able to see a proper trigger level, let alone compute the frequency from such small signal.

Now, if I read the graph properly, there's about 10ns between two peaks, which is consistent with a 96MHz frequency for the signal.

However, what I'm really wondering about is the fact that the faster the signal, the more distorted I observe it, to the point where it won't even reach full voltage swing between 0V and 3.3V.

Out the top of my head, I can see three reasons for these results:

  1. Reaching the limits of the MAX32666 pin switching capabilities
  2. Reaching the limits of what the oscilloscope can see
  3. Reaching the limits of my own stupidity

For point 1, I tried looking for rise and fall time on output pins in the electrical characteristics for the MAX32666 but could not find anything related to this in the (somewhat confusing) datasheet.

For point 2, the DSO is said to be "100MHz" so as 96 is lower than 100, it should be fine. But maybe Shannon law should be taken into account and 100/2 being lower than 96, the results are expected.

For point 3, well, it could come on top of the two other points, and so I won't rule it out just yet.

I know there is a "Oscilloscope 101" webinar in the works which might actually answer those questions just fine. If that's the case, I'd gladly wait for it.

Thanks for your attention.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes 11 months ago +3
    one thing I did not see being mentioned is about the scope (And probes). Bandwidth of 100Mhz will be 3db down already but the reference for this is a sine wave, not a square wave. A square wave is made…
  • michaelkellett
    michaelkellett 11 months ago +1
    A (very) quick scan of the MAX32666 suggets that they have 4 possible drive current settings for GPIO pins. 1mA drive into a 10pF load will give you a slew rate of 100mV per ns. (and of course…
  • Jan Cumps
    Jan Cumps 11 months ago in reply to obones +1
    The oscilloscope has a 100 Mhz bandwidth. If you probe a 100 MHz square wave signal with it, you 'll notice a few things - even with perfect probing techniques The signal root wave (a 96 MHz sinus…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes 11 months ago

    one thing I did not see being mentioned is about the scope (And probes). Bandwidth of 100Mhz will be 3db down already but the reference for this is a sine wave, not a square wave.

    A square wave is made up of an infinite series of odd-numbered harmonics, including the fundamental frequency. For an ideal square wave, these harmonics are all in phase, with the amplitude of each successive harmonic decreasing by an amount inversely proportional to its harmonic number

    so if the square wave is 96Mhz then you will also have signals of  288Mhz, 480Mhz and that's just 3rd and 5h harmonic there are a lot more to get a good square wave but as the scope is max 100Mhz with 3db down on a sine wave then these harmonics needed to shape the wave form are long gone into oblivion, hence you seeing more and more like a sign wave (Triangle ish in your case). even at the much lower frequencies you will see a distorted square wave due to harmonics being filtered . even a 30Mhz signal will have 3rd and 5th harmonics at or beyond the scopes bandwidth 30Mhz primary, 90Mhz 3rd harmonic and 150Mhz 5th harmonic. I hope this help you understand more of what your seeing.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes 11 months ago

    one thing I did not see being mentioned is about the scope (And probes). Bandwidth of 100Mhz will be 3db down already but the reference for this is a sine wave, not a square wave.

    A square wave is made up of an infinite series of odd-numbered harmonics, including the fundamental frequency. For an ideal square wave, these harmonics are all in phase, with the amplitude of each successive harmonic decreasing by an amount inversely proportional to its harmonic number

    so if the square wave is 96Mhz then you will also have signals of  288Mhz, 480Mhz and that's just 3rd and 5h harmonic there are a lot more to get a good square wave but as the scope is max 100Mhz with 3db down on a sine wave then these harmonics needed to shape the wave form are long gone into oblivion, hence you seeing more and more like a sign wave (Triangle ish in your case). even at the much lower frequencies you will see a distorted square wave due to harmonics being filtered . even a 30Mhz signal will have 3rd and 5th harmonics at or beyond the scopes bandwidth 30Mhz primary, 90Mhz 3rd harmonic and 150Mhz 5th harmonic. I hope this help you understand more of what your seeing.

    • Cancel
    • Vote Up +3 Vote Down