Test & Tools
  • Technologies
  • More
Test & Tools
Forum SMD Diode identification
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 386 subscribers
  • Views 6175 views
  • Users 0 members are here
  • component identification
  • diode
  • smd
  • replacement components
Related

SMD Diode identification

three-phase
three-phase over 8 years ago

In a moment of muppetness, I connected the output of a digital delay line channel to the output of the injection test set I was checking and appeared to have shorted the delay line out, so it doesn't work anymore.

 

I have dismantled it and carried out some measurements around the components and found that a diode (D8) is short circuit. It measures 0.05V in both polarities in and out of circuit, whereas channel B measures 0.58V forward biased and 1.31V reverse biased in circuit. Removing this diode has brought the resistance of the output circuit on channel A back up to the expected 10kOhms, which matches channel B.

 

image

 

Now the tricky part is identifying a replacement diode as it has no markings on it at all. As best as I can measure, the diode is 3.5mm long and 1.3mm in diameter.

 

image

 

I believe the diode is providing some sort of overvoltage protection for the output channel. I had the injection test set set to 5V DC output and presume this is what shorted out the channel. I have traced channel A output circuit below but do not know what the value of C72 is. The resistance values are pretty much the values measured using a DMM.

 

image

Can anyone provide some assistance in identifying a suitable replacement diode?

  • Sign in to reply
  • Cancel

Top Replies

  • jadew
    jadew over 8 years ago +5
    Looks like a clipping diode to me. What you're measuring on channel B indicates a zener, with a breakdown of 1.3 V (which is very uncommon - are you sure that's the whole schematic?). Edit: You should…
  • genebren
    genebren over 8 years ago in reply to jadew +5
    Clipping is possible, but it seems that the voltage divider could account for the voltage drops being seen. Removing the other diode and instrumenting a series of careful tests, might add insight as to…
  • three-phase
    three-phase over 8 years ago in reply to genebren +5
    Many thanks for the assistance. jadew Yes I am quite sure that is all of the output circuit. However, it was a fantastic question because it has made me study the opposite side of the board and I have…
Parents
  • genebren
    genebren over 8 years ago

    Donald,

     

    From your description of your measurement and from your schematic, it would appear to be a simple rectifier.  I would start by trying a 'generic' (standard or general purpose diode) in a SOD80 package and compare it's performance against the other channel.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 8 years ago

    Donald,

     

    From your description of your measurement and from your schematic, it would appear to be a simple rectifier.  I would start by trying a 'generic' (standard or general purpose diode) in a SOD80 package and compare it's performance against the other channel.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +4 Vote Down