Test & Tools
  • Technologies
  • More
Test & Tools
Forum Cool Tools To Giveaway for a Blog Review
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 117 replies
  • Subscribers 403 subscribers
  • Views 18292 views
  • Users 0 members are here
  • scasny
Related

Cool Tools To Giveaway for a Blog Review

rscasny
rscasny over 8 years ago

I kind of figured that anyone who considers him or herself a maker has a toolbox or a bench of tools they treasure. When I did technical work, I had my big tool box and a briefcase of my go-to tools, including a multimeter, driver set, sockets, extender magnet, etc. These were my cool tools. What are yours?

 

We are launching a cool tools campaign at element14 where we roadtest and giveaway some tools we think are pretty cool.

 

Cool Tools Giveaway for a Blog Review

Would you like to get any of these tools, play around with them, and write a blog review? I'm looking for a few members who are really into tools to do the reviews. Below are the tools I have to offer. If you are interested, drop me a line in the comments below. Tell me about your cool tools and persuade me to send you off any of these tools. And all you need to do for it is write a blog review on element14.


image

Milwaukee Tool 60-piece Shockwave Series Impact Driver Set

 

image

Leatherman 14 in 1 Multitool

 

image

Bit Set, Zyklop Mini Series

image

 

Peak Electronics ESR Meter (Capacitance)

 

image

Duratool PC Maintenance Tool Kit

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 8 years ago +16
    I started with 'making'(tearing down) stuff at a tender age and have gone through a lot of stuff. Unfortunately, I lost a big chunk of my tools in a burglary years ago and am left with only a large hammer…
  • jw0752
    jw0752 over 8 years ago +15
    My favorite tools are the ones that I have performed modifications on. When you twist a tool to your own purposes you make a special bond with it. Here are three of the tools which I have modified to do…
  • rsc
    rsc over 8 years ago +13
    This is my favorite tool, circa 1912:
  • 14rhb
    14rhb over 8 years ago in reply to rscasny

    I'd be happy to test that set out for you Randall image

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 8 years ago in reply to rscasny

    Well, I was going to say me, but 14rhb beat me to it image. I own a couple of Wera Kraftform screwdrivers sets (Lasertip and Micro), and the Joker Combination wrenches (metricmetric and imperialimperial), all I can say is, Wera makes fantastic tools.

     

    It's hard for me to say which ones are my most useful tools -I like many of them- but, since we are in an electronics collaboration community, these are my most used ones for my projects in this matter:

    image

    • Engineer PA-14 Wire Stripper: very clean and precise for thin wires.
    • Engineer PA-09 Micro Connector Crimpers
    • Hakko CHP-170 micro cutter: I use them for wires, pins and also to clean 3d-printed parts
    • Tweezers mostly for SMD work and soldering: Hozan P-89 self-closing tweezers, Goot standard precision tweezers TS-10 and Goot eagle-break precision tweezers TS-15
    • Measuring: Mitutoyo 950-300 pocket steel ruleMitutoyo 950-300 pocket steel rule and Mitutoyo 531-128 high accuracy caliper: both have Metric and Imperial graduations
    • OLFA Cushion Grip Knife (AK-4): used mostly for deburring 3d printed parts and custom-made PCBs. Used also for SMD work -to clean/move excess of solder paste-.
    • 1 mL Industrial Syringes with 18G x 1-1/2" Blunt Tip: for SMD work are very good, very little force required, small tip and only need to take just a small amount of solder paste out of the fridge.
    • Tamiya Basic File Set: used for custom-made PCB -yes I use OSH Park- and 3d printed parts.
    • Wera Kraftform Lasertip and Micro screwdrivers

     

    Luis

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Cancel
  • neuromodulator
    neuromodulator over 8 years ago in reply to rscasny

    I could do it... I own a the Wiha 75965 set, which is the same category. Both are quality German brands that come with a screwdriver and ratchet grip with small bits. I got a vernier and microscope I could use to compare them too, here are some photos:

    imageimage

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • snidhi
    snidhi over 8 years ago in reply to neuromodulator

    Hey neuromodulator,

     

    Interesting tools. I am also looking to buy a microscope as well. Can you share a link of the company where you bought it? 

    I am located in Germany. 

     

    Cheers,

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neuromodulator
    neuromodulator over 8 years ago in reply to snidhi

    That's a Wild Heerbrugg M3 stereomicroscope with 3 magnification levels. The company doesn't exist anymore, it was founded by a guy that worked at Zeiss, Wild later merged with Leitz, finally became part of Leica. The M3 is probably 30 or 40 years old, I was lucky to buy for around 170 usd. You will never go wrong with a Leica, but new Leica stereomicroscopes are quite expensive.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14phil
    e14phil over 8 years ago in reply to fvan

    I've lost / had stolen, two Leatherman skeletool with the extended screwdriver sets.

    Really rate them in a pinch.

     

    Phil

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to snidhi

    Hi!

     

    There are also some ideas here:

    Building a Digital PCB Inspection Microscope with the Gizmo 2

     

    There is a photo there from a Meiji microscope, which is often quite cheap when purchased used. I paid about £120GBP. There is a different Meiji one on ebay currently, at £110, although it is in the UK.

     

    That blog post is three years old now, but I still use that microscope regularly. The digital camera connected to Gizmo-2 that is described in that blog post is still used too, but I just connect it to my laptop (the Gizmo-2 single board computer is used elsewhere now). My colleagues found the digital camera useful for component placement. If I could change anything, I'd replace the half-inch posts with 1-inch posts for more stability when fully extended, but they cost more : (

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 8 years ago

    This is my favorite tool, circa 1912:

    image

    • Cancel
    • Vote Up +13 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to rsc

    I'm picking that it is a Mill but with the chuck added for drilling ...

    It will still be going in another 100 years .... well done.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scmclain
    scmclain over 8 years ago in reply to gordonmx

    Gordon,

     

    The last picture, Klein Catapults do have a wire cutter in them. It is the hole in the center of the silver rectangle. It works well, but you have to pass the wire through the hole. This works well for prepping the wire to crimp a lug onto, not so much to cut a wire like with side cutters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>