Test & Tools
  • Technologies
  • More
Test & Tools
Forum Need help with some measurements.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 387 subscribers
  • Views 5588 views
  • Users 0 members are here
  • non_slip_probes
Related

Need help with some measurements.

jw0752
jw0752 over 7 years ago

I need some help collecting data about Oscilloscope Probes. I am thinking of making some low frequency Non-Slip probe tip adapters for Oscilloscope probes. With the limited number of Oscilloscope probes with in my reach it does not look like there is any standardization.

 

image

As you can see the two probes that I own each have different diameter probe tips. It would help me plan my project if I could find out what the diameter and length of oscilloscope probes from as many of you as possible. Please measure length of the consistent diameter of the tip and also the diameter itself. I can accept measurement in inches or millimeters. Here is what I hope to be able to build without having to custom make each one.

 

image

 

Your help would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago in reply to dougw +9
    I have 3 types of probe: pin diameter = PD pin length = PL ground ferule diameter = GD ground ferule length = GL plastic barrel diameter = BD plastic barrel length = BL all dimensions in mm
  • Gough Lui
    Gough Lui over 7 years ago in reply to Gough Lui +7
    jw0752 - I decided to give my improvised method a go - I grabbed a piece of foil and corrugated cardboard, punched the probe tip through the foil into the cardboard and scanned the foil at 4800dpi to judge…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jw0752 +7
    w2aew - a field engineer of Tektronix - has made nice videos on (among other interesting subjects) probing techniques. I use this one at times when direct probing with the pig tail ground is not enough…
Parents
  • Gough Lui
    Gough Lui over 7 years ago

    Thanks for the link image.

     

    I was thinking maybe foil + puncturing holes and then scanning it using my high-resolution scanner might actually not be a bad way to do it given the tools I have. Or maybe removing the probe tip for those that are removable and scanning that directly.

     

    I'll let you know if I turn up any results - got some Picoscope, Rigol, R&S, Vellemann and ''generic" probes here which I regularly use. Have some Keysight at the uni lab.

     

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 7 years ago

    Thanks for the link image.

     

    I was thinking maybe foil + puncturing holes and then scanning it using my high-resolution scanner might actually not be a bad way to do it given the tools I have. Or maybe removing the probe tip for those that are removable and scanning that directly.

     

    I'll let you know if I turn up any results - got some Picoscope, Rigol, R&S, Vellemann and ''generic" probes here which I regularly use. Have some Keysight at the uni lab.

     

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Gough Lui
    Gough Lui over 7 years ago in reply to Gough Lui

    jw0752 - I decided to give my improvised method a go - I grabbed a piece of foil and corrugated cardboard, punched the probe tip through the foil into the cardboard and scanned the foil at 4800dpi to judge the size of the depression as a way to measure the probe tip diameter.

    image

     

    My pin diameters measured out to be (using Photoshop to the nearest 0.1mm):

    R&S - 0.5mm

    Rigol - 0.7mm

    Generic #2 - 0.7mm

    Generic #1 - 0.8mm

    Pico - 0.9mm

    Velleman - 1mm

     

    Of course, I'm not sure how accurate it is, but judging from the R&S RT-ZP10 specs which shows the gold plated spring tip (that I'm using) is 0.5mm, I'd have to say that my measurement mode is likely to be accurate "enough". Sorry, no information on pin length as yet image.

     

    - Gough

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to Gough Lui

    You have awesome ingenuity. Thanks for the effort above and beyond the call of duty.

    John