Test & Tools
  • Technologies
  • More
Test & Tools
Forum Need help with some measurements.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 387 subscribers
  • Views 5574 views
  • Users 0 members are here
  • non_slip_probes
Related

Need help with some measurements.

jw0752
jw0752 over 7 years ago

I need some help collecting data about Oscilloscope Probes. I am thinking of making some low frequency Non-Slip probe tip adapters for Oscilloscope probes. With the limited number of Oscilloscope probes with in my reach it does not look like there is any standardization.

 

image

As you can see the two probes that I own each have different diameter probe tips. It would help me plan my project if I could find out what the diameter and length of oscilloscope probes from as many of you as possible. Please measure length of the consistent diameter of the tip and also the diameter itself. I can accept measurement in inches or millimeters. Here is what I hope to be able to build without having to custom make each one.

 

image

 

Your help would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago in reply to dougw +9
    I have 3 types of probe: pin diameter = PD pin length = PL ground ferule diameter = GD ground ferule length = GL plastic barrel diameter = BD plastic barrel length = BL all dimensions in mm
  • Gough Lui
    Gough Lui over 7 years ago in reply to Gough Lui +7
    jw0752 - I decided to give my improvised method a go - I grabbed a piece of foil and corrugated cardboard, punched the probe tip through the foil into the cardboard and scanned the foil at 4800dpi to judge…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jw0752 +7
    w2aew - a field engineer of Tektronix - has made nice videos on (among other interesting subjects) probing techniques. I use this one at times when direct probing with the pig tail ground is not enough…
  • hlipka
    hlipka over 7 years ago

    I have no permission to see the pictures image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 7 years ago

    Hi John, I cannot see it either...  Frank

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to fmilburn

    Thanks Frank and hlipka  for the heads up. It was strange as I did the picture insertion as always and the pictures showed on the computer that I made the post with but my computer in the office was just like you said "No Pictures". I have edited the post and re loaded the pictures and now I see them on both of my computers. Let me know if you still have a problem on your end.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to jw0752

    I see the pictures.

    Cool idea.

    It might be worth making the sleeve come up onto the plastic barrel. The most common problem I have with probes is when they get dropped, or if the pin is in a socket when the cable gets yanked, the exposed pin can get snapped off.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 7 years ago

    I can see the pics now.

     

    Siglent 1102 CML: 0.045” diameter, .0160” length (base to point)

    Rigol DS1054Z: 0.0375” diameter, 0.185” length

     

    The Siglent has a short base with step in it.  The base is 0.098” diameter and quite short. The length given above is from the where .045” starts to the tip (excludes base).

     

    The metal barrels are 0.189 and 0.185”. The plastic parts have a slight taper and differ between the two.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi John,

     

    I'll measure up several later today, and post the results.

    Also, have you considered making the entire 'scope probe? There could perhaps be interest in that.. I'd be interested : )

    There is a brief comment mentioned in 'Art of Electronics' where the profs just use co-ax cable (RG178 in their case) and attach a 953 ohm resistor in series on the end, and it becomes the probe. This then is a X20 probe (and it expects the 'scope end to be set to 50 ohms, or use a T-piece and a 50 ohm terminator for 'scopes that don't have that built-in. This would be good for up to 100-200MHz perhaps, covering many use-cases.. It is mentioned here, in a yellow box:

    https://electronics.stackexchange.com/questions/351368/high-speed-passive-probe-contradiction-between-authors-or-differe…

    Trouble is, a resistor is too flimsy for general probing. Maybe it would be nice to have a complete probe with the co-ax, resistor, and your probe attached.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to dougw

    I have 3 types of probe:

    pin diameter = PD

    pin length = PL

    ground ferule diameter = GD

    ground ferule length = GL

    plastic barrel diameter = BD

    plastic barrel length = BL

    all dimensions in mm

     

    image

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to fmilburn

    Thanks Frank, That is exactly what I am looking for.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to dougw

    Thanks Douglas,

     

    I appreciate your organization and categorization as well. Thanks for taking the time to get the measurements for me.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    I haven't considered it as I felt that there needed to be physical tuning that I wasn't capable of. My partner in the Non-Slip probe adventure Neil asked me today about making Oscilloscope probes and so I thought that perhaps I could make adapter tips for probes that would not be a problem at lower frequencies. That is what got this inquiry started. I have gotten so spoiled using the meter non-slip probes that every time I use my oscilloscope probe I get real frustrated with keeping the probe point where I want it. Since I am pretty much a low frequency tech I decided to make a set of adapter tips for my scopes. When I found the probes had different diameter pins I suspected that there wasn't  a standard size like there is for the meter probes. Now I am collecting data just to see how bad the dis-uniformity really is.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
>