Test & Tools
  • Technologies
  • More
Test & Tools
Forum Can an ESD mat be tested without special tools?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 385 subscribers
  • Views 9529 views
  • Users 0 members are here
Related

Can an ESD mat be tested without special tools?

baldengineer
baldengineer over 7 years ago

There are inexpensive continuity testers that let you verify a loop between you, your wrist strap, and ground.

 

Without investing into special weights (probes), is there an effective way to measure an ESD mat’s resistance? Or more simply, verify areas of an ESD mat are still effective?

 

Can it be done with “just” a multimeter and a power supply?

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 7 years ago +6
    I've tried it with the two kinds of mat I have. This is with 10V from a bench PSU and my 5.5 digit Fluke meter (I also put a 100 ohm resistor in series, in case I touched the probes together, though I…
  • rsc
    rsc over 7 years ago +6
    ANSI / ESD S4.1-2006 Test Procedure According to ANSI / ESD S20.20-2014, an acceptable work surface will have a point to point and a point to groundable point resistance of less than 1.0 x 10^9 ohms. ANSI…
  • Gough Lui
    Gough Lui over 7 years ago +5
    I suspect some meters which cam measure in the tens of megohms can probably produce a reading on some carbon impregnated rubber mats. Then again there are other with a lot higher resistance rubber - I…
Parents
  • jc2048
    jc2048 over 7 years ago

    I've tried it with the two kinds of mat I have. This is with 10V from a bench PSU and my 5.5 digit Fluke meter (I also put a 100 ohm resistor in series, in case I touched the probes together, though I  realised after that I could have just used the current limit on the PSU).

     

    Cheap, black, rubbery mat.

     

    a reading over a distance of 10mm of around 8uA

     

    Old, blue, 'Farnell' branded mat

     

    maybe something like 3nA (this is right down near the limits of what this particular meter will read)

     

    Neither is really a resistance. There isn't too much variation with distance.

     

    On a cheap handheld meter, the black one reads about half a megaohm. The probes are more pointed and dig into the surface a bit which is probably why it's less than the 10V/8u reading would suggest (1.25M).

    The professional blue one is over-range.

     

    The 3nA figure for the Farnell mat sort of suggests a rough equivalent resistance of 3.33  G ohms but it could be quite a bit different to that (the meter reads 2nA with the probes in mid air and the reading goes up to 5nA on the mat, so I'm not all that confident in it).

     

    Edited because somehow I stupidly wrote Tera rather than Giga.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 7 years ago

    I've tried it with the two kinds of mat I have. This is with 10V from a bench PSU and my 5.5 digit Fluke meter (I also put a 100 ohm resistor in series, in case I touched the probes together, though I  realised after that I could have just used the current limit on the PSU).

     

    Cheap, black, rubbery mat.

     

    a reading over a distance of 10mm of around 8uA

     

    Old, blue, 'Farnell' branded mat

     

    maybe something like 3nA (this is right down near the limits of what this particular meter will read)

     

    Neither is really a resistance. There isn't too much variation with distance.

     

    On a cheap handheld meter, the black one reads about half a megaohm. The probes are more pointed and dig into the surface a bit which is probably why it's less than the 10V/8u reading would suggest (1.25M).

    The professional blue one is over-range.

     

    The 3nA figure for the Farnell mat sort of suggests a rough equivalent resistance of 3.33  G ohms but it could be quite a bit different to that (the meter reads 2nA with the probes in mid air and the reading goes up to 5nA on the mat, so I'm not all that confident in it).

     

    Edited because somehow I stupidly wrote Tera rather than Giga.

    • Cancel
    • Vote Up +6 Vote Down