Wireless
  • Technologies
  • More
Wireless
Blog In Search of a Good HD Radio
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 20 Jul 2013 8:20 PM Date Created
  • Views 995 views
  • Likes 0 likes
  • Comments 4 comments
  • hd_radio
Related
Recommended

In Search of a Good HD Radio

gervasi
gervasi
20 Jul 2013

image

After having decent results testing my first HD Radio, I bought a JVC KT-HDP1 HD Radio receiver to test AM HD Radio.  The performance was disappointing.

 

The connectors were unusual sizes, except for the headphone output.  None of the connectors I found on Digikey fit. 

 

The antenna out port is for retransmitting the received signal in analog FM on the frequency of your choice. 

 

The unit pulls 0.3A at 12V, around 4W.  The current draw is about the same regardless of whether the radio is tuned to an HD station and whether the re-transmit feature is enabled. 

 

Inside the unit there is a user interface board and a receiver board.  The receiver board has a metal can that appears to function as a shield and heatsink.  The can is attached by screws, no solder.  It gets hot to the touch after a few minutes.  I suspect most of that heat comes from the TI DSP. 

 

We soldered a two-meter wire to the RX antenna port.  The radio picked up no stations on AM and only the analog portion of FM stations.  The digital subcarrier is 20dB down from the the FM, so HD radio only works with strong stations. 

 

We soldered another two-meter wire to the TX antenna port.  A trace going to the TX port also goes to a matching network connected to a metal antenna, perhaps making the external TX antenna optional.  With a wire on the TX port, the radio began receiving many more stations, including some HD signals.  It’s unclear why a wire on the TX port improved receive reception.  It was still nowhere near as good as the Insignia radio we tested first. 

 

image

The user interface was very frustrating.  I couldn’t find any way to go to a frequency other than searching.  If the signal doesn’t exceed the fixed threshold when the radio gets to that frequency, it just passes by. 

 

Surprisingly, the re-transmit feature worked well.  The Insignia radio picked up the analog signal transmitted from the JVC radio from across the room.

 

I feel so disappointed in this radio because it should be good. 

  • It’s a rare receiver that supports AM HD.
  • It has a real receive antenna port, not some crude piece of wire.
  • The transmit feature allows you to use it anywhere there’s an FM receiver. 

 

This could have been something you could use in a car, with a stereo, or with an antenna on the roof for DXing.  This radio obviously isn’t even close to that caliber.  Someone should design a nice high performance radio that does HD and is good enough for DXing.  CCrane says the discontinued Sony HDRF1HD is the only thing that comes close, and then only for FM.  If someone makes a product or a kit for a high-performance HD radio, I’ll be eager to try it. 

image

  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    HD Radio is a scam!

     

    http://hdradiofarce.blogspot.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gervasi
    gervasi over 13 years ago in reply to e14 Contributor

    @Greg

    Thanks for joining the site.  I checked out the website critical of HD.  I agree with some of the criticism there.  Why do you say, though, that it's a scam.  Do you think it's just a bad standard or do you think there's actually some wrongdoing where someone is profiting by promoting a flawed digital radio standard?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sqkybeaver
    sqkybeaver over 13 years ago in reply to gervasi

    someone is obviously profiting from adoption of the standard, if the standard is not as good as what it is to replace

     

    if it quacks it must be a duck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sqkybeaver
    sqkybeaver over 13 years ago in reply to gervasi

    someone is obviously profiting from adoption of the standard, if the standard is not as good as what it is to replace

     

    if it quacks it must be a duck