Wireless
  • Technologies
  • More
Wireless
Forum MDO4014-3 Spectrum Analyzer Scope-Porn Noise
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 218 subscribers
  • Views 973 views
  • Users 0 members are here
Related

MDO4014-3 Spectrum Analyzer Scope-Porn Noise

gervasi
gervasi over 13 years ago

Tektronix let me borrow one of their mixed-mode scopes that has a spectrum analyzer and a full-featured scope in the same box. It's cool because you can watch one domain and trigger of the other.  You can watch them at the same time and stop them both to look at the frequency domain during a time-domain event.  Very cool.

 

I'm getting this weird noise on the spectrum analzyer side.  It is a set of two large symmetric peaks centered around 2.5GHz.

image

 

The signal presists even when I terminate the input with a 50 ohm dummy load.  I have another spectrum analyzer and have confirmed there's no noise in the area. 

 

I'm guessing I'm doing something wrong because this is a new scope. 

  • Sign in to reply
  • Cancel
Parents
  • sqkybeaver
    sqkybeaver over 13 years ago

    I have seen this too,(bolth mdo4104-6 and mdo4014-3) all though not as bad. the sample clock of 2.5Ghz presents a small ~10dB average peak

     

    have you compensated signal path?

     

    if not, after compensating signal path, is it still there?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gervasi
    gervasi over 13 years ago in reply to sqkybeaver

    What do you mean by compensating for the signal path?  I thought the SA just shows you the magnitude of power present at the input port.  I termiated it with a 50 ohm load and expected to see just the noise floor.  Instead the peaks persist. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sqkybeaver
    sqkybeaver over 13 years ago in reply to gervasi

    image

    remove RF input, and run compensation. also try pushing "default setup" to remove any other settings

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gervasi
    gervasi over 13 years ago in reply to sqkybeaver

    I had tried reset-to-defaults.  Running Compensation fixed the problem. image   Thanks!!

     

    I left it in the car in the garage last night.  It was about 0F outside last night, so maybe the cold affected it.  It's non-operating range is down to -80F, so it shouldn't have damaged it.  But maybe it caused it to need to be compensated.  Thanks again. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gervasi
    gervasi over 13 years ago in reply to sqkybeaver

    I had tried reset-to-defaults.  Running Compensation fixed the problem. image   Thanks!!

     

    I left it in the car in the garage last night.  It was about 0F outside last night, so maybe the cold affected it.  It's non-operating range is down to -80F, so it shouldn't have damaged it.  But maybe it caused it to need to be compensated.  Thanks again. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • sqkybeaver
    sqkybeaver over 13 years ago in reply to gervasi

    Your welcome, I often run the compensation as my "lab" is not temperature controlled and as noisy as could be.

    The noise floor should be better than -60dBm @ 0dBm ref, also fairly close to linear.