1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Blog# 8.1 (Part 1 of 2) EAS - System Build
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
  • Author Author: skruglewicz
  • Date Created: 26 Dec 2020 4:05 PM Date Created
  • Views 885 views
  • Likes 4 likes
  • Comments 1 comment
  • mentioned in my mongo db will be used to store the data . what i have decided to implement i
Related
Recommended

Blog# 8.1 (Part 1 of 2) EAS - System Build

skruglewicz
skruglewicz
26 Dec 2020

image

BLOG# 8.1 -Edible Algae System - (Growing Spirulina in space)

System Build

This is Part 1 of my 8th blog post in a series of blog post for the Design Challenge 1 Meter of Pi

version 1.1

,<<< PREVIOUS BLOG

NEXT BLOG  >>>

Blog# 7 System Designs -- Software Design

Blog# 8.2 (Part 2 of 2) EAS - DATA REPOSITORY MongoDB

 

INTRODUCTION

Ok, here we are on the 9th of December the year 2020. I'm on the home stretch.

 

As of today, the Challenge Page Dates states, that the Challenge Projects are due on the "5th January. 2020.". I know that we did lose the year 2020 because of a global covid-19 pandemic. This was kind of surreal when I checked on the finish line date. I'm assuming you meant to say the year 2021.

Updated Just checked the date has now been changed to 2021

 

"5th January. 2020.", That is lest than 4 weeks away, time to get cranking on the implementation of my design..

Updated  Now 10 days away as of this blogs first publish to the Design Challenge.

 

  • This blog will describe the implementation of my system design from my previous Blog# 7 EAS -  System Designs -- Software Design
  • I divided up the build process into two build phases.
    • Part 1, describes the devices attached and controlled by the Rasberry PI.,
    • Part 2, decribes the classes developed to implement the management of the attached devices.
  • List Additional Material needed for the project showing links to sourced.

  • Electronics Build
    • Enviro Hat and Automation Mini Hat
    • Water temp Sensor
    • Devices attached to the Automation Mini Hat
  • Software Build
    • Class Diagram
    • CODE
      • Sensors (senors.py)
        • Base class
        • Child classes that inheret from Sensors:
          • Light
          • WaterTemp
          • RoomHumidity
          • RoomTemp
      • Controller (controllers.py)
        • BASE Class Controllers
        • Child Classes that inheret from Controller
          • LEDLight
          • WaterPump
          • WaterHeaterPad
          • RoomHeater
          • IntakeFan
          • OutTakeFan
      • Alerts (alerts.py)
        • BASE Class
        • Child Classes that inheret from Alerts
          • RoomHumidityAlert
          • WaterTempAlert
          • RoomTempAlert
          • LightAlert
          • Timers
      • Timers (timer.py)
        • BASE Class
        • Child Classes that inheret from Timers
          • Generic Timer
          • LightTimer45
          • LightTimer15
          • WaterpumpTimer
        • BASE Class
        • Database  PUT methods:
          • PutSensor
          • PutController
          • PutAlert
          • PutTimer
  • REFERENCES

Electronics Build

The Electronic Build section will describe the Wireing for the connections of the 2 hats, water temp sensor  and the devices attached to the Automation Mini Hat

  • Enviro Hat and Automation Mini Hat

    are wired to the rasberry using the wireing scheme
    • I was somewhat disappointed that I could not stack the Hat's using the Pico Hat Hacker,but happy to find that another challenger, dules had a solution in one of his blogs Aquaponics Box: #2 - Hacking the HATs (both HATs from the challenger kit on single RPi)
    • I was able to get both HATs working, using the wiring diagram and his PIN analyst contained in this blog.
    • Thanks dules
    • The only wiring I did different is that I used GPIO 13 for the Enviro display backlight.
    • image
  • Water temp Sensor

    • This sensor is attached to the breadboard off the rasberry pi as described in my Blog# 5 EAS - Research Temperature Sensor - DS18B20
  • Devices attached to the Automation Mini Hat

    • LEDLight

      • Automation Hat output1

    • WaterPump
      • Automation Hat output2
    • WaterHeaterPad
      • Automation Hat output3
    • RoomHeater
      • not Implemented YET
    • IntakeFan
      • Automation Hat relay NO
    • OutTakeFan
      • Automation Hat relay NC

 

Additional Devices needed for the project

IItemNOTES
Glass Container

I bought this at my local store. Not 20 gallons, but It will surfice for now

Heating Unit

 

Used to Heat the water to grow Algae. The glass container will be placed on this

 

Icstation 5V 1W Flexible Polyimide Heater Plate Adhesive PI Heating Film 30mmx40mm (Pack of 4)
Icstation 5V 1W Flexible...View product details
Air Pump

 

Used to Airerate the water to grow Algea

 

hygger Mini Aquarium Air Pump Kit Small Fish Tank Air Pump 1W for 1-20 Gallon Fish Bowl with Air Tube Air Bubbler Stone Check Valve (1W)
hygger Mini Aquarium Air Pump Kit...View product details
Lamp LED

HAVE

 

This needs to be 12Volt

Room heater

TO Purchase

The problem is the power draw of a heater. Is there a heater on the maket that uses 12 Volts.'

Intake and OutTake

Fans

Purchased 2 small ones with 2 leads

 

MakerFocus 2pcs Raspberry Pi DC Brushless Cooling Fan Heatsink Cooler Radiator Connector Separating One-to-Two Interface 3.3V 5V for Raspberry Pi 2/ Pi 3/3B+ and Pi Zero/Zero W or Other Robot Project
MakerFocus 2pcs Raspberry Pi DC...View product details

 

 

 

 

Software Build

The Software Build will contain sections on the python code used to implement each class from the from the class diagram described in Blog#7

For this build, I developed 6 Python scripts that implement the classes described in my Design Challenge Blog# 7 EAS -  System Designs -- Software Design

Each of the following sections contain the classes code..

Class Diagram

 

image

CODE

Sensors (senors.py)

Base class

 

# --Sensors
# This module will contain all communication with the sensors on the Enviro Hat
# and on a seperate sensor the W1ThemSensor

# BASE CLASS
classSensors:
     def__init__(self,type):
          self.value = 0
          self.type = type
          iftype != 2 :
               self.device = "Enviro"
          else:
               self.device = "W1ThemSensor"
          self.description = "Sensor"

Child classes that inheret from Sensors:

Light

class Light(Sensors):
    def __init__(self,type=1):
        super().__init__(type)


    def getValue(self):
    # gets the value of the sensor    
        import logging
        import time


        try:
            # Transitional fix for breaking change in LTR559
            from ltr559 import LTR559
            ltr559 = LTR559()
        except ImportError:
            import ltr559


        logging.basicConfig(
            format='%(asctime)s.%(msecs)03d %(levelname)-8s %(message)s',
            level=logging.INFO,
            datefmt='%Y-%m-%d %H:%M:%S')


        #sleep for a moment
        time.sleep(1)


        self.value = ltr559.get_lux()
        
        logging.info("""Light: {:05.02f}""".format(self.value))
        return self.value


    def IsInRange(self):
        pass

WaterTemp

class WaterTemp(Sensors):
    def __init__(self,type=2):
        super().__init__(type)
    def getValue(self):
    # gets the value of the water Tempreture sensor    
        import logging
        from w1thermsensor import W1ThermSensor

        logging.basicConfig(
            format='%(asctime)s.%(msecs)03d %(levelname)-8s %(message)s',
            level=logging.INFO,
            datefmt='%Y-%m-%d %H:%M:%S')

        sensor = W1ThermSensor()
        temperature_in_celsius = sensor.get_temperature()
        temperature_in_fahrenheit = sensor.get_temperature(sensor.DEGREES_F)
        #temperature_in_fahrenheit = sensor.get_temperature(2)

        self.value = temperature_in_fahrenheit 
        
        logging.info("""Water Tempreture: {:05.02f}C  {:05.02f}F""".format(temperature_in_celsius,temperature_in_fahrenheit))
        return self.value

    def IsInRange(self):
        pass

 

RoomHumidity

class Humidity(Sensors):
    def __init__(self,type=3):
        super().__init__(type)
        
    def getValue(self):
    # gets the value of the sensor    
        import logging
        from bme280 import BME280
        # BME280 temperature/pressure/humidity sensor
        bme280 = BME280()


        logging.basicConfig(
            format='%(asctime)s.%(msecs)03d %(levelname)-8s %(message)s',
            level=logging.INFO,
            datefmt='%Y-%m-%d %H:%M:%S')


        self.value = bme280.get_humidity()
        
        logging.info("""Room Humitity: {:05.02f}%""".format(self.value))
        return self.value


    def IsInRange(self):
        pass

 

RoomTemp

 

class RoomTemp(Sensors):
    def __init__(self,type=4):
        super().__init__(type)

    def getValue(self):
        from bme280 import BME280

        try:
            from smbus2 import SMBus
        except ImportError:
            from smbus import SMBus

        import logging
        logging.basicConfig(
            format='%(asctime)s.%(msecs)03d %(levelname)-8s %(message)s',
            level=logging.INFO,
            datefmt='%Y-%m-%d %H:%M:%S')

        bus = SMBus(1)
        bme280 = BME280(i2c_dev=bus)

        # Get the temperature of the CPU for compensation
        def get_cpu_temperature():
            with open("/sys/class/thermal/thermal_zone0/temp", "r") as f:
                temp = f.read()
                temp = int(temp) / 1000.0
            return temp

        # Tuning factor for compensation. Decrease this number to adjust the
        # temperature down, and increase to adjust up
        factor = 2.25
        factor = 18
        cpu_temps = [get_cpu_temperature()] * 5
        cpu_temp = get_cpu_temperature()
        # Smooth out with some averaging to decrease jitter
        cpu_temps = cpu_temps[1:] + [cpu_temp]
        avg_cpu_temp = sum(cpu_temps) / float(len(cpu_temps))
        raw_temp = bme280.get_temperature()
        comp_temp = raw_temp - ((avg_cpu_temp - raw_temp) / factor)

        # Conversion to F (0°C × 9/5) + 32 
        temp_f = (comp_temp * 9/5) + 32

        logging.info("Room Temperature: {:05.2f}C  {:05.2f}F".format(comp_temp,temp_f))

        self.value = temp_f         
        return self.value

    def IsInRange(self):
        pass

 

Controller (controllers.py)

 

BASE Class Controllers

 

# Controllers
# this module will contain all communication with the Automation HAT Mini

#set up logging
import logging
logging.basicConfig(
    format='%(asctime)s.%(msecs)03d %(levelname)-8s %(message)s',
    level=logging.INFO,
            datefmt='%Y-%m-%d %H:%M:%S')


# BASE CLASS
class Controllers:
    def __init__(self,type):
        self.value = "OFF"        # "OFF"   "ON"
        self.type = type          # 1 -- light      # 2 -- WaterPump    # 3 -- WaterHeater
                                  # 4 -- RoomHeater # 5 -- IntakeFan    # 6 -- OutTakeFan
        self.channel = "NONE"     # ADC     INPUT   OUTPUT  RELAY
        self.chanNum = 0          # 1,2,3   1,2,3   1,2,3   -1=NO 0=COM 1=NC 
        self.IsOn = False

import automationhat #use the automation hat module


Child Classes that inheret from Controller

 

LEDLight

 

# 1 -- Light    Growing LAMP
class Light(Controllers):
    def __init__(self,type=1):
        super().__init__(type)
        self.channel = "OUTPUT"   # ADC     INPUT   OUTPUT  RELAY
        self.chanNum = 1          # 1,2,3   1,2,3   1,2,3   -1=NO 0=COM 1=NC 
        self.IsOn = False

    def Set(self,value):
        logging.info("""START Light.Set({:})""".format(value))
        self.value = value
        #check value 
        if (value == "ON"):
            automationhat.output.one.on()
        else:
            automationhat.output.one.off()

    def Get(self):
        return self.value

    def IsOnCheck(self):
        #check value
        if automationhat.output.one.is_on():
            return True
        else:
            return False

 

WaterPump

 

# 2 -- WaterPump
class WaterPump(Controllers):
    def __init__(self,type=2):
        super().__init__(type)
        self.channel = "OUTPUT"   # ADC     INPUT   OUTPUT  RELAY
        self.chanNum = 2          # 1,2,3   1,2,3   1,2,3   -1=NO 0=COM 1=NC 
        #ERROR IN2 is not working !!! WHY?????
        self.IsOn = False

    def Set(self,value):
        logging.info("""START WaterPump.Set({:})""".format(value))
        self.value = value
        #check value 
        if (value == "ON"):
            automationhat.output.two.on()
        else:
            automationhat.output.two.off()

    def Get(self):
        return self.value

    def IsOnCheck(self):
        #check value
        if automationhat.output.two.is_on():
            return True
        else:
            return False

 

WaterHeaterPad

 

# 3 -- WaterHeater
class WaterHeater(Controllers):
    def __init__(self,type=3):
        super().__init__(type)
        self.channel = "OUTPUT"   # ADC     INPUT   OUTPUT  RELAY
        self.chanNum = 3          # 1,2,3   1,2,3   1,2,3   -1=NO 0=COM 1=NC 
        self.IsOn = False

    def Set(self,value):
        logging.info("""START WaterHeater.Set({:})""".format(value))
        self.value = value
        #check value 
        if (value == "ON"):
            automationhat.output.three.on()
        else:
            automationhat.output.three.off()

    def Get(self):
        return self.value

    def IsOnCheck(self):
        #check value
        if automationhat.output.three.is_on():
            return True
        else:
            return False

 

RoomHeater

# 4 -- RoomHeater     - NOT IMPLEMENTED YET
class RoomHeater(Controllers):
    pass

IntakeFan

# 5 -- IntakeFan      - NOT IMPLEMENTED YET
class IntakeFan(Controllers):
    pass

OutTakeFan

# 6 -- OutTakeFan     - NOT IMPLEMENTED YET
class OutTakeFan(Controllers):
    pass

 

 

Alerts (alerts.py)

BASE Class

# Alert class
# this module contains the alert class used to
# - save alert message to the data repository 
# - sending message in an email to the system Admin
# - logging message to stderr

#######Child classes that inherit from base class: Sensors
#type -- Nane
# 1 -- RoomHumidityAlert
# 2 -- WaterTempAlert
# 3 -- LightAlert
# 4 -- RommTempAlert
# 5 -- other     - NOT IMPLEMENTED YET

#set up logging
# Logging Levels
# The numeric values of logging levels are given in the following table. 
# These are primarily of interest if you want to define your own levels, 
# and need them to have specific values relative to the predefined levels. 
# If you define a level with the same numeric value, it overwrites the predefined value; 
# the predefined name is lost.
# Level Numeric value
# CRITICAL 50
# ERROR     40
# WARNING     30
# INFO     20
# DEBUG     10
# NOTSET    0
import logging
logging.basicConfig(
    format='%(asctime)s.%(msecs)03d %(levelname)-8s %(message)s',
    level=logging.NOTSET,
    datefmt='%Y-%m-%d %H:%M:%S')

# BASE CLASS Alerts
class Alerts:
    def __init__(self,type):
        self.type = type
        self.message = "none"
        #Valud Values NOTSET, DEBUG, INFO, WARNING,ERROR, CRITICAL
        self.severity = logging.NOTSET  

# sendEmail to be implemented
import email
def sendEmail(message):
    pass

Child Classes that inheret from Alerts

RoomHumidityAlert

import db
# 1 -- RoomHumidityAlert
class RoomHumidityAlert(Alerts):
    def __init__(self,type=1):
        super().__init__(type)

    def send(self,message):
        self.message = message
        self.severity = logging.WARNING

        sendEmail(message)

        logging.warning("""ALERT-WARNING: RoomHumidity({:})""".format(message))

        database=db.Db()
        database.putAlert(self.type, self.message,self.severity)

WaterTempAlert

 

# 2 -- WaterTempAlert
class WaterTempAlert(Alerts):
    def __init__(self,type=2):
        super().__init__(type)

    def send(self,message):
        self.message = message
        self.severity = logging.CRITICAL

        sendEmail(message)

        logging.warning("""ALERT-CRITICAL: WaterTemp({:})""".format(message))

        database=db.Db()
        database.putAlert(self.type, self.message,self.severity)

RoomTempAlert

# 4 -- RommTempAlert
class RommTempAlert(Alerts):
    def __init__(self,type=4):
        super().__init__(type)


    def send(self,message):
        self.message = message
        self.severity = logging.WARNING


        sendEmail(message)


        logging.warning("""ALERT-WARNING: RommTemp({:})""".format(message))


        database=db.Db()
        database.putAlert(self.type, self.message,self.severity)

 

LightAlert

# 3 -- LightAlert
class LightAlert(Alerts):
    def __init__(self,type=3):
        super().__init__(type)

    def send(self,message):
        self.message = message
        self.severity = logging.CRITICAL

        sendEmail(message)

        logging.warning("""ALERT-CRITICAL: Light({:})""".format(message))

        database=db.Db()
        database.putAlert(self.type, self.message,self.severity)

 

Timers

# 5 -- OTHER - Critical
class OtherAlert(Alerts):
    def __init__(self,type=5):
        super().__init__(type)


    def send(self,message):
        self.message = message
        self.severity = logging.CRITICAL


        sendEmail(message)


        logging.warning("""ALERT-CRITICAL: OTHER({:})""".format(message))


        database=db.Db()
        database.putAlert(self.type, self.message,self.severity)

 

Timers (timer.py)

BASE Class

#Timer Class
#sets a timer

#set up logging
import logging
logging.basicConfig(
    format='%(asctime)s.%(msecs)03d %(levelname)-8s %(message)s',
    level=logging.INFO,
            datefmt='%Y-%m-%d %H:%M:%S')

#######Child classes that inherit from base class: Timers
#type -- Nane
# 1 -- GenericTImer
# 2 -- WaterPumpTImer
# 3 -- LightTimer45
# 4 -- LightTimer15

#BASE Class
class Timers(object):
    def __init__(self,type):
        self.status=""
        self.type = type
import time
def countdown(t):
    while t:
        mins,secs=divmod(t,60)
        status = " STATUS:{:02d}:{:02d}".format(mins,secs)
        print(status ,end="\r")
        time.sleep(1)
        t-=1

Child Classes that inheret from Timers

 

Generic Timer

import db

#1 generic timer
class timer(Timers):
    def __init__(self,type=1):
        super().__init__(type)

    def Set(self,value):
        mins,secs=divmod(value,60) 
        status = "Start Timer for: {:02d}:{:02d}".format(mins,secs)      
        database=db.Db()
        database.putTimer(self.type,status)
        logging.info(status)
        countdown(value)
        logging.info("DONE Timer: ")

 

LightTimer45

# 3 -- LightTimer45
class LightTimer45(Timers):
    def __init__(self,type=3):
        super().__init__(type)

    def Set(self):
        value = 60 * 45 # set timer for 46 miinutes
        mins,secs=divmod(value,60) 
        status = "Start Timer for: {:02d}:{:02d}".format(mins,secs)      
        database=db.Db()
        database.putTimer(self.type,status)
        logging.info(status)
        countdown(value)
        logging.info("DONE Timer: ")

LightTimer15

# 4 -- LightTimer15
class LightTimer15(Timers):
    def __init__(self,type=4):
        super().__init__(type)

    def Set(self):
        value = 60 * 15 # set timer for 15 miinutes
        mins,secs=divmod(value,60) 
        status = "Start Timer for: {:02d}:{:02d}".format(mins,secs)      
        database=db.Db()
        database.putTimer(self.type,status)
        logging.info(status)
        countdown(value)
        logging.info("DONE Timer: ")

 

WaterpumpTimer

# 2 -- WaterPumpTimer
class WaterPumpTimer(Timers):
    def __init__(self,type=2):
        super().__init__(type)

    def Set(self):
        value = 60 #set timer to 1 minute
        mins,secs=divmod(value,60) 
        status = "Start Timer for: {:02d}:{:02d}".format(mins,secs)      
        database=db.Db()
        database.putTimer(self.type,status)
        logging.info(status)
        countdown(value)
        logging.info("DONE Timer: ")

 

DATA (db.py)

BASE Class

# Data Repository Class
# Connect to MongoDB Atlas in the cloud.
# use the eas database to store telemetry data
from pymongo import MongoClient
import datetime

class Db(object):
    def __init__(self):
        uri = "<YOUR CONNECTION STRING HERE>"
        client = MongoClient(uri)
        self.db = client.eas

 

Database  PUT methods:

PutSensor

    def putSensor(self,type,value):
        timestamp = datetime.datetime.now()
        data = { "type" : type,"value": value, "timestamp":timestamp }

        # 1 - light
        # 2 - waterTemp
        # 3 - humidity
        # 4 - roomTemp

        if type  == 1:
            self.db.light.insert_one(data)
        if type  == 2:
            self.db.waterTemp.insert_one(data)
        if type  == 3:
            self.db.humidity.insert_one(data)
        if type  == 4:
            self.db.roomTemp.insert_one(data)      

 

PutController

def putController(self,type,value):
        timestamp = datetime.datetime.now()
        data = { "type" : type,"value": value, "timestamp":timestamp }

        #type -- Nane
        # 1 -- LedLight
        # 2 -- WaterPump
        # 3 -- WaterHeater
        # 4 -- RoomHeater     - NOT IMPLEMENTED YET
        # 5 -- IntakeFan      - NOT IMPLEMENTED YET
        # 6 -- OutTakeFan     - NOT IMPLEMENTED YET

        if type  == 1:
            self.db.LedLight.insert_one(data)
        if type  == 2:
            self.db.WaterPump.insert_one(data)
        if type  == 3:
            self.db.WaterHeater.insert_one(data)
        if type  == 4:
            self.db.RoomHeater.insert_one(data)  
        if type  == 5:
            self.db.IntakeFan.insert_one(data) 
        if type  == 6:
            self.db.OutTakeFan.insert_one(data)

 

PutAlert

    def putAlert(self,type,message,severity):
        timestamp = datetime.datetime.now()
        data = { "type":type,"severityLevel":severity,"message":message,"timestamp":timestamp }
        self.db.Alerts.insert_one(data)

 

PutTimer

    def putTimer(self,type,status):
        timestamp = datetime.datetime.now()
        data = { "type":type,"status":status,"timestamp":timestamp }
        self.db.Timers.insert_one(data)


Conclusion and summary

  • Ths blog documents the classes that I wrote to implement my design diagram from my Blog# 7 EAS -  System Designs -- Software Design
  • It includes all the code to be used by the python scripts to be produced and featured in a later blog post.
  • Unit test of each module, will be featured in a future blog post.
  • I started using Microsoft Visual Code, which I was pleased to find, ran the same as on Windows. I had a few problems getting familier to the Python environment (I use C# on the PC), but all in all it was a plesent experience
  • Part 1 and 2 of this blog post took a lot of my time to complete, but I was able to get most of the connections in my design implemented. I spent a lot of time researching and experimenting with the new technologies.
  • I am farlly new to Python programming and I needed  to get up to speed with Object Oriented Programming in the language. I'll need to do some refactoring, but in order to reach the challenge deadline , I'm going to plow ahead.
  • I will still need to implement the email fuction in alerts, I just didn't have the time.
  • The mongoDB  database section started to get to long, so I decided to include it  in another blog. I had a lot of fun with it, and it will help with analysing the data generated during the growing cycle.
  • Be sure to take a look at the next blog. The DATA class uses mongoDB and it will show how flexible this tool is to store data.
  • Now onto testing the classes.

 

 

 

 

REFERENCES

Mongo Atlashttps://www.mongodb.com/cloud/atlas/lp/day-zero?tck=brand-campaign-page
Mongo Coursehttps://university.mongodb.com/mercury/M220P/2019_May/overview
Mongo Documentationhttps://docs.mongodb.com/
Mongo client APIhttp://api.mongodb.com/python/current/api/pymongo/mongo_client.html

 

,<<< PREVIOUS BLOG

NEXT BLOG  >>>

Blog# 7 System Designs -- Software Design

Blog# 8.2 (Part 2 of 2) EAS - DATA REPOSITORY MongoDB
  • Sign in to reply
  • DAB
    DAB over 5 years ago

    Nice detailed update.

     

    DAB