• Products and Partners
    Products and Partners
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
Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Stirling Blue - Power Measurement - Blog 7 (updated)
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
  • Author Author: dougw
  • Date Created: 11 Jun 2018 3:41 AM Date Created
  • Views 2917 views
  • Likes 14 likes
  • Comments 11 comments
  • stirling blue
  • doug wong
  • bluetooth unleashed
  • stirling engine
  • bluetooth unleashed design challenge
Related
Recommended

Stirling Blue - Power Measurement - Blog 7 (updated)

dougw
dougw
11 Jun 2018

In this blog I am trying to figure out if the Stirling engine generates enough power to run the electronic data acquisition system based on a PSoC6.

First I am going to measure how much current and voltage the PSoC6 requires. Then I am going to measure how much current and voltage the Stirling engine generates.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Finally, I am going to measure the engine speed:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The motor-generator set puts out about a quarter Watt, which is easily enough to run a low power microcontroller, but for now I will keep it simple and power the electronics separately.

 

Update - Temperature Measurement:

I added a temperature measurement adventure with the Stirling engine...

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Upcoming blogs:

  • how Stirling engines work
  • start connecting some sensors to the PSoC6
  • designing the sensor interface PCB
  • the micro:bit keyboard

 

Related Links:

Bluetooth Unleashed Design Challenge

Bluetooth Unleashed Design Challenge: The Challengers

Bluetooth Unleashed Design Challenge: About This Challenge

 

Links to other blogs for this project:

Stirling Blue - Project Description - Blog 1

Stirling Blue - Unboxing Hero - Blog 2

StirlingBlue1

Stirling Blue - micro:bit TXTR - Blog 3

Stirling Blue - Fuel Measurement - Blog 4

FuelMeasurement1

Stirling Blue - Interface Description - Blog 5

Stirling Blue - BBC micro:bit LCD - Blog 6

microbitLCD1

  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 8 years ago +5
    Very cool! I love how that little thing hums along! Where did you get the sterling engine? ps, your video popped up as a suggestion on my tv earlier today, so I knew there'd be an e14 blog post to go along…
  • dougw
    dougw over 8 years ago in reply to ntewinkel +4
    That is a pretty cool lantern. It has been a while since I dropped in to Lee Valley Tools - time for another visit. The engine is from ebay - I liked the workmanship on this model.
  • jw0752
    jw0752 over 8 years ago +3
    Hi Doug, Very nice demonstration. What was the source of the strobe effect on the connecting rods. I am guessing you are under florescent light. John
Parents
  • BigG
    BigG over 8 years ago

    Hi Doug,

     

    Very nice demo on the power (open voltage & load).

     

    Regarding PSoC 6. There is a switch (SW5), which gives you 3 power options. Top - 1.8V, Middle - 3.3V and Bottom is variable between 1.8 & 3.3V. So the MCU should be quite happy with the variable setting. The EPD shield requires a 3V input (vin & 5V are NC). So you would need some sort of power regulation for that. Also, the USB-C charge controller (CYPD3125-40LQXIT) min-max voltage range is 2.7V to 5.5V. So, you are just reaching min voltage under load.

     

    G://

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • BigG
    BigG over 8 years ago

    Hi Doug,

     

    Very nice demo on the power (open voltage & load).

     

    Regarding PSoC 6. There is a switch (SW5), which gives you 3 power options. Top - 1.8V, Middle - 3.3V and Bottom is variable between 1.8 & 3.3V. So the MCU should be quite happy with the variable setting. The EPD shield requires a 3V input (vin & 5V are NC). So you would need some sort of power regulation for that. Also, the USB-C charge controller (CYPD3125-40LQXIT) min-max voltage range is 2.7V to 5.5V. So, you are just reaching min voltage under load.

     

    G://

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 8 years ago in reply to BigG

    Thanks for the info. I will look at low power modes after I get everything working.