Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Stirling Blue - PSoC Bluetooth Terminal Keyboard - Blog 9
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
  • Author Author: dougw
  • Date Created: 27 Jun 2018 4:01 AM Date Created
  • Views 1453 views
  • Likes 11 likes
  • Comments 5 comments
  • stirling blue
  • doug wong
  • qwerty keyboard
  • psoc 4
  • bluetooth unleashed
  • bluetooth unleashed design challenge
Related
Recommended

Stirling Blue - PSoC Bluetooth Terminal Keyboard - Blog 9

dougw
dougw
27 Jun 2018

I have to go away for a few days to play in a golf tournament with my Dad, but I wanted to get a blog out before I go. This blog is a continuation of the PSoC Bluetooth terminal sub-project. This section is just a quick demonstration of the PSoC scanning the keyboard and displaying the characters on an LCD:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I have to say soldering dozens of switches is not a thrill of a lifetime, but doing it without a PCB would be a real nightmare.

So far this PCB is working as designed, and the software is working well. All the tactile switches are nicely debounced.

Progress is always gratifying, but there is a lot left to do.

 

Upcoming blogs:

  • the micro:bit keyboard
  • how Stirling engines work
  • start connecting some sensors to the PSoC6
  • designing the sensor interface PCB

 

Related Links:

Bluetooth Unleashed Design Challenge

Bluetooth Unleashed Design Challenge: The Challengers

Bluetooth Unleashed Design Challenge: About This Challenge

 

Links to other blogs for this project:

Stirling Blue - Project Description - Blog 1

Stirling Blue - Unboxing Hero - Blog 2

StirlingBlue1

Stirling Blue - micro:bit TXTR - Blog 3

Stirling Blue - Fuel Measurement - Blog 4

FuelMeasurement1

Stirling Blue - Interface Description - Blog 5

Stirling Blue - BBC micro:bit LCD - Blog 6

microbitLCD1

Stirling Blue - Power Measurement - Blog 7 (updated)

PowerMeasurement1

SpeedMeasurement1

Stirling Blue - Bluetooth Terminal Awakening - Blog 8

BluetoothTerminalAwake1

  • Sign in to reply

Top Comments

  • dougw
    dougw over 8 years ago in reply to DAB +3
    I had lots of design constraints that I didn't do a good job of documenting: I want to make the micro:bit into a communications device (a texting terminal) that would allow students to use them in a communal…
  • dougw
    dougw over 8 years ago in reply to genebren +3
    genebren your prolofic comments across the forum are always positive, always encouraging and I'm sure they are always much appreciated. Thanks from all of us.
  • DAB
    DAB over 8 years ago +2
    Nice update Douglas. I am curious, why did you not just use a regular keyboard? DAB
Parents
  • DAB
    DAB over 8 years ago

    Nice update Douglas.

     

    I am curious, why did you not just use a regular keyboard?

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 8 years ago in reply to DAB

    I had lots of design constraints that I didn't do a good job of documenting:

    I want to make the micro:bit into a communications device (a texting  terminal) that would allow students to use them in a communal paradigm instead of just a solitary learning tool. My vision is a pocket texting device.

    • It must be low cost.
    • It must interface to a micro:bit. This means I2C, SPI, UART or BLE. I2C is entangled by the sensors on micro:bit and UART is uncharted territory.(read undocumented). BLE is costly if it is even available, and it takes the solution out of the pocket device category. That leaves SPI. I couldn't find any commercial keyboards with an SPI interface.
    • The micro:bit solution needs to be small and mobile and self-contained - a complete communications terminal. A normal keyboard is too big.

    I also had a motive to make a general purpose QWERTY terminal for use in low cost microcontroller applications. This solution has a UART, SPI and Bluetooth interfaces and it costs about $1 for the PCB, $4 for the PSoC4, and about 90 cents for all 60 tactile switches - total about $6. The displays add $2.83 each. I did quite a bit of work to try and make a capacitive keyboard, but the extra size of the PCB for capacitive switches (= extra cost) was unattractive and the larger PCB cost more than the tactile switches.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago in reply to dougw

    Doug,

     

    Thanks for sharing your design constraints.  I love the idea of a micro:bit enabled communications device.  Also the idea that this part can be modified and re-deployed is a great idea.  This is sort of the hardware version of the 'design for reuse' concept that was supposed to make C++ so powerful.  A great idea, that so few people have been able to master.  It takes a lot of upfront work in order to make a good re-usable item and it seems like you have done your homework here.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 8 years ago in reply to genebren

    genebren your prolofic comments across the forum are always positive, always encouraging and I'm sure they are always much appreciated. Thanks from all of us.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 8 years ago in reply to genebren

    genebren your prolofic comments across the forum are always positive, always encouraging and I'm sure they are always much appreciated. Thanks from all of us.

    • Cancel
    • Vote Up +3 Vote Down