Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog Open Source EMDR Machine #4. Breadboard layout and Schematics
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ilvyanyatka
  • Date Created: 18 Apr 2021 7:29 PM Date Created
  • Views 3083 views
  • Likes 8 likes
  • Comments 10 comments
  • health care
  • breadboard
  • open source emdr machine
  • design for a cause - design challenge
  • schematic
  • medical
  • arduino nano 33 iot
  • design_for_a_cause_2021
Related
Recommended

Open Source EMDR Machine #4. Breadboard layout and Schematics

ilvyanyatka
ilvyanyatka
18 Apr 2021

Open Source EMDR Machine. The Whole Blog.

 

So there is some bad news. I started working with my Arduino Nano 33 IoT board and tried to implement the Bluetooth communication part first. And I successfully burned (fried?) my board. Not sure why exactly but it died when I was uploading/running for the first time my sketch with Bluetooth code. Previous simple version with just lights and without Bluetooth communication was working fine.

 

While I am waiting for a new one, I will continue working on my old Arduino UNO, postponing Bluetooth implementation and just connecting all hardware parts and making sure they work. I also have to supplement DFPlayer for Piezo disks. I will see how it works out and most likely get back to using the DFPlayer module after I get my new Arduino Nano 33 IoT board.



Here are the images of my Fritzing breadboard layout and Schematics. For some reason I cannot attach the full Fritzing file to this post. When I make this project public on GitHub I will add a link to the Fritzing file itself. Both use Arduino UNO as it is preliminary design, when I am done testing it, I will make a new layout and schematic using Arduino Nano 33 IoT.

 

 

Breadboard layout:

 

image

 

 

 

 

Schematic:

 

image

  • Sign in to reply

Top Comments

  • javagoza
    javagoza over 5 years ago in reply to ilvyanyatka +3
    Hi, Victoria, Press the reset button on the board twice before loading the new binary. The two LEDs on the board will illuminate, indicating that it is in boot load mode. It will change the serial connection…
  • cjodrey
    cjodrey over 5 years ago +2
    Nice schematics!
  • fmilburn
    fmilburn over 5 years ago +2
    Are you having a problem with the DFPlayer? I used it successfully on a recent project so just curious but perhaps could help if you ran into an issue.
Parents
  • javagoza
    javagoza over 5 years ago

    Victoria, I'm sorry about your Arduino Nano 33 IoT.

     

    When you say you've burned the board, what do you mean? What are the symptoms?

     

    Have you taken into account in your design that the Arduino nano 33 IoT does not tolerate 5v? The Arduino NANO 33 IoT microcontroller runs at 3.3V, which means you should never apply more than 3.3V to your digital and analog pins.

     

    It must have care to connect the sensors and actuators to ensure that this limit never exceeds 3.3V.

     

    Connecting higher voltage signals, such as the 5V commonly used with the other Arduino boards, will damage the Arduino NANO 33 IoT.

     

    Also note that the maximum current per pin is 7 mA compared to 40 mA on other Arduino boards.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 5 years ago

    Victoria, I'm sorry about your Arduino Nano 33 IoT.

     

    When you say you've burned the board, what do you mean? What are the symptoms?

     

    Have you taken into account in your design that the Arduino nano 33 IoT does not tolerate 5v? The Arduino NANO 33 IoT microcontroller runs at 3.3V, which means you should never apply more than 3.3V to your digital and analog pins.

     

    It must have care to connect the sensors and actuators to ensure that this limit never exceeds 3.3V.

     

    Connecting higher voltage signals, such as the 5V commonly used with the other Arduino boards, will damage the Arduino NANO 33 IoT.

     

    Also note that the maximum current per pin is 7 mA compared to 40 mA on other Arduino boards.