Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog Open Source EMDR Machine #4. Breadboard layout and Schematics
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ilvyanyatka
  • Date Created: 18 Apr 2021 7:29 PM Date Created
  • Views 3075 views
  • Likes 8 likes
  • Comments 10 comments
  • health care
  • breadboard
  • open source emdr machine
  • design for a cause - design challenge
  • schematic
  • medical
  • arduino nano 33 iot
  • design_for_a_cause_2021
Related
Recommended

Open Source EMDR Machine #4. Breadboard layout and Schematics

ilvyanyatka
ilvyanyatka
18 Apr 2021

Open Source EMDR Machine. The Whole Blog.

 

So there is some bad news. I started working with my Arduino Nano 33 IoT board and tried to implement the Bluetooth communication part first. And I successfully burned (fried?) my board. Not sure why exactly but it died when I was uploading/running for the first time my sketch with Bluetooth code. Previous simple version with just lights and without Bluetooth communication was working fine.

 

While I am waiting for a new one, I will continue working on my old Arduino UNO, postponing Bluetooth implementation and just connecting all hardware parts and making sure they work. I also have to supplement DFPlayer for Piezo disks. I will see how it works out and most likely get back to using the DFPlayer module after I get my new Arduino Nano 33 IoT board.



Here are the images of my Fritzing breadboard layout and Schematics. For some reason I cannot attach the full Fritzing file to this post. When I make this project public on GitHub I will add a link to the Fritzing file itself. Both use Arduino UNO as it is preliminary design, when I am done testing it, I will make a new layout and schematic using Arduino Nano 33 IoT.

 

 

Breadboard layout:

 

image

 

 

 

 

Schematic:

 

image

  • Sign in to reply

Top Comments

  • javagoza
    javagoza over 5 years ago in reply to ilvyanyatka +3
    Hi, Victoria, Press the reset button on the board twice before loading the new binary. The two LEDs on the board will illuminate, indicating that it is in boot load mode. It will change the serial connection…
  • cjodrey
    cjodrey over 5 years ago +2
    Nice schematics!
  • fmilburn
    fmilburn over 5 years ago +2
    Are you having a problem with the DFPlayer? I used it successfully on a recent project so just curious but perhaps could help if you ran into an issue.
  • fmilburn
    fmilburn over 5 years ago

    The one I am using is called the DFPlayer Mini, a link can be found here: https://wiki.dfrobot.com/DFPlayer_Mini_SKU_DFR0299

     

    An identical, or near identical version is sold by others and I got mine on Amazon.  It can be used in stereo or mono modes.  I'm using mine mono on an Arduino MKR1010 and using hardware serial but software serial should work.  The schematic for my project is in this post: make robot friend. Bender | element14 | Cheer Us Up

     

    To use mono (like I did) wire it up between what is marked SPK1 and SPK2 on my schematic.  For stereo use two speakers and hook them between SPK1 and GND, and SPK2 and GND.

     

    I am happy to help further if I can and good luck on your project image

     

    edit: for some reason the link to DF Robot doesn't seem to work.  But do a google search for DFPlayer Mini and you will find it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ilvyanyatka
    ilvyanyatka over 5 years ago in reply to cjodrey

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ilvyanyatka
    ilvyanyatka over 5 years ago in reply to fmilburn

    I didn't read the specs and got DFPlayer (as I can see now it is mono, correct?) instead of DFPlayer Pro. (Stereo, which I need). So I will need 2 DFPlayers, and from what I understand on Arduino Uno I can add only one and access it thru Software serial.

    On Arduino Nano, again, as I understand, I can add both and play "left ear" and "right ear" sounds sequentially.

    Do I understand it all correctly?

    So I will switch to DFPlayer when I get my new Nano board, but for now, just to be able to code my sound logic I will use piezo disks.

     

    Thank you so much for your offer. It is highly likely i will have issues, so I will ask you for help!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago

    Are you having a problem with the DFPlayer?  I used it successfully on a recent project so just curious but perhaps could help if you ran into an issue.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cjodrey
    cjodrey over 5 years ago

    Nice schematics!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<