Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog Smart Exhibit: Blog #4: Electronic schematic, system building and sanity checks
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: alexandru.cohal
  • Date Created: 9 Apr 2021 9:16 PM Date Created
  • Views 1065 views
  • Likes 4 likes
  • Comments 4 comments
  • sanity check
  • smart exhibit
  • system building
  • schematic
  • design for a cause
Related
Recommended

Smart Exhibit: Blog #4: Electronic schematic, system building and sanity checks

alexandru.cohal
alexandru.cohal
9 Apr 2021

Hello!

 

As explained in my previous blog post ( Smart Exhibit: Blog #3: The hardware components ), I need some extra components (temperature, humidity, light, sound and motion sensors, speaker, push-button, battery and battery charger) for my project, Smart Exhibit. Last week I received these components together with the Arduino Nano 33 IoT board image So, I started playing with them and this is the summary of what I did:

  • I tested the functionality of all these components together with the Arduino Nano 33 IoT board
  • I designed the electronic schematic of my system using Fritzing. I pushed this schematic to my repository (https://github.com/alexandru-cohal/SmartExhibit). Below you can see it.


image

  • I implemented for each component a Sanity Check short program. I know from my previous projects that it is always useful to have such programs for testing different functionalities with each component in particular and also to verify that the respective component is actually working fine (for the moments when I am in doubt that something might have happened with the component or with the connection between the component and the board image)
  • I connected all the components and the Arduino board together using a breadboard (I spent some time with my obsession of very clean and neat wirings but in the end it worth the effort image). Below you can see some photos of how the system looks. Pretty good, right? imageimage

image

image

image

  • I implemented a Sanity Check program for the whole system (the Arduino board + all the components). Again, this is for checking that all the components are working when connected together with the board at the same time and all the connections are fine (Rule number 1: There are never enough tests and checks image)
  • I pushed all the Sanity Checks programs to my repository (https://github.com/alexandru-cohal/SmartExhibit)
  • I kept my Trello board updated (https://trello.com/b/qwcDuQMy/smartexhibit).

 

I had a lot of fun playing with all the components and the Arduino Nano 33 IoT board but I am pretty sure that this is only the beginning image

  • Sign in to reply

Top Comments

  • alexandru.cohal
    alexandru.cohal over 5 years ago in reply to javagoza +2
    Hi! I was also a bit skeptical in the beginning if this will work or not. But until now, based on the tests I did, I didn't notice any problems (e.g. slowness, glitchy analogue pins) when I power the Arduino…
  • javagoza
    javagoza over 5 years ago +1
    Hi, I am curious. You're powering the board with only 3.7 volts. The MPM3610 Step Down Converter specifications indicate an input range between 4.5V and 21V. Have you noticed any problems in your tests…
  • alexandru.cohal
    alexandru.cohal over 5 years ago in reply to makervanlabs +1
    Thank you I will tell you the secret of how I managed to make the breadboard to look like this I used the wires from a general breadboard jumper wire set (like this one, for example) but I cut them in…
Parents
  • javagoza
    javagoza over 5 years ago

    Hi,

    I am curious. You're powering the board with only 3.7 volts. The MPM3610 Step Down Converter specifications indicate an input range between 4.5V and 21V. Have you noticed any problems in your tests?

     

    image

    image

    Arduino nano 33 IoT Schematics:

     

    https://content.arduino.cc/assets/NANO33IoTV2.0_sch.pdf

     

    MPM3610 Step Down Converter Datasheet

     

    https://www.monolithicpower.com/en/documentview/productdocument/index/version/2/document_type/Datasheet/lang/en/sku/MPM3…

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alexandru.cohal
    alexandru.cohal over 5 years ago in reply to javagoza

    Hi!

     

    I was also a bit skeptical in the beginning if this will work or not. But until now, based on the tests I did, I didn't notice any problems (e.g. slowness, glitchy analogue pins) when I power the Arduino Nano 33 IoT board with a LiPo 3.7V battery.

     

    Though, the battery's nominal voltage is 3.7 V, but when it is fully charged it reaches 4.2 V. Based on the MPM3610's datasheet, the range between 4.5V and 21V is the recommended input, so I guess it is not a strict limitation but a limitation for guaranteeing the functionality. These 2 aspects also count.

     

    I will do more tests with the whole range of the battery's voltage and I will see if I will notice some problems. I will also write here what will be the results image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • alexandru.cohal
    alexandru.cohal over 5 years ago in reply to javagoza

    Hi!

     

    I was also a bit skeptical in the beginning if this will work or not. But until now, based on the tests I did, I didn't notice any problems (e.g. slowness, glitchy analogue pins) when I power the Arduino Nano 33 IoT board with a LiPo 3.7V battery.

     

    Though, the battery's nominal voltage is 3.7 V, but when it is fully charged it reaches 4.2 V. Based on the MPM3610's datasheet, the range between 4.5V and 21V is the recommended input, so I guess it is not a strict limitation but a limitation for guaranteeing the functionality. These 2 aspects also count.

     

    I will do more tests with the whole range of the battery's voltage and I will see if I will notice some problems. I will also write here what will be the results image