Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The Genie's Day Brightens
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
  • Author Author: RParkerE
  • Date Created: 22 May 2015 9:12 PM Date Created
  • Views 2738 views
  • Likes 4 likes
  • Comments 14 comments
  • enchanted_objects
  • mini_automator
Related
Recommended

The Genie's Day Brightens

RParkerE
RParkerE
22 May 2015

The week was full of rain and clouds for the poor genie all week. Unable to leave his house and make any progress on the things that needed to get done, due to the unfortunate consequences of doing your electrical work in the rain, but today the sun peeked out from behind the clouds and shone with the brightness of 2000-2500 lumen. It was magnificent! However, shortly after its arrival, the clouds took over again . But while the sun was out the genie made headway on his electrical wiring of his sweet new crib. He set the power supply to roughly thirty volts and tested out his lights to see if they worked.

                                                                       imageimage

And it worked! How excited the genie was! This was a huge step in the right direction with the build of his new pad. Now all that was needed to be done was wire it all up to his sweet new dimmer and you could call him Xzibit Jr.

                                                                                                      image

WAIT! There is no light!!!! What in the world is going on? No explosions, check. No fire or smoke, check. Then what? The genie checked the voltage coming out and the light intensity and found:

                                                                  imageimage

But that doesn’t make sense! 30 Volts in and only a 100th of that out? How could this be? The genie has yet to figure this out, but he will be working diligently over the weekend to figure out a solution!

                                                                                   

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to Jan Cumps +3
    Jan Cumps You wouldn't be the first or last to miss something in a post ... You raised a very good pint about the meter though. I wonder if someone who has a working LED can do some checking using a simple…
  • RParkerE
    RParkerE over 11 years ago in reply to mcb1 +3
    I found the culprit and it was much simpler than assumed. I had a poor connection, after I soldered the pins it worked perfectly fine. I am working on my next update now
  • Jan Cumps
    Jan Cumps over 11 years ago +2
    The week was full of rain and clouds for the poor genie all week. Unable to leave his house and make any progress on the things that needed to get done, We seem to have the opposite way of working . I…
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    I just checked the current with my multimeter. The libraries are all very similar, here's a comparison http://www.element14.com/community/docs/DOC-73603/l/compare-the-infineon-rgb-libraries-that-spawned-from-the-internet-of-holiday-lights

     

    I wonder if the circuit is going into shut down due to too much current? The power LEDs normally have a voltage drop of 6v, so perhaps a couple of power diodes in series with the lamp?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago

    I just checked the current with my multimeter. The libraries are all very similar, here's a comparison http://www.element14.com/community/docs/DOC-73603/l/compare-the-infineon-rgb-libraries-that-spawned-from-the-internet-of-holiday-lights

     

    I wonder if the circuit is going into shut down due to too much current? The power LEDs normally have a voltage drop of 6v, so perhaps a couple of power diodes in series with the lamp?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed

    The power LEDs normally have a voltage drop of 6v

    The large 30w devices I have are 32v (if you get the right spec) and since there are 10 individual elements you can see, I imagine they are 3.2v across each element.

    Different colours do tend to have different forward drop voltages, and 3.2v is within the range I expect for a high power LED.

     

    Do these '6v' device have two elements to them.?

     

    Personally I'd be stringing some cheap LEDs together even if you need to do two or three strings.

    The other option is a resistor, and it is amazing what water cooling can do for a high power load.

     

    Mark