Experimenting with Extreme Environments
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Extreme Environments
  • More
  • Cancel
Experimenting with Extreme Environments
Blog PicoPorch Motor Controller
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Extreme Environments to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 27 May 2024 2:22 AM Date Created
  • Views 523 views
  • Likes 9 likes
  • Comments 0 comments
  • dougw
  • PicoPorch
  • Midas MC42005A6W-SPTLYI-V2
  • Experimenting with Extreme Environments
  • Hammond Manufacturing
  • motor controller
Related
Recommended

PicoPorch Motor Controller

dougw
dougw
27 May 2024

Intro

I finally assembled the PicoPorch motor controller. This blog shows it in operation using manual switches to control motor direction and limit switches to prevent over rotation in either direction.

Motor Controller CCA

image

You can see 2 places where I substituted SOT23 transistors for larger transistors. Fortunately this motor does not require high current.

Schematic

image

This bi-directional DC motor controller features a shoot-through protected H-bridge with directional limit switches. For an explanation of its operation see the video below. I wanted to perform both the shoot-through protection and limit switch functions in hardware for maximum safety.

Motor Controller Video Demo

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

It is nice to get the motor controller working. Even though one of the transistors did not arrive, I was able to substitute some I had in stock. They are lower power devices, but this motor only draws 15 mA so power is not an issue.

This demo means that both custom PCBs are functional, which is a key milestone in the project.

There is still some mechanical design to get the limit switches to activate at the correct positions and the stands to mount all the apparatus need to be designed and built. Although it is still a significant amount of work, the remaining work mostly involves mechanical tinkering and assembly rather than risky design.

There is also some firmware to be developed, but a fully functional system should be fairly straightforward. I might add some complexity as a stretch goal, if there is time.

Next up:

  • Build more cables 
  • Program the Pico to control the motor
  • Wire up the system and test it.
  • Design and build the motor controller case mounting stand
  • Design and build the limit switch mounts and triggers
  • Design and build  the rain guard for the motor mechanism
  • Test he system in the wild (extreme environment)
  • Make more videos and blogs

Links:

  • Garden Secrets System
  • ComputeCam and PicoPorch - Early Muddling
  • PicoPorch and ComputeCam - The Motor System
  • PicoPorch - LCD PCB & Bezel
  • PicoPorch power wiring
  • PicoPorch Motor Controller Demo
  • PicoPorch System Demo
  • PicoPorch Final Touches
  • Deep Dive On Kit Components
  • Backyard Secrets 1
  • MotionEyeOS Tutorial
  • Garden Secrets Project Summary
  • Experimenting with Extreme Environments Design Challenge
  • Pi 4 Compute Module Datasheet
  • Pi 4 Compute Module I/O Board Datasheet
  • Midas Display Datasheet
  • Enclosure Drawing
  • Enclosure Manufacturer Page
  • Antenna Datasheet
  • Connectors Datasheet