Experimenting with Supercapacitors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Supercapacitors
  • More
  • Cancel
Experimenting with Supercapacitors
Blog SuperCap Meter Shield Functional Test
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Supercapacitors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 5 Sep 2023 1:20 AM Date Created
  • Views 1361 views
  • Likes 7 likes
  • Comments 2 comments
  • dougw
  • SuperCap Magic Meter
  • supercap meter shield
  • experimenting with supercapacitors
Related
Recommended

SuperCap Meter Shield Functional Test

dougw
dougw
5 Sep 2023

image

Intro

This installment on my Super Capacitor Experimentation Project covers functional testing of the supercapacitor meter shield. The last blog covered assembly of the PCB. This blog shows the shield is able to charge and discharge with constant current under MCU control. The software for this installment does not implement the full capacitance meter function, it is aimed at proving all of the circuitry is fully functional and properly connected to the MCU. The test software also allows the circuitry to be calibrated.

Operational Description

The shield has 6 functions, selected by the rotary switch, these functions are displayed, but not fully implemented:

  1. Voltage Mode - displays capacitor-under-test voltage, used to monitor leakage
  2. LiC Mode - used to measure capacitance of Lithium Capacitors
  3. EDLC Mode - used to measure capacitance of EDL Capacitors
  4. ESR Mode - used to measure equivalent series resistance of capacitors
  5. Charge Mode - supplies constant charging current to the capacitor-under-test
  6. Discharge Mode - extracts constant discharging current from the capacitor-under-test

The functional test software can charge and discharge at constant current rates while monitoring capacitor voltage.

image

Functional Test Software Demo

The following video shows the shield and test software in action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

The functional test is successful - all circuitry is working. The resistors and voltages have been calibrated and the currents are reasonably accurate - checked by measuring resistance and voltage at the shunt to calculate current. (Using a 4 digit DVM)

I discovered (the hard way) that the I2C pins are connected to 2 of the analog input pins, which means there are only 3 usable analog inputs. I am pretty disappointed about that situation, although I can get by with 3 analog inputs for this project by doing more manual calibration.

The functional test is the biggest hurdle in the project, so it is great to get past this stage.

Next Steps

Next I will design a case for the capacitance meter to make it look like a real meter and of course I have to finish programing the meter functions.

Links

The Magic of SuperCaps 

 SuperCap Magic Meter Circuit 

 The SuperCap Rack 

 The SuperCap Magic Meter Shield 

 SuperCap Meter Shield Functional Test 

 SuperCap Magic Meter - Operational 

 SuperCap Magic Meter - Experimenting with Supercapacitors 

Experimenting with Supercapacitors Design Challenge

Cornell Dubilier Supercapacitor Technical Guide

Cornell Dubilier Supercapacitor Handling Guidelines

Challengers

Leaderboard

  • Sign in to reply
  • dang74
    dang74 over 3 years ago

    I like that you support an ESR test.  The general assumption is that ceramic capacitors have a small ESR.  Unfortunately, ESR is rarely ever reported in their datasheets.  Every once in a while you will encounter regulators that impose an ESR range on their output capacitors.  When you consider using a multilayer ceramic for this application you are kind of operating blind as far as ESR is concerned.... so yeah I like that your project measures ESR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 3 years ago

    Very good update Douglas.