Experimenting with Thermal Switches
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermal Switches
  • More
  • Cancel
Experimenting with Thermal Switches
Challenge Blog Blog #3: LED Life Booster/Extender
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • RoadTests
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: karthikrajagopal
  • Date Created: 27 Mar 2022 3:01 PM Date Created
  • Views 2350 views
  • Likes 9 likes
  • Comments 6 comments
  • thermal switch
  • kemet
  • reed switches
  • experimenting with Thermal Switches
Related
Recommended

Blog #3: LED Life Booster/Extender

karthikrajagopal
karthikrajagopal
27 Mar 2022

The block diagram:

The plan explained in the first blog was to use 4 thermal switches for more controlled and reliable sensing. The experimental setup uses 2 thermal switches instead of 4, since the outcome is the same.image

Developing the logic:

There are 4 possible combinations that can be achieved using the 2 thermal switches TS1 and TS2. The decision based on these 4 combinations would be meaningless since the current state transitions of TS1 and TS2 are independent of each other. Hence, the previous state of the switches is also to be considered to ensure smoother transition between various levels of brightness.

image

image

Arduino code:

#include <elapsedMillis.h>
elapsedMillis timer;
elapsedMillis timer1;
elapsedMillis timer2;
elapsedMillis timer3;
#define ledPin1 3    
#define ledPin2 9
#define thermal1 4
#define thermal2 5
byte y=255;
bool from10=0;
bool from11=0;
bool from01=0;
byte dly=5000; // state transition time
byte stand=20;

void setup() 
{
pinMode(4,INPUT);
pinMode(5,INPUT);
pinMode(ledPin1,OUTPUT);
pinMode(ledPin2,OUTPUT);
}

void loop() 
{
  
    if(digitalRead(thermal1)== 0 && digitalRead(thermal2)== 0)
    { delay(10);
      if(digitalRead(thermal1)== 0 && digitalRead(thermal2)== 0)   
    {if( (from10 == 1 || from11 == 1) && y!=255)
      {analogWrite(ledPin1,y);
       analogWrite(ledPin2,255-y);
        if(timer>= dly)
        {y++;timer=0;}
       
      }
      else if(from01==1 && y!=255)
      {analogWrite(ledPin1,y);
       analogWrite(ledPin2,255-y);
       if(timer>=dly)
       {y--;timer=-0;}
       
      }
      else
      {from10 =0;from11=0; from01=0;
      analogWrite(ledPin1,255);
      analogWrite(ledPin2,0);
      
      }
      timer2=0;
    }
    }
//*************************************************************************************
    else if(digitalRead(thermal1)== 1 && digitalRead(thermal2)== 0)
    {delay(10);
     if(digitalRead(thermal1)== 1 && digitalRead(thermal2)== 0)
       {if(timer2>dly)
        {analogWrite(ledPin1,y);
        analogWrite(ledPin2,255-y);
        if(timer>=dly && y!=stand)
        {y--; timer=0;}         
        from10=1;
        from01=0;
        from11=0;
      }
      timer3=0;
      }
    }
//*************************************************************************************
   else if(digitalRead(thermal1)== 0 && digitalRead(thermal2)== 1)
    {delay(10);
     if(digitalRead(thermal1)== 0 && digitalRead(thermal2)== 1)
        {if(timer1>dly)
          {analogWrite(ledPin1,y);
          analogWrite(ledPin2,255-y);
          if(timer>= dly  && (255-y)!=stand)
          {y++; timer=0;}        
          from01 = 1;
          from11=0;
          from10=0;
          }
          timer2=0;
          timer3=0;
        }
    }
//*************************************************************************************
    else if(digitalRead(thermal1)==1 && digitalRead(thermal2)==1)
    { delay(10);
      if(digitalRead(thermal1)==1 && digitalRead(thermal2)==1)
        {if(timer3>dly)
        { if(from10==1 && y!=125)
          {analogWrite(ledPin1,y);
           analogWrite(ledPin2,255-y);
           if(timer>dly)
           {y++;timer=0;}
           
     
          }
          else if(from01==1 && y!=125)
          {analogWrite(ledPin1,y);
           analogWrite(ledPin2,255-y);
           if(timer>dly)
           {y--;timer=0;}
           
          }
          else
          {from10=0; from01 = 0;
          analogWrite(ledPin1,125);
          analogWrite(ledPin1,125);
          }
         from11 = 1;
         timer2=0;
        }
        }
    }
}

Different states of brightness:

image

The picture1(top left corner) shows the initial brightness level. After entering the subsequent states of the logic, it returns back to the initial state only if both the thermal switches go below the 40°C mark.

The reason for maintaining  a 40-100% brightness level after crossing the initial state is to reduce the thermal expansion and contraction effects on the LED filaments (as mentioned by Gough Lui in my blog1 comment). This aspect is also taken care of by the software where the brightness level changes gradually depending on the set timer value.

  A 0-100% brightness level and a 40-100% / 100-40% brightness level both have the same light output with only subtle difference, which when used in a larger space would have negligible impact.

Mounting the Thermal Switch:

The OHD1-50B type KEMET thermal switch was mounted on to the backside of the heatsink. The switches were accurate and the cutoff temperature recorded was around 49°C.

image

image

The final output:

The circuit installation was done on the workbench and the change in light intensity was recorded. A video clip focusing the light bulbs is included along with a video of a user-perspective view of the light intensity change over the workbench. The transition time of the LEDs had to be reduced to 200ms and further the video had to be played at 2x speed for the light intensity change to be noticeable. So, it is understood that, on normal circumstances, the change in light intensity is unnoticeable.

In the video, the light intensity change can be observed by noticing the difference in the shadow cast by the wire at various instances of the clipping.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Conclusion:

KEMET Thermal switches are useful for a variety of switching applications. They are accurate and a long-lasting solution as they have reduced metal fatigue due to no metal expansion. However, the downside could be the power rating. While their bimetallic counter parts have higher ratings, these reed switches have a maximum power rating of 75W, which in most cases can be a bit less  considering a direct series connection with the device’s mains input.

<Blog #2

  • Sign in to reply

Top Comments

  • karthikrajagopal
    karthikrajagopal over 4 years ago in reply to navadeepganeshu +1
    Thanks navadeepganesh! Yes, I have applied thermal paste on the back side of the heatsink. I have included the picture of it in 'Mounting the Thermal Switch' section.
  • karthikrajagopal
    karthikrajagopal over 4 years ago in reply to Gough Lui

    Yes, I directly had the thermal switch mounted on the backside of the panel. Initially tried with the top heatsink plate the LED bulb had, but the testing took too long to produce result as it was exposed to cool air and had a better air cooling than it was in the enclosure. 

    For the switch mounting, I did the bare minimum to hold the switch in place while also ensuring proper thermal conductivity. It could have been improvised by having proper mounting brackets. Thought of such a construction but didn't get the needed materials on time. Maybe I can update it once I get the mechanical parts.

    Thanks for letting me know the error in the 1st diagram, have corrected and updated now.

    In the brightness logic, having a 40-40 makes sense.. In view of maintaining the balance between light output and a cooler temperature, I went with 50-50. 

    Thanks for the observations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago

    Hmm. It seems your LED panels have been mounted to the thermal switch and not to any real heatsink which sort of defeats the purpose of maximising the LED's lifetime. In such a scenario, I would expect the LEDs to run much hotter than they absolutely have to - the zip-tie may not last all that long either and then if the thermal switch falls off the LED MCPCB, it may falsely read a low temperature at all times.

    It also seems your first diagram has "Thermal Switch 2" written twice!

    However, the brightness logic is also interesting - in case both panels are hot, you suddenly decide to run both at 50% which means that if an existing panel is already hot and throttled back to 40%, it would then have to increase its output to 50% thus warming it up more. Perhaps putting both to 40% and dealing with a small loss of light output is more sensible. But as a demonstration of thermal switch behvaiour, that is fine -  it just doesn't seem all that practical as a real-life application as the cost could have been spent on better heatsinking/more LEDs to share the current.

    An interesting outcome nevertheless ...

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • karthikrajagopal
    karthikrajagopal over 4 years ago in reply to DAB

    Thanks DAB!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 4 years ago

    Nice experiment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • karthikrajagopal
    karthikrajagopal over 4 years ago in reply to navadeepganeshu

    Thanks navadeepganesh!
    Yes, I have applied thermal paste on the back side of the heatsink. I have included the picture of it in 'Mounting the Thermal Switch' section.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>