Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Experimenting with Waterproof Connectors Forum Enclosure IP rating confusion
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 36 subscribers
  • Views 3401 views
  • Users 0 members are here
  • waterproof connectors
Related

Enclosure IP rating confusion

JWx
JWx over 3 years ago

Hello!

after briefly studying enclosure datasheet I have found something strange: it is described as IP68 (NEMA 4, 4X, 6, 6P, 12, 13), but PDF provided

www.farnell.com/.../2239464.pdf

states only: NEMA 4, 4X

in addition, family description from manufacturer's site:

https://www.hammfg.com/electronics/small-case/plastic/1554

states that this family is "NEMA Type 4, 4X, 6, 6P, 12 & 13", "Except 1554/55 V size which is 4,4X only"

as there are a few part numbers with V inside (VGY, VALGY, VAGY, VBGY) I wonder if our enclosure (1554VA2GYCL) can be considered IP68 or NEMA4X (so no submersion allowed)?

  • Sign in to reply
  • Cancel

Top Replies

  • charlieo21
    charlieo21 over 3 years ago +3 verified
    I had a little chat with a Hammond Technical Product Specialist. She confirmed that our enclosure meets IP68.
  • ralphjy
    ralphjy over 3 years ago +1
    I saw that also. I had planned on a submersion test, but submersion is not required for my application. I would expect that since most of the enclosures have an IP68 rating, that it should meet the temporary…
  • dougw
    dougw over 3 years ago +1
    I think the statement that V size is only rated for Nema 4 (IP65) applies to this enclosure. I will be using it in an immersion application anyway and hopefully taking enough precautions to ensure the…
Parents
  • charlieo21
    +1 charlieo21 over 3 years ago

    I had a little chat with a Hammond Technical Product Specialist. She confirmed that our enclosure meets IP68.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ralphjy
    0 ralphjy over 3 years ago in reply to charlieo21

    Did you recommend that they amend the product description for the V size enclosures?  I missed that there were 4 and 6 screw versions (V vs VA/B).

    Maybe put an asterisk on the NEMA 4 units.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • charlieo21
    0 charlieo21 over 3 years ago in reply to ralphjy

    I think they need to improve the way that the information is showed or maybe a better part number definition.

    I did my own analysis, and I don't think that V means 4 screws and VA 6 screws. Also, you can have IP68 in a 4 screws version, the quantity of screws is determined by the size of the enclosure.

    My understanding is that the ABS lid is IP66, and the polycarbonate lid is IP68.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • charlieo21
    0 charlieo21 over 3 years ago in reply to ralphjy

    I think they need to improve the way that the information is showed or maybe a better part number definition.

    I did my own analysis, and I don't think that V means 4 screws and VA 6 screws. Also, you can have IP68 in a 4 screws version, the quantity of screws is determined by the size of the enclosure.

    My understanding is that the ABS lid is IP66, and the polycarbonate lid is IP68.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • JWx
    0 JWx over 3 years ago in reply to charlieo21

    Hello!

    I think it is unnecessary complicated (too many versions under one P/N) - ABS version is also for indoor use only...

    https://www.hammfg.com/electronics/small-case/plastic/1554

    • ABS Versions are molded from general purpose material which carries a flammability rating of UL94-HB.  For indoor use.
    • Polycarbonate versions are UV stabilized for outdoor use.  Gray polycarb carries a UL94-5VA rating, while clear and smoked lids carry a UL94V-0 rating.
    • [...]
    • Polycarb versions are designed to meet NEMA Type 4, 4X, 6, 6P, 12 & 13 ratings which meet and exceed IP ratings up to and including IP68.  (Except 1554/55 V size which is 4,4X only)
    • ABS Plastic versions are designed to meet IP66.