In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog Dust, Temperature and Humidity Monitor Chapter 5
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
  • Author Author: engswee
  • Date Created: 24 Nov 2014 4:39 AM Date Created
  • Views 989 views
  • Likes 2 likes
  • Comments 2 comments
  • haze_monitor
  • in_the_air
Related
Recommended

Dust, Temperature and Humidity Monitor Chapter 5

engswee
engswee
24 Nov 2014

(Best view still 1900 x 1200)

In this chapter I will introduce some detail for the hardware (humidity and temperature sensor) and a little bit on software.

  • Hardware:
    • BBB and BB view:
      • BBB
      • BB View 4.3"
    • SENSIRION EK-H5 & SHT75:
  • Software:
    • USB Sensor Viewer
    • MSP 430 Software Platform
      • IAR
      • Energia
      • CCS

Hardware:

Hardware is one of the important part for a device so I will try my best to go detail for this section.

I have list down most of the hardware use for this project (please refer to previous blog for detail).



BBB and BB view:


BBB

image

Testing the BBB out of the box. It just working like charm image

Using the cable HDMI D to HDMI A from element 14 (http://sg.element14.com/jsp/search/productdetail.jsp?sku=2127550&COM=drawer-part-list+CMPNULL)

Plug to TV, power it up and it working with no issue. It also working with the DC-DC converter supply from power bank with no issue.

Will going for WIFI connection or Ethernet connection and try for programing in future after finish with the hardware.

 


BB View 4.3"

It toke me few hour to found the correct link for the image file support the BB view and few more hour to download it image

I think better share it here so other have another alternative getting the file.

Tips: Google drive share file here (https://drive.google.com/folderview?id=0B7Dl_WxBoZJSSG0tNnU3RVpxUUU&usp=sharing) This share link is not permanent maybe broken without notice.

TI-SDK image and source code toke about 2hour each to download in Singapore.

The share file from Google drive with hope it will be faster then the given link.

 

Image NameImage (patched for BB View)Source Codes (patched for BB View)
DebianDebian ImageDebian Source Code
TI-SDKTI-SDK ImageTI-SDK Source Code
AngstromAngstrom ImageAngstrom Source Code
Utility Tools Download Tools

  

element14: BB View LCD Cape Software Download Centre[1]

 

 

 

SENSIRION EK-H5 & SHT75:

To the summary for this testing Sensirion EK-H5 + SHT75

Sensirion EK-H5 and SHT75 humidity sensor and temperature sensor is a complete set for testing.

This system only work in window OS. The application call Sensirion AG/USB RS485 Sensor Viewer.

It can be download from Sensirion webpage or by the given link (http://www.sensirion.com/en/products/humidity-temperature/evaluation-kits/ek-h5/ )

 

image

STH75 sensor and SHT2 sensor that come together with the evaluation kit.

Tips: please handle the SHT75 sensor with care because the PCB is small

 

image

This picture show the complete set of the Sensirion EK H5 and Sensor. It easy to setup.

There is no polarity for the sensor connection but it do not damage if install wrongly. So don't worry.

Software will show error when the sensor install wrongly. Just flip the sensor and problem solve.

 

image

This is the inside look of the USB converter. They using Cypress MCU for this and look like EZ USB Cypress chipset to me.

Almost remove the label to see the chip model he..he.. Maybe will do it if have request image

 

 

Software:

I will show some of the software related to the using hardware. This will not cover the detail of the software for this project.

There are few option for BBB, CC3200 and MSP430FR5969. It come with IAR, Energia and CCS

I like the IAR but this one come with size limitation image.

Energia is arduino similar platform. For those who using arduino it will be easy to get use of it.

 

 

USB Sensor Viewer

This is the software for the Sensirion sensor. I have tested with SHT2 sensor and SHT75 sensor.

Data also can be log using this software and the format is in excel sheet .csv file.

image

Picture show the USB Sensor Viewer work with SHT2x sensor.

 

image

This picture show the USB Sensor Viewer hock up with SHT75 sensor.

Face some issue at the beginning due to wrong polarity sensor install but problem solve when flip the sensor and reload the program (Tips: reload is place at the bottom right)

 

image

Taking some data with SHT75 sensor. Sampling rate at 1Hz

Maybe will make a more detail in future for this.

 

image

This is the example of data logging taking form the sensor using USB sensor viewer from Sensirion.

 

 

MSP 430 Software Platform

 

IAR

image

This is the IAR software for the MSP430 platfrom. This software can only use in Window OS.

 

 

Energia

image

Energia is arduino similar platform. This support OS platfrom and look like the only choice for MAC user.

 

 

CCS

image

CCS (code composer studio) from TI. Come with a lot of example and it just run in Linux and window.

This software is design to support a lot of MSP430 family. It will be long story if want to do a step by step for this, I think.

 

Some information related with the CCS but I think it not support the MSP430 family. I need to go a bit detail to tell about this GUI Composer from TI.

Category:GUI Composer - Texas Instruments Wiki

 

That all for software introduction more detail about software will be posted in the future chapter depend on which software is using for this project.

 

 

Interesting Information:

While doing search for example and getting reference form online. I just come across this spark io, they look interesting and using cc3000 TI WIFI module.

 

Plan to get one of this to try it out. But now can just pre order only image

https://www.spark.io/

 

The spark is available in cpc Farnell. Have anyone know what the different cpc farnell and just farnell or element14??

CORECA - SPARK - SPARK CORE, WIFI DEV BOARD, CHIP | CPC

 

For simple data capture service.

Internet of Things application development platform


Another data capture service for easy and simple use.

https://thingspeak.com/

 

 

Sharing:


Doraemon movie image

http://www.youtube.com/watch?v=LKc8q9GFeJc


 

Previous:

Dust, Temperature and Humidity Monitor Chapter 4

 

Next:

Dust, Temperature and Humidity Monitor Chapter 6

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    Very good update.

     

    I like the way you are approaching the problem and trying out the various tools.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Very good update.

     

    I like the way you are approaching the problem and trying out the various tools.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • engswee
    engswee over 11 years ago in reply to DAB

    TQ DAB

     

    Cheer

    ES