IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog BLOG 3 : The Kit Arrives
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
  • Author Author: gsgill112
  • Date Created: 9 Nov 2017 6:32 PM Date Created
  • Views 1556 views
  • Likes 2 likes
  • Comments 1 comment
  • iot on wheels design challenge
  • iot on wheels
  • stm32
  • iotonwheels
Related
Recommended

BLOG 3 : The Kit Arrives

gsgill112
gsgill112
9 Nov 2017

  PREVIOUS BLOG

  NEXT BLOG

 

Hello everyone, Sorry for delay in blogs, I was in transit and I am currently located HERE image So It Kinna difficult to stay connected to the world.

image

Moving on, as the part of the Challengers Kit we received the following Hardware,

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

But first lets go through the Unboxing Video image sorry for camera orientation image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

   UNBOXING VIDEO

 

{tabbedtable} Tab LabelTab Content
STM32L476RG NUCLEO

 

The Main processor board

image

The board is based on STM32L476RG MCU which boasts

    ARMRegistered 32-bit CortexRegistered-M4 CPU with FPU & ART Accelerator @ 80MHz

     1MB Flash memory

     128KB SRAM

    USB OTG 2.0 full-speed

    RTC with HW calendar, alarms and calibration

    24 capacitive sensing channels

    16x timers

    1x USER LED

    1x USER LED

    Arduino style headers + ST Morpho connectors (20x2 +20x2 Headers)

    ... And many more DATASHEET Download

 

 

For more details ON Development Board Click Here

Click here for info on the MCU

BLE Expansion Board

 

BLE Expansion Board - X-NUCLEO-IDB05A1X-NUCLEO-IDB05A1

imageimage

This Board is based on SPBTLE-RF BlueNRG-MS RF module and connects to the main Controller board over SPI BUS and Interrupts. It has Arduino comparable connectors and can be used with a Arduino comparable board.

 

The Kit is FCC Certified so you are goos to get the same in the final product.

image

And I am a huge fan of the Star Ground Pad on the 2x20 Header image image

 

Click here for E14 product page

Click here for ST page

Sensor Expansion Board

 

MEMS Sensor Expansion Board X-NUCLEO-IKS01A2X-NUCLEO-IKS01A2


This is a All in One Sensor package by ST which boasts the following

image  ST LSM6DSL MEMS 3D accelerometer (± 16 g) and 3D gyroscope (±2000 dps) 

image  ST LSM303AGR MEMS 3D accelerometer (±16 g) and 3D magnetometer (±50 gauss)

image  ST LPS22HB MEMS pressure sensor, 260 - 1260 hPa

image ST  HTS221HTS221 capacitive relative humidity and temperature sensor

image  It also packs the Arduino Headers image image

 

It connects all the sensors on an I2C bus for easy connectivity. and features some advance configurations like Free Fall detection, Single/Double tap gesture detection with sensitivity adjustment,  Etc.

 

Click here for E14 product page

Click here for ST page

 

imageimage

WiFi Expansion Board

 

WiFi Expansion Board X-NUCLEO-IDW01M1X-NUCLEO-IDW01M1

imageimage

This is a WiFi Expansion board based on the SPWF01SA module. The module itself is an STM32 WiFi SoC seen in wafer package. It boasts

image  512KB on chip memory

image  1 MB program flash memory 

image   Integrated TCP/IP, TLS/SSL

image   AT command set host interface

 

Click here for E14 product page

Click here for ST page

 

 

Moving on.

First Impressions

The unboxing of the package was more like a Squashed fruit opening, with the box completely crushed and the pins of the board somewhat damaged (nothing a powerful nail couldn't fix)

imageimageimage

after some Nailing image

image

 

So I moved on and Seams like there is a lot go GunK on the PCB's. Eeeyyuuuu .. .. ....

imageimage

And yes the Yellowish part on the headers is factory flux

imageimage

 

The WiFi Expansion board has ST Morpho connectors as only one side headers !!

 

 

Thanks for reading, More coming soon !!

Ohh I forgot This.

image

Thanks rscasny, for this lovely card.

//GS Gill

 

  PREVIOUS BLOG

  NEXT BLOG

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +1
    Nice update. Now you have to the toys to play with. DAB
  • DAB
    DAB over 8 years ago

    Nice update.

     

    Now you have to the toys to play with.

     

    DAB