IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog Traffic Predictor #10 - Evading traffic like a Bat
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
  • Author Author: dixonselvan
  • Date Created: 4 Nov 2017 9:54 AM Date Created
  • Views 1713 views
  • Likes 3 likes
  • Comments 4 comments
  • iot on wheels design challenge
  • iot on wheels
  • ardexpert
  • trafficpredictor
Related
Recommended

Traffic Predictor #10 - Evading traffic like a Bat

dixonselvan
dixonselvan
4 Nov 2017

Week 9 - Oct 30 - Nov 5

 

     This week I have planned to design and build module 2 & 3 in my trafficpredictor project. Check out the plan - Traffic Predictor #3 - The Plan and revisions, hardware & software list - Traffic Predictor #9 - Revisions and Hardware, Software list for a better understanding of the progress as I pause module 1 progress and shift to progress in module 2 & 3.

Module 2 - Auto-pilot mode with predefined speed using Sensor Expansion board

 

Module 3 - Speed adjustment with correspondence to current vehicular movement and real-time traffic

This module 2 title has been revised as above to "Auto-pilot mode with predefined speed". Please note in future I will be referring module 2 with the revised title.

 

Auto-pilot mode - term explained

     The term Auto-pilot is used to refer the act of helping the driver/ rider of the vehicle at frustrating times of traffic by providing speed values. This will not mean or involve integrating an auto driving mechanism without a driver/ rider into a fossil fuel/ electricity-powered vehicle. The output from this module in my trafficpredictor project can be used to auto drive electric vehicles [After alterations in the electric vehicle].

 

Introduction

     Module 2 & 3 have been integrated as one module as they both stand out to be similar in terms of functionality. Both are going to output or instruct the driver/ rider to maintain a particular speed. But they have minor difference in the way of gaining the output.

  • Module 2 - Static speed output from predicted route
  • Module 3 - Dynamic speed output from real-time traffic

 

Ultrasonic sensor to measure the speed

     An ultrasonic sensor is used here to determine the distance of the moving/ static traffic objects from the vehicle. Using change in distance and time, the speed alteration required in order to avoid a collision can be calculated. The formula to do this would be,

     image

     The setup has Ultrasonic sensor [Range: 0 to ~75cm] mounted on a Servo motor which will move from 0 to 180 degrees. This will capture a semicircle RADAR like output as shown below [Processing IDE has been used to display output as graph]. Using this the speed with which the driver/ rider should proceed will be calculated.

image

                   Processing IDE showing RADAR like output with input from Ultrasonic sensor

image

                              Ultrasonic sensor mounted on Servomotor

 

Hardware Explained - Video

 

The below video will explain the various hardware parts used for the entire trafficpredictor project. This has been achieved after a week's time of struggle with soldering, unit testing and integration of all the parts.

 

Do let me know your comments on the hardware build in terms for improvisation.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Progress made so far,

||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||   70%

{tabbedtable} Tab LabelTab Content
Entry & Introduction

IoT on Wheels Design Challenge - Traffic predictor and auto pilot mode

Traffic Predictor #1 - The Official Announcement

PlanTraffic Predictor #3 - The Plan
Initial Setup

Traffic Predictor #2 - Quest for the Code Editor

Traffic Predictor #4 - Finally, the kit arrives

Module 1

Traffic Predictor #5 - Machine Learning and Building a case for the kit

Traffic Predictor #6 - Into the traffic [Part 1 of 2]

Traffic Predictor #7 - Into the traffic [Part 2 of 2]

Traffic Predictor #8 - Predicting the best route to avoid traffic [Part 1 of 2]

Module 2 & 3

This blog

IntegrationYet to Begin
Revisions and Hardware, Software ListTraffic Predictor #9 - Revisions and Hardware, Software list

image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Nice update. DAB
  • dixonselvan
    dixonselvan over 8 years ago in reply to DAB +1
    Thanks DAB
  • phoenixcomm
    phoenixcomm over 6 years ago +1
    neat stuff as always
Parents
  • phoenixcomm
    phoenixcomm over 6 years ago

    neat stuff as always

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 6 years ago

    neat stuff as always

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dixonselvan
    dixonselvan over 6 years ago in reply to phoenixcomm

    Thanks phoenixcomm image