Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog Path II Programmable Blog 7 - Completing Zynq UltraScale+ MPSoC Software with Xilinx SDK
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
  • Author Author: avnrdf
  • Date Created: 3 Nov 2019 6:52 AM Date Created
  • Views 1574 views
  • Likes 4 likes
  • Comments 2 comments
  • ultra96-v2
  • path ii programmable
  • xilinx sdk
Related
Recommended

Path II Programmable Blog 7 - Completing Zynq UltraScale+ MPSoC Software with Xilinx SDK

avnrdf
avnrdf
3 Nov 2019

This blog post completes the Zynq MPSoC software training, most of which has been covered in Path II Programmable Blog 5 - Starting with Zynq UltraScale+ MPSoC Software with Xilinx SDK  and Path II Programmable Blog 6 - More Zynq UltraScale+ MPSoC Software with Xilinx SDK

 

SW Chapter 9 video: Interrupts

 

  • An introduction to hardware & software interrupts.
  • A look at the interrupt interface on Zynq MPSoc - multiple sources and multiple endpoints. The GICs are configurable and support multiple options.
  • A recap of how interrupt service routines handle interrupts.
  • ISR tips & tricks - keep things short, disable other interrupts when servicing certain IRQs etc.

 

imageimage

image

SW Lab 9 - Interrupts

 

  • Executed 2 applications which were the same as the applications we used in the HW lab to control the PWM IP - they accept a number over the UART and program the compare register of the PWM IP. The first application didn't use the interrupt capability, but the second application added that - which involved configuring the Zynq GIC to pass the interrupt signal from the PL to the PS.

 

 

SW Chapter 10 video: Xilinx Libraries

 

  • Xilinx libraries can be enabled (and imported) into a BSP. Each library may have some settings, which can also be configured using the wizard.
  • Different Xilinx System Access Libraries: FAT file system, TCP/IP stack, security algorithms, serial flash library
  • Xilinx includes example code with their libarries

image

 

SW Lab 10 - Xilinx Libraries

 

  • Created a new application & BSP. The xilffs (Xilinx Fat File System) library was imported during BSP generation.
  • Imported the provided C source file for an application that writes values from the System Monitor to a CSV file on the SD card, and explored the xilffs APIs that it uses
  • I didn't want to overwrite my SD card which had already been flashed with an image, so I didn't execute the application. It's pretty simple - it initializes the System Monitor, reads the temperature using the driver API and stores it in an array. It then creates a file on the SD card and prints a formatted string in a buffer to the card.

 

image

 

SW Chapter 11 video: Interfacing with Sensors

 

  • Connecting to a MikroElectronika 'click' sensor board via the mezzanine card which is connected to low speed connector.
  • There is a large ecosystem of 'click' boards.
  • Will use the PS SPI to talk to the click board. Will use the Xilinx SPI library (driver).

imageimage

imageimage

image

SW Lab 11 - Click Mezzanine Standalone Environment

 

I did not have a LSM6DSL sensor with me, so I did not complete this lab. However, it did not involve anything too complex:

 

  • Had a look at the Xilinx SPI driver APIs.
  • A short part on how the SPI clock prescaler needs to be calculated - the root clock is much more flexible than on a MCU. While a MCU might have a couple of possible values, the larger number (and range) of possible PLL settings on Zynq mean that users need to be a little more careful.

 

SW Chapter 12 video: Next Steps

 

  • A recap of what we covered in the software training.
  • Another recap of the Xilinx ecosystem: IP, reference designs, design kits.
  • Where to get help & support, and find documentation.

image

 

That completes the software course!

  • Sign in to reply
Parents
  • aspork42
    aspork42 over 6 years ago

    Nice write up. Have you gotten through the Petalinux stuff yet?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 6 years ago

    Nice write up. Have you gotten through the Petalinux stuff yet?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • avnrdf
    avnrdf over 6 years ago in reply to aspork42

    Some of it - will be posting those blogs when I get the time.