Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog Pi Control Hub:Spoke2:Blinds Automation(continued)-3D Printing Holder and Motor mount
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
  • Author Author: carmelito
  • Date Created: 11 Aug 2016 11:21 PM Date Created
  • Views 2170 views
  • Likes 1 like
  • Comments 4 comments
  • 3dprint
  • pi
  • picontrolhub
  • piiot
  • enocean
  • raspberry pi
  • piiot challenge
Related
Recommended

Pi Control Hub:Spoke2:Blinds Automation(continued)-3D Printing Holder and Motor mount

carmelito
carmelito
11 Aug 2016

The previous two blog post, we added the EnOcean Transceiver module to a Raspberry Pi B+ and setup up FHEM home automation server and wrote python code taking advantage of the telnet port to blink some LEDs and capture the temperature from the EnOcean sensor Kit. In addition we also used a Motor driver to drive a gear motor when the Push Button is pressed. These two blog post,  are the perquisite to this blog

Pi Control Hub:Spoke 2:Blinds Automation-- Setting up EnOcean Sensor and Blinking LEDs 

Pi Control Hub:Spoke2:Blinds Automation(continued)--Driving Motor with EnOcean PushButton

 

Here is a video demo of the blinds opening and closing in action, using the EnOcean Push button..

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

3D print the STL files attached below to hold the Raspberry Pi B+ and the motor driver. And also print a holder for the gear motor and mount for the blind's turning rod.

Here are the slicer setting I used on my Flashforge creator pro

Layer height - 0.3 mm

Infill density - 20%

Temperature - 205 C (i am using Hatchbox White 1.75mm PLA )

 

 

 

{gallery:width=900,height=400,autoplay=true} 3D printed part for Blind Automation using Raspberry Pi and EnOcean Sensors

image

Final setup of the with the 3D printed parts + Raspberry Pi with the EnOcean Transceiver module+ Gear Motor attached to roller rod of the blinds.

image

3D printed base holder for the Raspberry Pi B+..Parts designed in Autodesk Fusion 360

image

3D printed base and top, that is the case for the Pi and the EnOcean Transceiver module

image

Soldering ...

image

Putting the Circuit together

image

Adding zip tie to hold the motor driver, and adding screws to hold the 3D printed parts together..

image

Adding the motor to the 3D printed part

image

Adding 3D printed motor mount, ensure that the screw lines up with the notch in the gear motor.

image

Mount your setup on the wall next to the blinds and test it using an EnOcean Push button..

 

 

In addition to 3D printing the STL's attached , we will also need a zip tie to hold the motor driver to the 3D printed part as shown in the picture above.

And 4-40x3/8 screws to fit all of the 3D printed parts together

Hot glue to add the blinds rolling rod to the motor mount and screws and a drill to mount the parts to the wall ..

 

As part of the next steps, i am going to have to

- Find a longer USB cable image.

- Also find another USB cable which I will have to cut to power the gear motor, instead of the 4 AA battery pack.

- Measure the approximate time it takes the blinds to Open/Close and modify the python program, so that I can use the other two side of he EnOcean push button for some other functionality ,      like switch the table lamp On/Off ..

Attachments:
BlindsAutomationSTLs.zip
  • Sign in to reply
Parents
  • clem57
    clem57 over 10 years ago

    Love the blinds opener.

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • carmelito
    carmelito over 10 years ago in reply to clem57

    Thanks for the comment clem57, did some more testing in the night, pretty happy with the way it turned out image..the only annoying bit is sound the gear motor makes, i think I am going to replace it with a stepper in the future..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • carmelito
    carmelito over 10 years ago in reply to clem57

    Thanks for the comment clem57, did some more testing in the night, pretty happy with the way it turned out image..the only annoying bit is sound the gear motor makes, i think I am going to replace it with a stepper in the future..