PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - Kinetic Art Mobile - Post 5 - Finally a PCB design.
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
  • Author Author: genebren
  • Date Created: 2 May 2019 3:45 PM Date Created
  • Views 3229 views
  • Likes 14 likes
  • Comments 21 comments
Related
Recommended

PiCasso Design Challenge - Kinetic Art Mobile - Post 5 - Finally a PCB design.

genebren
genebren
2 May 2019

Prior posts in the PiCasso Design Challenge:

PiCasso Design Challenge - Kinetic Art Mobile - Post 1

PiCasso Design Challenge - Kinetic Art Mobile - Post 2

PiCasso Design Challenge - Kinetic Art Mobile - Post 3 - Will it go round in circles????

PiCasso Design Challenge - Kinetic Art Mobile - Post 4 - Crash of the Death Star

 

Things have been crazy here lately.  I have been very busy trying to finish out the interior of my new workshop, while attempting to keep my PiCasso project moving.  I have stuck in a re-design cycle, where I have been moving components from board to board, trying to get everything to fit, in a reasonable way.  After multiple re-starts on the design, I think I have a workable design.

 

There are several different requirements on the design that have made it fairly difficult to find the right approach.  Here are a few of them:

  • uniform LED spacing to allow proper illumination of the orb and to allow some 'animations' based on different LED color patterns and sequences.
  • relatively high power (LED and Fan power)
  • fan speed control (based on programmable constant current)
  • BLE transciever
  • Magnetic compass and accelerometer

 

I went through several trade off, trying to keep all of the high speed stuff on a single board, versus the space required for connectors should I distribute the components across multiple boards.  Here is what I ended up with:

imageimage

The Main PCB is riddled with 12 - 0.1" holes to allow additional air flow, through the board, into the fans below (there will also be some airflow around the board edges).  I will be trimming the PCB into a circle, as my PCB vendor (lower cost) only allows for rectangular boards.  The LED boards are sort of a universal design that will be connected to the main PCB, providing pairs of  LEDs along the circumference of orb and a single LED providing downward lighting (right angle mounted, hacked LED PCB).  This will provide me with 18 - fully programmable RGB LED to illuminate the sides and bottom of the orbs.

 

Here are the schematics of the main controller and LED board:

imageimage

image

 

I will need to send these boards of soon and order up parts for the board, but for now, I heading out to the workshop to install drywall and lighting.

 

Thanks for reading along.  I hope that I can get this project moving along a bit faster, so I can meet the deadlines.

 

Thanks,

Gene

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago in reply to dubbie +6
    Thanks Dubbie. I have been laying out PCBs for quite a while (45+ years). I go back to self etched boards, using resist pens, tape or photoresist film (1970's), through many different design packages.…
  • genebren
    genebren over 7 years ago in reply to ralphjy +6
    Ralph, I do all of my assembly by hand (under a microscope). I do not have a reflow oven yet, but it is on my wish list for future tool purchases. The LSM303C (3D accelerometer and 3D magnetometer) is…
  • dubbie
    dubbie over 7 years ago +5
    Gene, Impressive PCB design. I've done a few simpler ones in my time but nothing like this. Dubbie
  • genebren
    genebren over 7 years ago in reply to dougw

    Doug,

     

    That is a very nice looking PCB.  I really like the white mask.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to genebren

    I laid out a 32-pin LGA a couple of evenings ago (some clock part for my old DDS project) and for any 0.5mm pitch although I guess it isn't best practice (I don't know : ( but personally I switch off the tStop and tCream layers, and do them manually (i.e. so that the overall design rules don't apply). That way, I can get a bit of solder mask in-between the pads (although it can arrive broken! the low-cost manufacture seems to not be able to do the mask in-between reliably especially at 0.4mm pitch, but 0.5mm is just-about feasible I hope).

    Like you, I have variable results, I'm confident of the pasting and positioning, but I suffer from low-power heat sources : (

    With the low-temp solder I'm going to try to get nearly all heat from the pre-heater, so that the hot air gun is barely (or not) needed.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to genebren

    If you need a circular card in the future, I had a low-cost Heart Reactor PCB made at itead that turned out great - it was white to reflect light well.

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to shabaz

    Thanks shabaz,

     

    I rarely change angles away from 90 degree increments, but in this case, in order to get the LED pointed correctly, I had to do at least the connector at an angle.  Once that was done, it did not make sense to have the connected ICs at a different angle, so they moved too.  It sure is strange routing traces away from the off angle components, back to my normal 45/90 degree traces.

     

    The LGA packages are going to be an adventure.  I has tried some leadless parts in the past, with varying degrees of success, so it is hard to predict how this will go.  I have put some serious thought into getting/building a small reflow oven just for these types of parts.

     

    Thanks again,

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to balearicdynamics

    Thanks Enrico,

     

    Your suggestion is valid, but in this instance, the PCB manufacturer is building a square.  I will be trimming the square down into a circle.  I may in fact, merge some of the close drill holes into a single opening, gladly losing some of the circle edge to increase the opening size to increase airflow (my air intake to the orb will be above the controller PCB).

     

    Thanks again,

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>