PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - Kinetic Art Mobile - Post 5 - Finally a PCB design.
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
  • Author Author: genebren
  • Date Created: 2 May 2019 3:45 PM Date Created
  • Views 3234 views
  • Likes 14 likes
  • Comments 21 comments
Related
Recommended

PiCasso Design Challenge - Kinetic Art Mobile - Post 5 - Finally a PCB design.

genebren
genebren
2 May 2019

Prior posts in the PiCasso Design Challenge:

PiCasso Design Challenge - Kinetic Art Mobile - Post 1

PiCasso Design Challenge - Kinetic Art Mobile - Post 2

PiCasso Design Challenge - Kinetic Art Mobile - Post 3 - Will it go round in circles????

PiCasso Design Challenge - Kinetic Art Mobile - Post 4 - Crash of the Death Star

 

Things have been crazy here lately.  I have been very busy trying to finish out the interior of my new workshop, while attempting to keep my PiCasso project moving.  I have stuck in a re-design cycle, where I have been moving components from board to board, trying to get everything to fit, in a reasonable way.  After multiple re-starts on the design, I think I have a workable design.

 

There are several different requirements on the design that have made it fairly difficult to find the right approach.  Here are a few of them:

  • uniform LED spacing to allow proper illumination of the orb and to allow some 'animations' based on different LED color patterns and sequences.
  • relatively high power (LED and Fan power)
  • fan speed control (based on programmable constant current)
  • BLE transciever
  • Magnetic compass and accelerometer

 

I went through several trade off, trying to keep all of the high speed stuff on a single board, versus the space required for connectors should I distribute the components across multiple boards.  Here is what I ended up with:

imageimage

The Main PCB is riddled with 12 - 0.1" holes to allow additional air flow, through the board, into the fans below (there will also be some airflow around the board edges).  I will be trimming the PCB into a circle, as my PCB vendor (lower cost) only allows for rectangular boards.  The LED boards are sort of a universal design that will be connected to the main PCB, providing pairs of  LEDs along the circumference of orb and a single LED providing downward lighting (right angle mounted, hacked LED PCB).  This will provide me with 18 - fully programmable RGB LED to illuminate the sides and bottom of the orbs.

 

Here are the schematics of the main controller and LED board:

imageimage

image

 

I will need to send these boards of soon and order up parts for the board, but for now, I heading out to the workshop to install drywall and lighting.

 

Thanks for reading along.  I hope that I can get this project moving along a bit faster, so I can meet the deadlines.

 

Thanks,

Gene

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago in reply to dubbie +6
    Thanks Dubbie. I have been laying out PCBs for quite a while (45+ years). I go back to self etched boards, using resist pens, tape or photoresist film (1970's), through many different design packages.…
  • genebren
    genebren over 7 years ago in reply to ralphjy +6
    Ralph, I do all of my assembly by hand (under a microscope). I do not have a reflow oven yet, but it is on my wish list for future tool purchases. The LSM303C (3D accelerometer and 3D magnetometer) is…
  • dubbie
    dubbie over 7 years ago +5
    Gene, Impressive PCB design. I've done a few simpler ones in my time but nothing like this. Dubbie
  • genebren
    genebren over 7 years ago in reply to DAB

    Thanks DAB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to fmilburn

    Frank,

     

    (Funny, but I thought that I replied to your comment earlier)

     

    Thanks.  I have trimmed PCBs before, with a metal cutting blade in a bandsaw.  I sold my last bandsaw prior to moving to Texas, and it was my first planned purchase to outfit my new workshop (maybe I might have to buy one sooner, as it will help with some of the finish details).  After rough cutting the board outline, I finished the edges on a benchtop belt sander.  I have also used the rotary stage on my benchtop mill, to score the edge and then nibble away the corners and then again, finish with sanding.

     

    It is a very messy process, but going slow and cleaning frequently, it comes out pretty well.

     

    Thanks again,

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to genebren

    Nice layout.

    That reminds me - I still have a bunch of red and blue tape of different widths, and a light table, but there is no chance that tape will be used for future layouts....

    (although... thinking about it - it would now be simple with digital photography editing to separate the layers by colour)

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi Gene,

     

    This is looking fantastic : ) It's nice that you're not afraid to change angles to get your components located where you want them : ) Regarding circle, the low-cost PCB manufacturers seem fine with routing out shapes, e.g. with the mouse-bites, so that could be an option too (i.e. lines on layer 46 in EAGLE). They do sometimes query via an e-mail to double-check they've got it right, so if you're on a timeline that's something to watch out for.

    For the LGA package etc., my pre-heater and hot air tool are underpowered, so recently I've thought about trying low-temp solder paste with it. I don't know if it will work though! I'll try it in a few weeks time, I'll be sending a couple of PCBs to be made in a week or so. The one I went for is called Qualitek Delta 670.

     

    Anyway, it's a really nice design and layout, it's clear a lot of effort went into it! It takes me days to route out stuff tidily.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago

    professional PCB design... Really!  Can I suggest something that has already created issues for me in the past?

    Well, I suppose you say yes image The idea of the holes for air flow is really great. The top left two holes, in my opinion, are too near to the border, so you risk that during the fabrication the PCB will be damaged as they make holes drilling the finished printed PCD (at least in most of the cases). As well as the same holes seem dangerously near to the PCB track.

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>