Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog Automatic Dough Shaper - Blog #1
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
  • Author Author: a_davis_22
  • Date Created: 21 Jan 2018 5:27 AM Date Created
  • Views 2026 views
  • Likes 10 likes
  • Comments 12 comments
Related
Recommended

Automatic Dough Shaper - Blog #1

a_davis_22
a_davis_22
21 Jan 2018

Wow, I'm so excited to be doing this challenge! But I'm also really nervous. There are a lot of more experienced engineers and this will be the most complicated project I've done on my own. But what better project to do than a fun and not quite impossible challenge? Well, here I go - to the finish line!

 

Project Overview:

 

As stated in the synopsis, I'm basically making a cnc cookie machine. Dough goes in, cookies come out. It easily extends to other baked goods as well, like homemade crackers and pie crust, but the first goal is to get some creative cookies perfectly cooked!

 

The machine consists of 3 main parts. A dough sheeter, the xy plotter and a toaster oven. The dough is flattened to the correct thickness, cut into the perfect shape, and then put into the preheated toaster oven, cooked, and removed - all while I take care of other, non-automated household chores (but more likely just stand there and watch it in fascination).

 

image

 

 

The Raspberry Pi will control the following elements:

  • Display what is being cut
  • Get and interpret gcode from a pre-selected shape
  • Move the platform and cutting head to coordinate as an xy plotter
  • Move the roller up/down/hold position
  • Temperature control on oven
  • Options for delay times, preheating, cooking time, pausing, allowing user to clear excess dough from pan before cooking, etc.

 

The touch screen will be the user interface to select:

  • the dough height
  • the image to be cut
  • the preheat setting
  • the cooking time
  • starting/pausing/stopping the process, and
  • allowing the user to save settings

 

The kit is scheduled to arrive Monday for me and I'm really grateful for this opportunity. I hope you all enjoy this journey with me!

What kind of cookie do you want?

  • Sign in to reply

Top Comments

  • e14phil
    e14phil over 8 years ago +4
    Hi AnnaLisa This was one of my favorite proposed challenges of all time, I really look forward to seeing how you make this happen. Don't worry about people knowing more or less than you, this community…
  • three-phase
    three-phase over 8 years ago +3
    Quite an ambitious project, good luck with it! Kind regards
  • beacon_dave
    beacon_dave over 8 years ago +2
    This looks like a great project. An alternative approach might be something along the lines of the pancake printers which use an additive rather than a subtractive approach. Pancake CNC machine on Instructables…
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    This looks like a great project.

     

    An alternative approach might be something along the lines of the pancake printers which use an additive rather than a subtractive approach.

     

    Pancake CNC machine on Instructables (converted X Carve CNC machine)

    Pancake CNC Machine (Turn Your CNC Into a Pancake Machine): 11 Steps (with Pictures)

     

    Pancake Printer on Instructables

    Pancake Printer: 10 Steps (with Pictures)

     

    PancakeBot on Kickstarter

    https://www.kickstarter.com/projects/1853707494/pancakebot-the-worlds-first-pancake-printer

     

    The main difference I suspect here would be the thicker consistency of the dough versus batter and that it would require an oven rather than a hot plate.

     

    You used to get handheld gadgets with a plunger driven off a lead screw for cake decorating which could perhaps save some work by mounting one on the XY carriage and hooking up its motor to a motor controller connected to the R-Pi. This would allow you to plot the dough rather than carve it.

     

    However I suspect that the dough sheet may play an important part in the baking of cookies which is why it looks as if you are planning on carving out of the dough sheet ? By the sounds of it you are looking at taking more of a vinyl cutter type approach here with the CNC side controlling some sort of a blade.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to beacon_dave

    Was just thinking that for a cutter head you perhaps could use a pin punch technique to punch a line of small dots in the cookie dough to create the outline of the cookie using a mechanism similar to that of a dot matrix printer head or a tattoo gun. This could avoid the need to rotate a cutting blade as you change the direction of cut. Should be fairly easy to keep clean as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 8 years ago in reply to beacon_dave

    Was just thinking that for a cutter head you perhaps could use a pin punch technique to punch a line of small dots in the cookie dough to create the outline of the cookie using a mechanism similar to that of a dot matrix printer head or a tattoo gun. This could avoid the need to rotate a cutting blade as you change the direction of cut. Should be fairly easy to keep clean as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • a_davis_22
    a_davis_22 over 8 years ago in reply to beacon_dave

    Thanks, I hadn't even thought of doing an additive approach. That would be interesting.