Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog iTender #1
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
  • Author Author: justin.berger
  • Date Created: 22 Jan 2018 5:30 PM Date Created
  • Views 1634 views
  • Likes 9 likes
  • Comments 5 comments
  • cocktail
  • raspberry
  • itender
  • pi chef
  • drink
  • cooling system
  • raspberry_pi_design_challenge
Related
Recommended

iTender #1

justin.berger
justin.berger
22 Jan 2018

image

Hello,

My name is Justin BERGER and I am currently working on an automatic bar project.

This is a device for making cocktails with pumps sending different drinks into a glass.

I have been thinking about this project for several months. This contest will give me a deadline and give a boost for the realization of this automatic bar. But will also allow me to exchange with people interested on this project.

 

     1. The advantages of the project

 

More and more people drink cocktails, so to have a machine able to make them automatically seems a very good idea.

     -     Do you want to be able to make one of many cocktails with just one click?

     -     Do you want to be able make your favourite cocktails over and over again?

     -     Do you want to have your cocktail served cold?Do you want to be able to pour your cocktail at a distance by smartphone or web and have it ready when you arrive home or from the bath?

 

My goal is to build a project that packs all this into one machine.

image

     2. The initial tests

 

For the moment I have written a program for sending liquids in the proportions we want and I have installed the pumps to conduct pilot tests which have proven conclusive. I will make a cabinet to install it in and to present it all beautifully. To do this I have access to a joinery  workshop.I plan to improve the project by installing a cooling system so as to serve the drinks cold. To do this I will use Peltier modules. I have started testing on this. It represents a significant amount of work.

 

    imageimage               image     image                   image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

     3. Project timeline :

 

    • Study
      • Design and modelling in 3D
      • Studying the different possibilities for pouring a cocktail
      • Researching a cooling system - the objective is to have a system that is easy to use,  similar to a beer tap.
    • Production
      • The building of the pump system
      • Programming the raspberry
      • Installing the components
      • Wiring
      • Pilot testing
    • Building the cooling system
      • Studying the best system allowing cooling of the drink whilst respecting food and electrical norms and avoiding getting too cluttered
      • The goal is to design a system that is easy to start up
      • Pilot testing
      • Installing the various components of the cocktail maker into the cabinet
    • Electrical power source. The Peltier modules require a DC power supply.
    • Building into the cabinet. The objective is to have beautiful object which is easy to use and, if possible, transportable


JanuaryFebruaryMarch
12345678910111213
Test with big pump for alcohol
Implementation of the probe DS18B20
Test of cooling regulation with PID
Plan of the cooling system
Manufacturing of the cooling system
Manufacturing of the electric part for installing in the cabinet
Modelling of the cabinet
Manufacturing of the "tap"
Integrating the additional relays + heat exchanger
Building the cabinet
Integrating a system of voice command
Integrating a Matrix LED or touch screen

 

I believe this project fits well into the "Pi Chef Design Challenge Cook, Bake & Brew with Raspberry Pi"”competition as it allows us to develop a system to make a multitude of cocktails relatively easily. It is also an object which is attractive as allows people to make cocktails easily using a straightforward program.

 

     4. 2 important points

    • Innovation : I have not yet seen a cocktail machine which cools your drink. The cooling system is therefore an innovation.
    • Engineering: there is an important technical aspect as this involves a good electrical power source and an effective hydraulic circulation and heat exchange system 

 

     5. Received Element14 parcel

 

imageimageimage

I was delighted to receive the element14 parcel. It’s a huge boost towards the completion of this project. I’m sure i’ll make really good use of many of these. I plan to use and test the :

  • Explore NFC Expansion board

  • Sense Hat

  • 2.4" Touch Screen Hat

  • Raspberry Pi3

Conclusion

I constantly set myself challenges, but must admit that this is the first time that I have embarked upon such an adventure. I am very invested in this project and it interests me alot.

This drinks and fresh cocktail distribution system is a real challenge. I will probably face difficulties, but I will set up work processes that will solve these one after another. I have already started testing/tasting cocktails and ordering the equipment to test for cooling. This will allow me to expand my skills.

I will have to study many possibilities and make several tests for the "cooling" system because it requires transversal knowledge in several domains (electronics, refrigeration, hydraulics ...).

Furthermore once the cooling system works well, integrating an android app with voice control will add significant innovation to the project.

Taking part in this competition gives a huge boost to this project and means a lot to me.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 8 years ago +2
    Looks like another great project. The 'Drinkmotizer' project posted on here around 4 years ago may be of some interest to you: The Drinkmotizer - a Raspberry Pi Drink Mixing Robot It takes a slightly different…
  • justin.berger
    justin.berger over 8 years ago in reply to genebren +2
    You are welcome in France to a future party with iTender! I would like to cool the liquids while they are in the tubes. I will create similar system as the beer shooter. For cooling the heat part of the…
  • genebren
    genebren over 8 years ago +1
    Justin, When is the party? It looks like you are off to a great start. Heating and cooling liquids with Peltier devices takes quite a bit of energy. Do you plan to cool the liquids while they are in the…
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    Looks like another great project.

     

    The 'Drinkmotizer' project posted on here around 4 years ago may be of some interest to you:

    The Drinkmotizer - a Raspberry Pi Drink Mixing Robot

     

    It takes a slightly different approach to the challenge but it still may give you some ideas.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 8 years ago

    Looks like another great project.

     

    The 'Drinkmotizer' project posted on here around 4 years ago may be of some interest to you:

    The Drinkmotizer - a Raspberry Pi Drink Mixing Robot

     

    It takes a slightly different approach to the challenge but it still may give you some ideas.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • justin.berger
    justin.berger over 8 years ago in reply to beacon_dave

    Hello Dave,

    Thanks for your advices  I read it...

    Justin