Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog The Spice of Pi - Blog Doug 5
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
  • Author Author: dougw
  • Date Created: 12 Feb 2018 4:36 AM Date Created
  • Views 1026 views
  • Likes 7 likes
  • Comments 2 comments
  • doug wong
  • spice of pi
  • pi chef design challenge
  • pi chef
Related
Recommended

The Spice of Pi - Blog Doug 5

dougw
dougw
12 Feb 2018

This week the Spice of Pi project has seen incremental steps in both the right direction an the wrong direction along with a lot of spinning of wheels both figuratively and literally. Last week I got the jar lifting servo mechanism built and this week I worked on getting the platter rotation mechanism working.

The first few days were spent trying to assemble and tune a low-cost 3-D printer that was large enough to print the platter. It is together and printing but I'm still not happy with the performance. It did a reasonable job on some tripod brackets for my camera, but I'm sure it can do better, I just need to adjust the temperatures I think. Anyway, I'm waiting for a new roll of filament before attempting the big spice jar platter shown in my last blog.

Next I designed an adapter to allow a servo motor to rotate a 15 tooth pulley. I am using a rubber belt pulley drive because I want to minimize shock to the servo gears. The adapter worked pretty well as seen in the next video, but I discovered the set screws in the pulley were not actually at 90 degrees as I had assumed from looking at them. The actual angle is around 112 degrees. I carved the adapter up to make things fit but it was going to require a new adapter to make things fit well.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

When I tried the servo motor I discovered it was a continuous rotation servo instead of a 360 degrees servo. I was sure the motor spec indicated it was a 360 degree servo, but the terminology seems to be loosely used.

I happened to have a 180 degree servo, but to make it work for 360 degrees, I needed to have a drive pulley with twice as many teeth as the platter pulley, so I did not fix the adapter for the old pulley - I worked on a new pulley instead.

China is shut down for 2 weeks and an order now might not get here in time, so I designed the entire pulley to be 3-D printed. Fortunately it came out beautifully and fit the belt perfectly.

Then it crossed my mind to check why the servo wasn't the 360 degree servo that I expected. It turns out that it was a spare servo I ordered in case we need to build a second unit for Glenn (my partner on the project). The original servo actually works the way I intended, although I was surprised that without power the gears are completely locked. So now I had a nice pulley with the wrong number of teeth since this servo needs a 1-to-1 ratio.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

So back to the drawing board to design a corresponding pulley for the platter. Again the print came out great, so I put a couple of bearings in a vise to demonstrate the belt drive does indeed work.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

By the way, I find these rubber-jaw, ball joint vises indispensable for working on the bench. They make super third and forth hands for holding wires, components, PCBs or anything else at any angle and as shown above they are useful for mechanical mock-up and assembly as well. Suppose you want to hold a wire up to a component while you solder them together with solder in one hand and soldering iron in the other hand.

The next step is to design mounts for the bearings and the drive motor with a way to adjust belt tension.

This blog documents that incremental progress is being made on the project, although this last week was pretty hard slogging.

 

 

Design Challenge Links:

Pi Chef Design Challenge

About the challenge

The other challengers

The kit

Terms & Conditions

Summaries by Charles Gantt

 

Project Links:

Blog Doug 1 - The Concept

Blog Glenn 1 - AIY Voice Kit Unboxing

Blog Doug 2 - The Block Diagram and Bill of Materials

Blog Doug 3 - Spice Jar Lift Mechanism

Blog Glenn 2 - Firmware Considerations

Blog Doug 4 - Carousel Design

Blog Doug 5 - Platter Rotation Mechanism

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +2
    Very nice work. You did a great job on those gears. You are making great progress on your project. Gene
  • DAB
    DAB over 8 years ago +2
    Great update Douglas. Every project meets reality in the end and you have to adapt your design to the lessons learned during testing. Great fix. DAB
Parents
  • genebren
    genebren over 8 years ago

    Very nice work. You did a great job on those gears.  You are making great progress on your project.

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Very nice work. You did a great job on those gears.  You are making great progress on your project.

    Gene