Sci-Pi Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sci-Pi Design Challenge
  • More
  • Cancel
Sci-Pi Design Challenge
Blog Raspberry Pi-based Experiment Logger: Glimpses of the Kit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sci-Pi Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: aaryan2134
  • Date Created: 27 May 2023 7:31 AM Date Created
  • Views 1466 views
  • Likes 8 likes
  • Comments 2 comments
  • sci-pi
  • the kit
  • raspberry pi
  • raspberry pi 4 b
  • Remote Lab
  • unboxing
  • sci-pi design challenge
Related
Recommended

Raspberry Pi-based Experiment Logger: Glimpses of the Kit

aaryan2134
aaryan2134
27 May 2023

Blog List:

1. Raspberry Pi-based Experiment Logger and Analyzer with Remote Lab Control

2. Raspberry Pi-based Experiment Logger: Glimpses of the Kit

3. Raspberry Pi-based Experiment Logger: Wiring up Raspberry Pi 4 B

4. Raspberry Pi-based Experiment Logger: System Concept & Workflow

5. Raspberry Pi-based Experiment Logger and Analyzer with Remote Lab Control: Ready, Set, Go!

Introduction:

In this blog, I will go through the unboxing of the kit and have a broad view of the kit as well

Unboxing:

image

image

image

image

imageimage

image

image

Close Up view of the Raspberry Pi 4 Model B:

image imageimageimageimage image

Micro HDMI to HDMI Adapter:

image

I was waiting for this arrive before I completed the blog going into the kit. I earlier thought that it had an HDMI port but later on when I tried to connect it with my monitor I noticed that it had a Micro HDMI Port. So, I decided to go with the Micro HDMI to HDMI adapter in place of the cable as I had a few extra cables and this adapter was pretty cheap in comparison to the whole cable (Less than 1 USD).

You can find it here on Amazon.

Kit Specifications:

The Raspberry Pi 4 comes in 3 RAM versions - 1 GB, 2 GB and 4 GB variants. The one that I received for this challenge is the 4 GB LP-DDR4 RAM variant.

Additional Specifications are:

image Broadcom 2711, Quad-core Cortex-A72 64-bit SoC @ 1.5 GHz

image VideoCore VI Graphics Processor

image Gigabit Ethernet

image Dual micro-HDMI outputs

image 2x USB 2.0 “Hi-Speed” ports

image 2x USB 3.0 “Super-Speed” ports

image Bluetooth Low Energy (BLE) 5.0

image Dual Band Wireless LAN (2.4Ghz and 5Ghz) with IEEE 802.11 b/g/n/ac support with new on board antenna

image Up to 4K UHD native output over two HDMI ports (1x 4Kp60 or 2x 4Kp30)

image H.265 decode (4Kp60)

image H.264 decode (1080p60),

image OpenGL ES 1.1, 2.0, 3.0 graphics

image 40 pin extended General Purpose Input-Output (GPIO)

image 4 pole Stereo output and Composite video port

image Camera Serial Interface (CSI) port for connecting the Raspberry Pi Camera

image Display Serial Interface (DSI) port for connecting the Raspberry Pi Touch Screen Display

image microSD port for loading your operating system and storing data

image Upgraded USB-C power source (recommended 3Amps)

image The same standard form factor as previous Raspberry Pi boards!

The Ports:

image         image

Kit Contents:

1. Rasberry Pi 4 Model B - 4GB Variant

2. Instruction Manuals

Additionally, along with these things we require the below things:

1. Monitor (this is optional)

2. Micro HDMI to HDMI Cable (this is required if you want to use a monitor)

3. Keyboard and Mouse (for interfacing with the Raspberry Pi)

4. A Micro SD Card (Preferably a high speed one with atleast 16GB of Memory)

5. A Type C Adapter with 3 Amps (I am planning to use my mobile's charger which I is also able to provide 3 Amps)

Now, in the next blog we will see how we can wire up our Raspberry Pi 4 B for the first time and have a look at the experience as well!

  • Sign in to reply
Parents
  • DAB
    DAB over 3 years ago

    Yes, the Pi 4 is a nice system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aaryan2134
    aaryan2134 over 3 years ago in reply to DAB

    Yeah!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aaryan2134
    aaryan2134 over 3 years ago in reply to DAB

    Yeah!